Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) "Flip View" button
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 190 subscribers
  • Views 6441 views
  • Users 0 members are here
Related

"Flip View" button

e14 Contributor
e14 Contributor over 15 years ago

When routing the back of a board, it would be really nice to be able to

flip the view to see the back of the board as it really is.

 

It would be extremely useful when debugging a board, as it's really painful

to find a signal in eagle, then mentally flip it to find it on the physical

board.

 

It would also be useful for checking text layout on the back of the board.

Mentally flipping text is a bit of a pain, and almost impossible when

you're trying to evaluate its aesthetic appeal. Yes, I do consider

aesthetics important in PCB design!

 

I know I can print out the board mirrored, or group-then-mirror, and

various other hacks, but if this button existed, I'd click it every minute

or so when routing a complex design.

 

In fact, I'd prefer the board view to immediately mirror when I changed

routing layer to add a via! Other people probably wouldn't, so this would

have to be an option that defaulted to "off".

 

I've been using eagle for ten years, always wanting this feature, but only

just realised there was a suggestions forum!

 

gEDA, Orcad, Altium Designer, and probably others support this so I can't

be alone in desiring this feature! (see

http://wiki.altium.com/display/ADOH/AltiumDesignerViewer-ViewingPCBDocuments#AltiumDesignerViewer-ViewingPCBDocuments-FlippingtheBoard

for example)

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    On 2/26/2011 10:41 AM, Jeff Gough wrote:

    When routing the back of a board, it would be really nice to be able to

    flip the view to see the back of the board as it really is.

     

    It would be extremely useful when debugging a board, as it's really painful

    to find a signal in eagle, then mentally flip it to find it on the physical

    board.

     

    It would also be useful for checking text layout on the back of the board.

    Mentally flipping text is a bit of a pain, and almost impossible when

    you're trying to evaluate its aesthetic appeal. Yes, I do consider

    aesthetics important in PCB design!

     

    I know I can print out the board mirrored, or group-then-mirror, and

    various other hacks, but if this button existed, I'd click it every minute

    or so when routing a complex design.

     

    In fact, I'd prefer the board view to immediately mirror when I changed

    routing layer to add a via! Other people probably wouldn't, so this would

    have to be an option that defaulted to "off".

     

    I've been using eagle for ten years, always wanting this feature, but only

    just realised there was a suggestions forum!

     

    gEDA, Orcad, Altium Designer, and probably others support this so I can't

    be alone in desiring this feature! (see

    http://wiki.altium.com/display/ADOH/AltiumDesignerViewer-ViewingPCBDocuments#AltiumDesignerViewer-ViewingPCBDocuments-FlippingtheBoard

    for example)

    the only thing I would add is that it should be very clear that you are

    in flipped view, not requiring checking coordinates direction, pushing

    buttons, issuing commands. this should go without saying, but just to be

    sure, I'm saying it!

     

    I have just finished a board that is circle shape and almost symmetrical

    layout, what a nightmare if I don't know which side I'm looking at, it's

    hard to keep it straight even without flipping.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kcadsoft
    kcadsoft over 15 years ago in reply to e14 Contributor

    On 02/28/11 22:29, Gary Gofstein wrote:

    ...

    the only thing I would add is that it should be very clear that you are

    in flipped view, not requiring checking coordinates direction, pushing

    buttons, issuing commands. this should go without saying, but just to be

    sure, I'm saying it!

     

    Do you have any particular idea on how this could be made "very clear"?

    I guess any small icon indicating this will be overlooked, and a thick

    "yellow/black" border around the draw window indicating "Caution - you're

    in flip mode!" will be overkill...

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to kcadsoft

    Am 01.03.2011 09:20, schrieb Klaus Schmidinger:

    Do you have any particular idea on how this could be made "very clear"?

     

    2D/3D CAD programs often display a small overlay at the lower left part

    of the window, showing a coordinate cross with all available axis

    directions.

     

    In a drill program of my own invention, I use the attached pictures

    (plus others) to indicate the current view:

      1. "top0" shows the view at the top layer with no rotation

      2. "bottom90" shows the view at the bottom layer with additional

         90 degrees rotation.

     

    And yes, since the display of any vector objects needs matrix

    manipulations, anyway, it would be an additional bonus if one could

    ROTATE the view. Therefore, I propose the following:

      3. Add BOTH mirror and rotation (in 90deg steps) to the VIEW.

      4. In case neither rotation nor mirroring is selected, do not

         display any additional overlay.

      5. In case the view matrix is not "identity", display the small

         overlay the following way:

      6. Mirrored view: Blue "B", non-mirrored view: Red "T",

         plus the current direction of both axis.

      7. Expand the WINDOW command to make use of the standard

         rotation/mirror syntax used for MOVE etc., so that "MR90"

         can be used.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to kcadsoft

    Am 01.03.2011 09:20, schrieb Klaus Schmidinger:

    Do you have any particular idea on how this could be made "very clear"?

     

    2D/3D CAD programs often display a small overlay at the lower left part

    of the window, showing a coordinate cross with all available axis

    directions.

     

    In a drill program of my own invention, I use the attached pictures

    (plus others) to indicate the current view:

      1. "top0" shows the view at the top layer with no rotation

      2. "bottom90" shows the view at the bottom layer with additional

         90 degrees rotation.

     

    And yes, since the display of any vector objects needs matrix

    manipulations, anyway, it would be an additional bonus if one could

    ROTATE the view. Therefore, I propose the following:

      3. Add BOTH mirror and rotation (in 90deg steps) to the VIEW.

      4. In case neither rotation nor mirroring is selected, do not

         display any additional overlay.

      5. In case the view matrix is not "identity", display the small

         overlay the following way:

      6. Mirrored view: Blue "B", non-mirrored view: Red "T",

         plus the current direction of both axis.

      7. Expand the WINDOW command to make use of the standard

         rotation/mirror syntax used for MOVE etc., so that "MR90"

         can be used.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    "Andreas Weidner" <andreas.weidner@aei.mpg.de> wrote in message

    news:ikijgh$773$1@cheetah.cadsoft.de...

    In a drill program of my own invention, I use the attached pictures

    (plus others) to indicate the current view:

    Andreas Weidner

     

    Indeed, this is the widest used solution, and I tend to agree with the idea

    of replacing the crosshair in the origin with something like in the attached

    image. Mirroring the board will change the X arrow to the other direction.

    --

    Silviu Epure

    "Dunarea de Jos" University of Galati, Romania

    http://www.etc.ugal.ro/sepure

     

     

    begin 666 origin.jpg

    M_]C_X `02D9)1@`!`0```0`!``#_VP!#`!(,#A ."Q(0#Q 4$Q(5&RT=&QD9

    M&S<H*B$M0CI%1$ Z/SY(46A82$UB3CX_6GM<8FMO='9T1E> B7]QB&AR='#_

    MVP!#`1,4%!L8&S4='35P2S]+<'!P<'!P<'!P<'!P<'!P<'!P<'!P<'!P<'!P

    M<'!P<'!P<'!P<'!P<'!P<'!P<'!P<'#_P `1" $U`4X#`2(``A$!`Q$!_\0`

    M&P`!`0`"`P$```````````````4#!@$"! ?_Q `Z$ $``0,!! 8(! 8"`P``

    M`````0(#$00%$B$Q,T%A<I'1!A,5(C)14G%3@;'!%$)SLN'PH?$V8H+_Q `:

    M`0$``P$!`0```````````````0(#! 4&_\0`*!$!``(!`P,#! ,!````````

    M``$"$0,$,10A,A(S82)!8J$345)Q_]H`# ,!``(1`Q$`/P#1@ ``````)C',

    M`````````````````````````````````````````"0GL ``````````````

    M````````````````````````<Q$S,1$9F>40X&3I?ZG]W?U_.%HC/:.6.8

    MQS<XG&<</FYHIWLS,XICG)75O8B(Q3'*`QVS+J E4 ``````````````````

    M`<XG=BK$XF<1+@````````````````!EU%4S73$SPW:9_.8C,L3O=JBNJ)CZ

    M8CPB(=$1POJ3F\R )4 `````````````````````````````````````)C',

    M9+MFNU%$U1PJC,>7W8Q,Q,3B0 0`````````````````````````````````

    M```,VEMLNQF/=IXRPJ6EMKM1F/>JXRI>V(=.UTOY-3OQ#/>L?Q&@KBFGW[

    M<[U/;\X_WL1FSZ28]7,1B)CY0A;1T\Z?551CW:N-*NG/;#7>4^KUP\H#5P@`

    M``````````````````````````````````,NGIIJNQOS$4QQG,\UFJXS3,

    M51V<4A1V;T-7WG]F6K7[O0V6KB?1A[M-7%%R)GA$QB9ETVK_``]_33,7K7K+
    M?&(WHSVPZS\$)%[IJ^]*NGWEMO)]-<_VZ -WD@``````````````````````
    M`````````````"CLWHJN]Y)RALWHI[W[,]3Q=>S]UZI^!(O=-7WI5_Y/S2+W

    M35]Z5-ET[_QAT ;O ```````````````````````````````````%#9O13

    MWOV3U#9O13WOV9ZGBZ]G[KU8]R4B]TU?>E8GX9Z/>Z:OO2II<NG?,.@#=Y

    M8 ```````````````````````````````````H;.Z*>]Y)ZAL[HI[WDSU/%U

    M[W7J^I(O=-7WI5_J2W35]Z5-ET[_QAT ;O `````````````````````

    M``````````````%#9W13WO)/4-G=#5V5>3/4\77LO=>N8^)'O=-7WI6)GAGY

    MH][IJ^]*FERZ=_XPZ -WE@```````````````````````````````````"CL

    MWHJN]Y)RCLWHI[W[,]3Q=>S]UZ9^"$B]TU?>E7GX$B]TU?>E32Y=._\`&/\`

    MKH W>6 ```````````````````````````````````*&S>BGO?LGJ&S>BGO?

    MLSU/%U[/W7J_D_-(O=-7WI5_Y9Z1>Z:OO2II<NG?,.@#=Y8 ``````````

    M```````````````````````YHIJKKBBBF:JJIQ$1&9F2BFJNN***9JJJG$1$

    M9F9?0M@[&M;L9JQ7J:X]^Y\NR.S]?TY]QNZ-<SRF(RA;-]$KUS%>T+GJ:?

    MPZ)B:NOKY1U?/\FP:38>SM+%.Y8WICKKJFK,XQF8Y?\`"D/%U-SJZG,M:_3P

    M\EW9NBNT[M6FMQ&<^[&[/_"/M#T2TU[?N:2[79N3.8IJG>HY<OG''KX_9L8I

    M37U*3FLIM:;1B9?,MH[.U6SKT6]5;W<YW:HG,51V3_LO(^J:FQ:U5BNS?HBN

    MW7&*J9?.]N;,KV7KJK7O39JXVJZOYH\XY?\`;V-KNXUOIMVEE,83P':J````

    M````````````````````````````V7T*T,7=9=UE<3BQ&[1PX35//CV1U=K<

    MT;T1M4V]@6:J8Q-RJJJKCSG,Q^D0LOGMW>;ZT_'9I' #%J+]&GM[]S.,XB(C

    MFYXC/:%XB;3B&4>+2[1HOW=RJGU<S\/'.7M3:LUG$K7T[:<XM F^D.AC7;(O

    M48F;EN/66\1F=Z(Y8[8S'YJ04M-+1:/LS?)QL6IV'I:=5=IHF[33%<Q$15'"

    M,_9C]BZ?Z[OC'D^@C<TF'#.ZTXG""WL33_7=\8\CVI_P`2[XQY)ZBAU6F@

    MB][%T_XEWQCR<>Q=/]=WQCR1U%$=7IH0O>Q=/]=WQCR/8NG^N[XQY'44.KTT

    M$7O8NG^N[XQY'L73_7=\8\CJ*)ZO301>]BZ?Z[OC'D>Q=/\`B7?&/)/44.JT

    MT%ZM%HJM93<WXIJHQB)Y3G_`5/8NG_`!+OC'D]NS=!;TOK/5U53O8SO8GY

    MJVUXF,5Y4ON:S&<M8OV+NGJW;M$TSU9Y3^;&W6YIJZ)IKBFJF><51P1]9L

    M.F<U::K=[)G,>/\`VFNO_I:FYCB\80AEOZ>[IZMV];FB>K/*?S8F\3$]X=,3

    M$QF',1,S$1&9GE$.!DZ7^I_=_G]?OS$SAC<XG&<</F[44QC>JX4QXSV0XKJF

    MJ<SPB.$1'* RZ@)2``````````A>BG_`(]I?_O^59JWH/JZ)LZC1SPKBKU

    ML=L<(GPQ'BVE\YN:S75M$_VUC@>7:5BN_IXIMQ$U15$XR]0QK/IG,TO-1:

    M/LBZ'17JK]%=5,T4T59S5&,X[%MP7O-YS*^MK6U9SD</+M/51H=G7]3,Q$

    MVZ)FG,3,35RB.';A6M9M.(8HNKJC^+O?U*OU8=Z&HCW(VF(Y>9.SS.?4V[>@

    MWH:B)Z7Y1T7Y?IMV\YWNUJ =\G1?E^FW[W:;T?-J =\G1?E^FWS5'S<;T-

    M1#I?DZ+\OTV[>@WH:B'2_)T7Y?IMV]#M17,9Q./LT]0V7J:--1>FNJ(SNX[>

    M:MMM-8S$JWVDUC,3E?JN8XS/BQ7-H6[%N)JN1$=4<YE#U.TKEW,4>[3\YYO%

    M,S5.9F9GYRM3;SS:4Z>TGFTJFMVS7?IFBW;HBB><UTQ5,_ER2NK .JM8K&(=

    MU12,01P=Z8QO5<8\9[(=8QF,\8Z\.:ZIJG,\(CA$1RA9R[U3Z^?_`'ZH

    M?\`G]?OSQ=6!WKJBNF)G._F=Z?G\I_,Q@B,.D<`$I)XG5@`(X``3Q.K ``

    M```SZ57=%J[>ILS$7<YC,9B>J8\'TG0:VQM#2TZC3U;U%7..NF?E/:^7O9

    MLS:>IV9?F[IJH]Z,545<::OO#CW6V_FC,<PM$X?3!'V=Z1Z#64>_=C37(C,T

    MW9B(ZN4\IY_?L6.;Q+Z=J3BT87 >76;1T>BB9U.HMVYB,[N<U3&<<(CC*L5F

    MTX@>IHWI7M>G77Z=IZXJT]J<S5$?%7QXQ/RCSY\#;?I=UU%>GTM,V=/5&)

    MF?CJ<3QX1_O7A >OM-I-)]=5)D`>DJ````````````````````````````

    M``````,MC4ZC3Y]1?NVM[GN5S3GP8A$Q$]I'HNZ[67[<V[VKOW*)YTUW)F)_

    M)YP(B(X`!( `````````````````````````````````````````````````

    M````````````````````````````````````````````````````````````

    %````_]D`

    `

    end