Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) "Flip View" button
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 190 subscribers
  • Views 6464 views
  • Users 0 members are here
Related

"Flip View" button

e14 Contributor
e14 Contributor over 15 years ago

When routing the back of a board, it would be really nice to be able to

flip the view to see the back of the board as it really is.

 

It would be extremely useful when debugging a board, as it's really painful

to find a signal in eagle, then mentally flip it to find it on the physical

board.

 

It would also be useful for checking text layout on the back of the board.

Mentally flipping text is a bit of a pain, and almost impossible when

you're trying to evaluate its aesthetic appeal. Yes, I do consider

aesthetics important in PCB design!

 

I know I can print out the board mirrored, or group-then-mirror, and

various other hacks, but if this button existed, I'd click it every minute

or so when routing a complex design.

 

In fact, I'd prefer the board view to immediately mirror when I changed

routing layer to add a via! Other people probably wouldn't, so this would

have to be an option that defaulted to "off".

 

I've been using eagle for ten years, always wanting this feature, but only

just realised there was a suggestions forum!

 

gEDA, Orcad, Altium Designer, and probably others support this so I can't

be alone in desiring this feature! (see

http://wiki.altium.com/display/ADOH/AltiumDesignerViewer-ViewingPCBDocuments#AltiumDesignerViewer-ViewingPCBDocuments-FlippingtheBoard

for example)

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to kcadsoft

     

    "Klaus Schmidinger" <Klaus.Schmidinger@cadsoft.de> wrote in message

    news:ikia8r$nj4$1@cheetah.cadsoft.de...

    On 02/28/11 22:29, Gary Gofstein wrote:

    Do you have any particular idea on how this could be made "very clear"?

    I guess any small icon indicating this will be overlooked, and a thick

    "yellow/black" border around the draw window indicating "Caution - you're

    in flip mode!" will be overkill...

     

     

     

     

    What about if you colorize with yellow (for example) the background EXCEPT

    the board? (using min/max values for X,Y - we can access them right now from

    ulps).

     

    This way colors on the board remain as user set them, and it's highly

    visible that something it's not in "default mode".

     

    --

    Silviu Epure

    "Dunarea de Jos" University of Galati, Romania

    http://www.etc.ugal.ro/sepure

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    "Morten Leikvoll" <mleikvol@yahoo.nospam> wrote in message

    news:ikic6j$1p3$1@cheetah.cadsoft.de...

    "Klaus Schmidinger" <Klaus.Schmidinger@cadsoft.de> wrote in message

    news:ikia8r$nj4$1@cheetah.cadsoft.de...

    >> On 02/28/11 22:29, Gary Gofstein wrote:

    >>> ...

    >>> the only thing I would add is that it should be very clear that you are

    >>> in flipped view, not requiring checking coordinates direction, pushing

    >>> buttons, issuing commands. this should go without saying, but just to be

    >>> sure, I'm saying it!

    >>

    >> Do you have any particular idea on how this could be made "very clear"?

    >> I guess any small icon indicating this will be overlooked, and a thick

    >> "yellow/black" border around the draw window indicating "Caution - you're

    >> in flip mode!" will be overkill...

     

    Does it really matter if it's clear or not? People may want to draw the

    board from bottom instead from top and should be allowed to. Using the

    names "top" and "bottom" on the layers is maybe more confusing than just

    using 1 and 16. Even using the number 16 for bottom layer is a bit

    confusing for <16 layer boards.

     

    But here is a suggestion. Show an icon with a tilted square, where layer 1

    has the text "1" on it, and an arrow pointing in the view direction. It

    could be placed anywhere really, but maybe the toolbar is a natural place.

    Clicking it could toggle the view. The function and icon could also be

    placed in the view menu.

     

    For the ones that gets confused, I suggest also adding "top"/"bottom" in

    clear text at top/bottom layers, so that it gets mirrored in rear view.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to kcadsoft

    Klaus Schmidinger schrieb:

     

    On 02/28/11 22:29, Gary Gofstein wrote:

    >> ...

    >> the only thing I would add is that it should be very clear that you are

    >> in flipped view, not requiring checking coordinates direction, pushing

    >> buttons, issuing commands. this should go without saying, but just to be

    >> sure, I'm saying it!

     

    Do you have any particular idea on how this could be made "very clear"?

    I guess any small icon indicating this will be overlooked, and a thick

    "yellow/black" border around the draw window indicating "Caution - you're

    in flip mode!" will be overkill...

     

    Do you know NoScript (for FF/SM)? It displays a pale yellow bar with

    warnings/information at the lower screen border (directly above the

    status bar) if there are disabled scripts in the currently viewed web page.

     

    I think this method could be a good solution to this problem. It is

    clearly visible, but not overkill. Eventually it can be acknowledged and

    then disappear (to regain that screen area for the design).

     

    While we're at it, I think that presenting such a warning (maybe in the

    same style) also makes sense if annotation is inactive for whatever reason.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to kcadsoft

    "Klaus Schmidinger" <Klaus.Schmidinger@cadsoft.de> wrote in message

    news:ikia8r$nj4$1@cheetah.cadsoft.de...

    On 02/28/11 22:29, Gary Gofstein wrote:

    >> ...

    >> the only thing I would add is that it should be very clear that you are

    >> in flipped view, not requiring checking coordinates direction, pushing

    >> buttons, issuing commands. this should go without saying, but just to be

    >> sure, I'm saying it!

     

    Do you have any particular idea on how this could be made "very clear"?

    I guess any small icon indicating this will be overlooked, and a thick

    "yellow/black" border around the draw window indicating "Caution - you're

    in flip mode!" will be overkill...

     

    Does it really matter if it's clear or not? People may want to draw the

    board from bottom instead from top and should be allowed to. Using the names

    "top" and "bottom" on the layers is maybe more confusing than just using 1

    and 16. Even using the number 16 for bottom layer is a bit confusing for <16

    layer boards.

     

    But here is a suggestion. Show an icon with a tilted square, where layer 1

    has the text "1" on it, and an arrow pointing in the view direction. It

    could be placed anywhere really, but maybe the toolbar is a natural place.

    Clicking it could toggle the view. The function and icon could also be

    placed in the view menu.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kcadsoft
    kcadsoft over 15 years ago in reply to e14 Contributor

    On 02/28/11 22:29, Gary Gofstein wrote:

    ...

    the only thing I would add is that it should be very clear that you are

    in flipped view, not requiring checking coordinates direction, pushing

    buttons, issuing commands. this should go without saying, but just to be

    sure, I'm saying it!

     

    Do you have any particular idea on how this could be made "very clear"?

    I guess any small icon indicating this will be overlooked, and a thick

    "yellow/black" border around the draw window indicating "Caution - you're

    in flip mode!" will be overkill...

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    On 2/26/2011 10:41 AM, Jeff Gough wrote:

    When routing the back of a board, it would be really nice to be able to

    flip the view to see the back of the board as it really is.

     

    It would be extremely useful when debugging a board, as it's really painful

    to find a signal in eagle, then mentally flip it to find it on the physical

    board.

     

    It would also be useful for checking text layout on the back of the board.

    Mentally flipping text is a bit of a pain, and almost impossible when

    you're trying to evaluate its aesthetic appeal. Yes, I do consider

    aesthetics important in PCB design!

     

    I know I can print out the board mirrored, or group-then-mirror, and

    various other hacks, but if this button existed, I'd click it every minute

    or so when routing a complex design.

     

    In fact, I'd prefer the board view to immediately mirror when I changed

    routing layer to add a via! Other people probably wouldn't, so this would

    have to be an option that defaulted to "off".

     

    I've been using eagle for ten years, always wanting this feature, but only

    just realised there was a suggestions forum!

     

    gEDA, Orcad, Altium Designer, and probably others support this so I can't

    be alone in desiring this feature! (see

    http://wiki.altium.com/display/ADOH/AltiumDesignerViewer-ViewingPCBDocuments#AltiumDesignerViewer-ViewingPCBDocuments-FlippingtheBoard

    for example)

    the only thing I would add is that it should be very clear that you are

    in flipped view, not requiring checking coordinates direction, pushing

    buttons, issuing commands. this should go without saying, but just to be

    sure, I'm saying it!

     

    I have just finished a board that is circle shape and almost symmetrical

    layout, what a nightmare if I don't know which side I'm looking at, it's

    hard to keep it straight even without flipping.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    user wrote on Sun, 27 February 2011 11:18

    Being able to add new functionality (very flexible) by ULPs is

    *really

    great*, but trying to get a simple view from the bottom side by

    mirroring the complete board is really evil.

     

    Full ACK!

     

    I acknoledge Tilmann's post too, but in additional I also agree with him.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 27.02.2011 16:43, Tilmann Reh wrote:

     

    Being able to add new functionality (very flexible) by ULPs is *really

    great*, but trying to get a simple view from the bottom side by

    mirroring the complete board is really evil.

     

    Tilmann

     

    Full ACK!

     

    Markus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Silviu Epure schrieb:

     

    >> On 26.02.2011 21:10, Warren Brayshaw wrote:

    >> That's what I sometimes hate. For even the most basic things there are

    >> evil hacks using an ULP instead of having this implemented proper in the

    >> EAGLE application itself.

     

    If the most usefull ulps would be included by default in a submenu of the

    Eagle, I bet you wouldn't think this way, but "Eagle is a great software,

    that let you adjust it's own subrutines".

     

    Please don't compare apples with oranges.

     

    Being able to add new functionality (very flexible) by ULPs is *really

    great*, but trying to get a simple view from the bottom side by

    mirroring the complete board is really evil.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Jeff Gough wrote:

     

    >When routing the back of a board, it would be really nice to be able to

    >flip the view to see the back of the board as it really is.

    >It would be extremely useful when debugging a board, as it's really painful

     

    exactly, and there are more situations, e.g. wiring an ICT adapter.

     

    Oliver

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>