Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) "Flip View" button
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 190 subscribers
  • Views 6440 views
  • Users 0 members are here
Related

"Flip View" button

e14 Contributor
e14 Contributor over 15 years ago

When routing the back of a board, it would be really nice to be able to

flip the view to see the back of the board as it really is.

 

It would be extremely useful when debugging a board, as it's really painful

to find a signal in eagle, then mentally flip it to find it on the physical

board.

 

It would also be useful for checking text layout on the back of the board.

Mentally flipping text is a bit of a pain, and almost impossible when

you're trying to evaluate its aesthetic appeal. Yes, I do consider

aesthetics important in PCB design!

 

I know I can print out the board mirrored, or group-then-mirror, and

various other hacks, but if this button existed, I'd click it every minute

or so when routing a complex design.

 

In fact, I'd prefer the board view to immediately mirror when I changed

routing layer to add a via! Other people probably wouldn't, so this would

have to be an option that defaulted to "off".

 

I've been using eagle for ten years, always wanting this feature, but only

just realised there was a suggestions forum!

 

gEDA, Orcad, Altium Designer, and probably others support this so I can't

be alone in desiring this feature! (see

http://wiki.altium.com/display/ADOH/AltiumDesignerViewer-ViewingPCBDocuments#AltiumDesignerViewer-ViewingPCBDocuments-FlippingtheBoard

for example)

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    "Andreas Weidner" <andreas.weidner@aei.mpg.de> wrote in message

    news:ikijgh$773$1@cheetah.cadsoft.de...

    In a drill program of my own invention, I use the attached pictures

    (plus others) to indicate the current view:

    Andreas Weidner

     

    Indeed, this is the widest used solution, and I tend to agree with the idea

    of replacing the crosshair in the origin with something like in the attached

    image. Mirroring the board will change the X arrow to the other direction.

    --

    Silviu Epure

    "Dunarea de Jos" University of Galati, Romania

    http://www.etc.ugal.ro/sepure

     

     

    begin 666 origin.jpg

    M_]C_X `02D9)1@`!`0```0`!``#_VP!#`!(,#A ."Q(0#Q 4$Q(5&RT=&QD9

    M&S<H*B$M0CI%1$ Z/SY(46A82$UB3CX_6GM<8FMO='9T1E> B7]QB&AR='#_

    MVP!#`1,4%!L8&S4='35P2S]+<'!P<'!P<'!P<'!P<'!P<'!P<'!P<'!P<'!P

    M<'!P<'!P<'!P<'!P<'!P<'!P<'!P<'#_P `1" $U`4X#`2(``A$!`Q$!_\0`

    M&P`!`0`"`P$```````````````4#!@$"! ?_Q `Z$ $``0,!! 8(! 8"`P``

    M`````0(#$00%$B$Q,T%A<I'1!A,5(C)14G%3@;'!%$)SLN'PH?$V8H+_Q `:

    M`0$``P$!`0```````````````0(#! 4&_\0`*!$!``(!`P,#! ,!````````

    M``$"$0,$,10A,A(S82)!8J$345)Q_]H`# ,!``(1`Q$`/P#1@ ``````)C',

    M`````````````````````````````````````````"0GL ``````````````

    M````````````````````````<Q$S,1$9F>40X&3I?ZG]W?U_.%HC/:.6.8

    MQS<XG&<</FYHIWLS,XICG)75O8B(Q3'*`QVS+J E4 ``````````````````

    M`<XG=BK$XF<1+@````````````````!EU%4S73$SPW:9_.8C,L3O=JBNJ)CZ

    M8CPB(=$1POJ3F\R )4 `````````````````````````````````````)C',

    M9+MFNU%$U1PJC,>7W8Q,Q,3B0 0`````````````````````````````````

    M```,VEMLNQF/=IXRPJ6EMKM1F/>JXRI>V(=.UTOY-3OQ#/>L?Q&@KBFGW[

    M<[U/;\X_WL1FSZ28]7,1B)CY0A;1T\Z?551CW:N-*NG/;#7>4^KUP\H#5P@`

    M``````````````````````````````````,NGIIJNQOS$4QQG,\UFJXS3,

    M51V<4A1V;T-7WG]F6K7[O0V6KB?1A[M-7%%R)GA$QB9ETVK_``]_33,7K7K+
    M?&(WHSVPZS\$)%[IJ^]*NGWEMO)]-<_VZ -WD@``````````````````````
    M`````````````"CLWHJN]Y)RALWHI[W[,]3Q=>S]UZI^!(O=-7WI5_Y/S2+W

    M35]Z5-ET[_QAT ;O ```````````````````````````````````%#9O13

    MWOV3U#9O13WOV9ZGBZ]G[KU8]R4B]TU?>E8GX9Z/>Z:OO2II<NG?,.@#=Y

    M8 ```````````````````````````````````H;.Z*>]Y)ZAL[HI[WDSU/%U

    M[W7J^I(O=-7WI5_J2W35]Z5-ET[_QAT ;O `````````````````````

    M``````````````%#9W13WO)/4-G=#5V5>3/4\77LO=>N8^)'O=-7WI6)GAGY

    MH][IJ^]*FERZ=_XPZ -WE@```````````````````````````````````"CL

    MWHJN]Y)RCLWHI[W[,]3Q=>S]UZ9^"$B]TU?>E7GX$B]TU?>E32Y=._\`&/\`

    MKH W>6 ```````````````````````````````````*&S>BGO?LGJ&S>BGO?

    MLSU/%U[/W7J_D_-(O=-7WI5_Y9Z1>Z:OO2II<NG?,.@#=Y8 ``````````

    M```````````````````````YHIJKKBBBF:JJIQ$1&9F2BFJNN***9JJJG$1$

    M9F9?0M@[&M;L9JQ7J:X]^Y\NR.S]?TY]QNZ-<SRF(RA;-]$KUS%>T+GJ:?

    MPZ)B:NOKY1U?/\FP:38>SM+%.Y8WICKKJFK,XQF8Y?\`"D/%U-SJZG,M:_3P

    M\EW9NBNT[M6FMQ&<^[&[/_"/M#T2TU[?N:2[79N3.8IJG>HY<OG''KX_9L8I

    M37U*3FLIM:;1B9?,MH[.U6SKT6]5;W<YW:HG,51V3_LO(^J:FQ:U5BNS?HBN

    MW7&*J9?.]N;,KV7KJK7O39JXVJZOYH\XY?\`;V-KNXUOIMVEE,83P':J````

    M````````````````````````````V7T*T,7=9=UE<3BQ&[1PX35//CV1U=K<

    MT;T1M4V]@6:J8Q-RJJJKCSG,Q^D0LOGMW>;ZT_'9I' #%J+]&GM[]S.,XB(C

    MFYXC/:%XB;3B&4>+2[1HOW=RJGU<S\/'.7M3:LUG$K7T[:<XM F^D.AC7;(O

    M48F;EN/66\1F=Z(Y8[8S'YJ04M-+1:/LS?)QL6IV'I:=5=IHF[33%<Q$15'"

    M,_9C]BZ?Z[OC'D^@C<TF'#.ZTXG""WL33_7=\8\CVI_P`2[XQY)ZBAU6F@

    MB][%T_XEWQCR<>Q=/]=WQCR1U%$=7IH0O>Q=/]=WQCR/8NG^N[XQY'44.KTT

    M$7O8NG^N[XQY'L73_7=\8\CJ*)ZO301>]BZ?Z[OC'D>Q=/\`B7?&/)/44.JT

    MT%ZM%HJM93<WXIJHQB)Y3G_`5/8NG_`!+OC'D]NS=!;TOK/5U53O8SO8GY

    MJVUXF,5Y4ON:S&<M8OV+NGJW;M$TSU9Y3^;&W6YIJZ)IKBFJF><51P1]9L

    M.F<U::K=[)G,>/\`VFNO_I:FYCB\80AEOZ>[IZMV];FB>K/*?S8F\3$]X=,3

    M$QF',1,S$1&9GE$.!DZ7^I_=_G]?OS$SAC<XG&<</F[44QC>JX4QXSV0XKJF

    MJ<SPB.$1'* RZ@)2``````````A>BG_`(]I?_O^59JWH/JZ)LZC1SPKBKU

    ML=L<(GPQ'BVE\YN:S75M$_VUC@>7:5BN_IXIMQ$U15$XR]0QK/IG,TO-1:

    M/LBZ'17JK]%=5,T4T59S5&,X[%MP7O-YS*^MK6U9SD</+M/51H=G7]3,Q$

    MVZ)FG,3,35RB.';A6M9M.(8HNKJC^+O?U*OU8=Z&HCW(VF(Y>9.SS.?4V[>@

    MWH:B)Z7Y1T7Y?IMV\YWNUJ =\G1?E^FW[W:;T?-J =\G1?E^FWS5'S<;T-

    M1#I?DZ+\OTV[>@WH:B'2_)T7Y?IMV]#M17,9Q./LT]0V7J:--1>FNJ(SNX[>

    M:MMM-8S$JWVDUC,3E?JN8XS/BQ7-H6[%N)JN1$=4<YE#U.TKEW,4>[3\YYO%

    M,S5.9F9GYRM3;SS:4Z>TGFTJFMVS7?IFBW;HBB><UTQ5,_ER2NK .JM8K&(=

    MU12,01P=Z8QO5<8\9[(=8QF,\8Z\.:ZIJG,\(CA$1RA9R[U3Z^?_`'ZH

    M?\`G]?OSQ=6!WKJBNF)G._F=Z?G\I_,Q@B,.D<`$I)XG5@`(X``3Q.K ``

    M```SZ57=%J[>ILS$7<YC,9B>J8\'TG0:VQM#2TZC3U;U%7..NF?E/:^7O9

    MLS:>IV9?F[IJH]Z,545<::OO#CW6V_FC,<PM$X?3!'V=Z1Z#64>_=C37(C,T

    MW9B(ZN4\IY_?L6.;Q+Z=J3BT87 >76;1T>BB9U.HMVYB,[N<U3&<<(CC*L5F

    MTX@>IHWI7M>G77Z=IZXJT]J<S5$?%7QXQ/RCSY\#;?I=UU%>GTM,V=/5&)

    MF?CJ<3QX1_O7A >OM-I-)]=5)D`>DJ````````````````````````````

    M``````,MC4ZC3Y]1?NVM[GN5S3GP8A$Q$]I'HNZ[67[<V[VKOW*)YTUW)F)_

    M)YP(B(X`!( `````````````````````````````````````````````````

    M````````````````````````````````````````````````````````````

    %````_]D`

    `

    end

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to kcadsoft

    On 3/1/11 3:20 AM, Klaus Schmidinger wrote:

    Do you have any particular idea on how this could be made "very clear"?

    I guess any small icon indicating this will be overlooked, and a thick

    "yellow/black" border around the draw window indicating "Caution - you're

    in flip mode!" will be overkill...

     

    Klaus Schmidinger

     

    Klaus,

     

    First, please let me add my enthusiastic support for this idea.

     

    Second, here is my suggestion for what to do when you display the mirror

    image of the board:

     

    Nothing.

     

    I know my board designs. I know when I am looking at the front and when

    I am looking the back. A good tool stays out of the designer's way.

     

    Andrew Sterian

    Senior Designer

    Emsyde Design LLC

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

     

    "James Morrison" <james@eaglecentral.ca> wrote in message

    news:ikjj4p$llv$1@cheetah.cadsoft.de...

    Olin, I'm not sure this is such a bad idea.  Now maybe not yellow

    background (maybe dark grey), but it would be good to have some sort of

    visual clue as to what orientation you are currently looking at.  And I

    rarely have text visible during intense routing sessions, so just looking

    at text isn't enough for me.

     

    What's wrong with making your own indicator? Put the text "TOP" on your top

    copper layer where you got some space free.

    I agree with Olin that anything else than a normal view would be annoying.

    Maybe a middle way using an alternative palette in rear view would work for

    you?

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Olin wrote on Tue, 01 March 2011 14:23

    Silviu Epure wrote on Tue, 01 March 2011 04:28

    What about if you colorize with yellow (for example) the background

    EXCEPT the board?

     

    Yucc.  Please, no!  That would be very annoying.

     

     

    Olin, I'm not sure this is such a bad idea.  Now maybe not yellow

    background (maybe dark grey), but it would be good to have some sort of

    visual clue as to what orientation you are currently looking at.  And I

    rarely have text visible during intense routing sessions, so just looking

    at text isn't enough for me.

     

    I've used Altium which have this as a nice feature and it can be a bit

    disorienting.  So having some way to give yourself a mental framework would

    be helpful I think.

     

    Quote:

    Boards have two sides, sometimes with components on each.  It isn't any

    more right or wrong to view the board from the top than the bottom when

    you're doing placement and routing.  That's just a convenience choice

    that should be changeable easily without penalty.  I plan on setting up a

    hot key for it.  It would really piss me off if each time I toggle to

    bottom view I have to dismiss some warning or put up with a obnoxious

    background.

     

     

    A normal background and flipped background colour would serve both of us.

    I could set the flipped background to grey and you could set it to black.

    Viola, we both get what we want image

     

    Quote:

    Cadsoft: This brings up one point though.  A natural way to use this

    new command is to set up a hot key to toggle the top/bottom view state.

    Every time you hit the button it switches to the other orientation.  That

    means it would be useful for the native command to toggle the state, not

    just explicitly set it to top or bottom view mode.  Otherwise I'd have to

    write a ULP that gets the current state, flips it, writes a script with

    the new state, then runs the script.  That's doable, but I can't imagine

    it would be much trouble to allow the command toggle the state natively

    if this is considered from the start.

     

     

    Good point Olin.  All commands should be like that, including turning

    layers on and off.  I have ULP to do just that but the layer command should

    toggle directly.

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Does it really matter if it's clear or not? People may want to draw the

     

    board from bottom instead from top and should be allowed to.

     

    Agreed! Let's just get it implemented as cleanly, minimally and, above all,

    as quickly as possible!

     

    When it's released and 90% of Eagle's user base is breathing a collective

    sigh of relief, the other 10% can submit new suggestions of ways to

    "improve" the appearance, behaviour and "user friendliness" of our simple,

    humble Flip Board button.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Silviu Epure wrote on Tue, 01 March 2011 04:28

    What about if you colorize with yellow (for example) the background

    EXCEPT the board?

     

    Yucc.  Please, no!  That would be very annoying.

     

    Boards have two sides, sometimes with components on each.  It isn't any

    more right or wrong to view the board from the top than the bottom when

    you're doing placement and routing.  That's just a convenience choice that

    should be changeable easily without penalty.  I plan on setting up a hot

    key for it.  It would really piss me off if each time I toggle to bottom

    view I have to dismiss some warning or put up with a obnoxious background.

     

    Cadsoft: This brings up one point though.  A natural way to use this new

    command is to set up a hot key to toggle the top/bottom view state.  Every

    time you hit the button it switches to the other orientation.  That means

    it would be useful for the native command to toggle the state, not just

    explicitly set it to top or bottom view mode.  Otherwise I'd have to write

    a ULP that gets the current state, flips it, writes a script with the new

    state, then runs the script.  That's doable, but I can't imagine it would

    be much trouble to allow the command toggle the state natively if this is

    considered from the start.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to kcadsoft

    Klaus Schmidinger wrote on Tue, 01 March 2011 03:20

    Do you have any particular idea on how this could be made "very clear"?

    I guess any small icon indicating this will be overlooked, and a thick

    "yellow/black" border around the draw window indicating "Caution - you're

    in flip mode!" will be overkill...

     

    Yes, and annoying.

     

    Whatever you do, make sure it can be easily disabled.  I don't want yet

    another indicator cluttering up my screen or using up more precious

    pixels.

     

    While I think being able to flip the view (mirror left/right) would be

    quite useful (I'm looking forward to making a hot key for that command), I

    really don't see a problem with it causing confusion.  If there is any

    text, it will be immediately obvious.  Even if not, when you're working on

    a board you'll know it well enough to easily recognize whether you're

    looking from the top or the bottom.  There is no problem to solve unless

    you create one by adding nanny-ware.  Sometimes doing less is more.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Aargh!

     

    I'm currently populating and testing a board, looking at my eagle layout.

     

    I've just spent half an hour debugging my power supply.

     

    I've soldered a capacitor across the wrong two pads because I was looking

    at the bottom side and failed to mirror it in my brain!

     

    And before someone tells me to print out my layout before assembling it:

     

    1) many of the boards I make are too dense for unambiguous silkscreen

    labels

    2) It's 2011. I don't own a printer.

    3) Paper is not CAD. I can't say "show c1 c6 c39" to see all of the places

    where I should be mounting a 100nF cap.

     

    So I can add another reason to my original post - useful for assembling

    boards.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

     

    "Morten Leikvoll" <mleikvol@yahoo.nospam> wrote in message

    news:ikie63$bvo$1@cheetah.cadsoft.de...

    "Morten Leikvoll" <mleikvol@yahoo.nospam> wrote in message

    news:ikic6j$1p3$1@cheetah.cadsoft.de...

    >> "Klaus Schmidinger"  also be placed in the view menu.

     

    For the ones that gets confused, I suggest also adding "top"/"bottom" in

    clear text at top/bottom layers, so that it gets mirrored in rear view.

     

    I see this could be mis-interpreted. I meant the USER should do this. Not

    Cadsoft.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to kcadsoft

    Am 01.03.2011 09:20, schrieb Klaus Schmidinger:

    Do you have any particular idea on how this could be made "very clear"?

     

    2D/3D CAD programs often display a small overlay at the lower left part

    of the window, showing a coordinate cross with all available axis

    directions.

     

    In a drill program of my own invention, I use the attached pictures

    (plus others) to indicate the current view:

      1. "top0" shows the view at the top layer with no rotation

      2. "bottom90" shows the view at the bottom layer with additional

         90 degrees rotation.

     

    And yes, since the display of any vector objects needs matrix

    manipulations, anyway, it would be an additional bonus if one could

    ROTATE the view. Therefore, I propose the following:

      3. Add BOTH mirror and rotation (in 90deg steps) to the VIEW.

      4. In case neither rotation nor mirroring is selected, do not

         display any additional overlay.

      5. In case the view matrix is not "identity", display the small

         overlay the following way:

      6. Mirrored view: Blue "B", non-mirrored view: Red "T",

         plus the current direction of both axis.

      7. Expand the WINDOW command to make use of the standard

         rotation/mirror syntax used for MOVE etc., so that "MR90"

         can be used.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>