EAGLE User Support (English) Lost Consistency
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
  • Replies 8 replies
  • Subscribers 178 subscribers
  • Views 2027 views
  • Users 0 members are here
Related

Lost Consistency

Former Member
Former Member over 14 years ago

Hi,

 

I wonder if any one provide assistance.  I have lost consistency on my

board.  I have tried various methods to fix but without success.  I have run

ERC and identified say this error below:

 

"Different connections in IC2B pin OE and pad 4 (GND/ none)"

I interpret this to mean there is a net connection on GND but NOT on pin OE.

However there is deffinately a net connection in my schematic as I can move

the GND symbol or my device (74HCT125D) symbol and see that the net is

connected to both device and ground.

I have also tried deleting devices and nets and added new devices from

library, with no success.  I have also deleted nets and renamed there

another name and still no success.

 

How can I fix this ?

 

Many thanks,

Jim

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 14 years ago

    Hi Jorge,

     

    Thanks for getting back to me.

     

    Regarding your feedback, I understand your guidance. However, can I provide

    another example of my Lost Consistency problem, to aid more understanding.

    I have a 4 pin single inline connector directly connected to a 64 pin

    backplane connector, (I only tell you this so that you understand it is a

    simple direct connection).

    Again no matter if I delete all 4 nets and then add new nets, no matter if I

    delete 4 pin connector, from schematic and PCB and then add new connector, I

    get the Consistancy error "Different connections on SV10 pin 1 and pad 1

    (10RX1+ / none"

    SV10 = 4 pin connector

    10RX1+ = net name on pin 1

     

    For this connector and with the remaining 3 pins of the connector, I get the

    same error. This error type is the same or similar for a further 79 error

    instances in my design.

    My PCB has been tracked a great deal so deleting all tracks as you

    previously suggested is not a good option for me.

     

    I have checked that there are no such things as missing parts etc between

    schematic and PCB. Also to point out, there are some devices which have air

    wires attached to some pins while not being attached to other pins on the

    same device.

     

    Is there another way to achieve consistancy?

     

    The option you previuosly stated seems a bit of sledge hammer to crack a

    nut.  I'm also perplexed as to how this consitancy issue has arose since I

    always close both PCB and Schematic by closing Control Panel, and I never

    work with either the schematic or board open individually - they are always

    open as a pair and closed as a pair.

     

    Anyway I hope this provides a greater picture as to my problem, hope you can

    help.

     

    Many thanks.

     

    Jim

    "Jim D" <j.doyle@optosci.com> wrote in message

    news:il31ir$4g5$1@cheetah.cadsoft.de...

    Hi,

     

    I wonder if any one provide assistance.  I have lost consistency on my

    board.  I have tried various methods to fix but without success.  I have

    run ERC and identified say this error below:

     

    "Different connections in IC2B pin OE and pad 4 (GND/ none)"

    I interpret this to mean there is a net connection on GND but NOT on pin

    OE. However there is deffinately a net connection in my schematic as I can

    move the GND symbol or my device (74HCT125D) symbol and see that the net

    is connected to both device and ground.

    I have also tried deleting devices and nets and added new devices from

    library, with no success.  I have also deleted nets and renamed there

    another name and still no success.

     

    How can I fix this ?

     

    Many thanks,

    Jim

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    "Jim D" <j.doyle@optosci.com> wrote in message

    news:il4vih$fdo$1@cheetah.cadsoft.de...

    Is there another way to achieve consistancy?

     

    The simplest way is to delete all nets to the conflicting pins both in sch

    and brd. In sch its easy.

     

    In brd you need to get an airwire to the pin only before you delete it.

    -If there is a wire going to the pad, start by deleting that.

    -Do ratsnest

    -Llook for an airwire. Make sure there is just ONE airwire going to the pad.

    If you get two, you will have more problems after deleting them because you

    will split a net into two different net names. To fix that, do a temporary

    route around the pin (doesnt matter if you overlap) and do ratsnest again.

    Note, if the pin is surrounded by filled polygons, you should temporary

    rename the polygon to something else and redo ratsnest.

    -When you got one airwire to the pad, delete THE AIRWIRE.

    -Redo temporary changes 

    -Now try ERC again.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    "Jim D" <j.doyle@optosci.com> wrote in message

    news:il4vih$fdo$1@cheetah.cadsoft.de...

    Is there another way to achieve consistancy?

     

    The simplest way is to delete all nets to the conflicting pins both in sch

    and brd. In sch its easy.

     

    In brd you need to get an airwire to the pin only before you delete it.

    -If there is a wire going to the pad, start by deleting that.

    -Do ratsnest

    -Llook for an airwire. Make sure there is just ONE airwire going to the pad.

    If you get two, you will have more problems after deleting them because you

    will split a net into two different net names. To fix that, do a temporary

    route around the pin (doesnt matter if you overlap) and do ratsnest again.

    Note, if the pin is surrounded by filled polygons, you should temporary

    rename the polygon to something else and redo ratsnest.

    -When you got one airwire to the pad, delete THE AIRWIRE.

    -Redo temporary changes 

    -Now try ERC again.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    On 03/08/2011 01:12 PM, Morten Leikvoll wrote:

    "Jim D" <j.doyle@optosci.com> wrote in message

    news:il4vih$fdo$1@cheetah.cadsoft.de...

    >> Is there another way to achieve consistancy?

     

    The simplest way is to delete all nets to the conflicting pins both in sch

    and brd. In sch its easy.

     

    In brd you need to get an airwire to the pin only before you delete it.

    -If there is a wire going to the pad, start by deleting that.

    -Do ratsnest

    -Llook for an airwire. Make sure there is just ONE airwire going to the pad.

    If you get two, you will have more problems after deleting them because you

    will split a net into two different net names. To fix that, do a temporary

    route around the pin (doesnt matter if you overlap) and do ratsnest again.

    Note, if the pin is surrounded by filled polygons, you should temporary

    rename the polygon to something else and redo ratsnest.

    -When you got one airwire to the pad, delete THE AIRWIRE.

    -Redo temporary changes 

    -Now try ERC again.

     

     

     

    After removing erroneous nets, you must run ERC again for the brd and

    sch to become consistent again BEFORE you reconnect what once was

    removed. As long as there is an inconsistency noting you do in sch will

    end up in brd.

     

    1) Remove

    2) ERC

    3) Repeat 1) and 2) until consistency has been achieved

    4) Add what was once removed.

    5) Celebrate

     

    Breg

    Vidar(Z)