EAGLE User Support (English) How to clip silk layers using the stop mask layer?
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
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 1077 views
  • Users 0 members are here
Related

How to clip silk layers using the stop mask layer?

alank2
alank2 over 14 years ago

Hi Everyone,

 

In this picture you can see that I have a folded over PTC and its silkscreen runs over a couple of pads:

 

[img]http://home.earthlink.net/~alank2/f1.png[/img]

 

I know I could go into the library, make a custom package and copy the existing package and modify it to remove the silkscreen where it runs into the pads, but I wouldn't want to do this each and everytime I run into a situation like this.  I might end up with 20 packages for a single one with various silk screen parts missing because of different projects.

 

Is there a way that CAM job could do this automatically on its gerber output?  Is there another way to do this?

 

Thanks,

 

Alan

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 14 years ago

    alank2 schrieb:

     

    In this picture you can see that I have a folded over PTC and its

    silkscreen runs over a couple of pads:

    http://home.earthlink.net/~alank2/f1.png[/img]

     

    It's pretty common that the silkscreen runs over surface that is

    intended to be blank - maybe pads or vias.

     

    I know I could go into the library, make a custom package and copy

    the existing package and modify it to remove the silkscreen where it

    runs into the pads, but I wouldn't want to do this each and everytime

    I run into a situation like this.  I might end up with 20 packages

    for a single one with various silk screen parts missing because of

    different projects.

     

    Is there a way that CAM job could do this automatically on its gerber

    output?  Is there another way to do this?

     

    Normally, you don't need to care about this at all, since the board

    house will automatically mask the silkscreen with the solder stop mask

    to avoid printing on solderable surfaces. This is common practice.

     

    If you're not sure, talk to them before ordering your boards.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • alank2
    alank2 over 14 years ago in reply to Former Member

    Hi,

     

    I am surprised that Eagle has a drc error for this, but no way to correct it.  Wouldn't it be better to fix it in your board design instead of relying on a board house to fix it?

     

    Thanks,

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to alank2

    alank2 schrieb:

     

    I am surprised that Eagle has a drc error for this,

     

    IMHO, that should be rather a warning... BTW, if you don't display the

    stop mask layers during DRC, it won't show these "errors".

     

    but no way to

    correct it.  Wouldn't it be better to fix it in your board design

    instead of relying on a board house to fix it?

     

    It can't be "fixed" in the design. Just think about the vias, their

    position can always collide with the silkscreen of a part. The only way

    to fix this would be in the CAMP (masking the silkscreen with the stop

    mask). This has already been suggested, but not implemented - I think

    other issues are (much) more urgent...

     

    And, the board houses are used to do this, I /never/ had any problems

    with silkscreen on solderable surfaces. So it's more a flaw, not really

    erroneous data.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 14 years ago in reply to alank2

    alank2 schrieb:

     

    I am surprised that Eagle has a drc error for this,

     

    IMHO, that should be rather a warning... BTW, if you don't display the

    stop mask layers during DRC, it won't show these "errors".

     

    but no way to

    correct it.  Wouldn't it be better to fix it in your board design

    instead of relying on a board house to fix it?

     

    It can't be "fixed" in the design. Just think about the vias, their

    position can always collide with the silkscreen of a part. The only way

    to fix this would be in the CAMP (masking the silkscreen with the stop

    mask). This has already been suggested, but not implemented - I think

    other issues are (much) more urgent...

     

    And, the board houses are used to do this, I /never/ had any problems

    with silkscreen on solderable surfaces. So it's more a flaw, not really

    erroneous data.

     

    Tilmann