EAGLE User Support (English) Several ground nets
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
  • Replies 11 replies
  • Subscribers 178 subscribers
  • Views 1080 views
  • Users 0 members are here
Related

Several ground nets

Former Member
Former Member over 14 years ago

Hello,

 

in my current design I need a lot of ground nets, each one isolated from

the others.

For example: I use 8 ADM3251. The isolated side should be not connected

to the isolated side of another AMD3251.

 

I also use 8 digital isolator and so on...

 

 

Ok, I could draw a net without any ground symbol but it's not very clear

to read.

 

So, how to draw the same supply pin (e.g. AGND) but with a different

name so they won't be connected together?

 

Thanks!

Marco

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 14 years ago

    On 04/07/2011 07:51 AM, Marco Trapanese wrote:

    Hello,

     

    in my current design I need a lot of ground nets, each one isolated from

    the others.

    For example: I use 8 ADM3251. The isolated side should be not connected

    to the isolated side of another AMD3251.

     

    I also use 8 digital isolator and so on...

     

     

    Ok, I could draw a net without any ground symbol but it's not very clear

    to read.

     

    So, how to draw the same supply pin (e.g. AGND) but with a different

    name so they won't be connected together?

     

    Look in supply2.lbr.  There are several ground symbols labeled 0V, AGND,

    DGND, GND, GND1, GND2, etc.

     

    Enjoy,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Il 07/04/2011 15:30, Chuck Huber ha scritto:

     

    Look in supply2.lbr.  There are several ground symbols labeled 0V, AGND,

    DGND, GND, GND1, GND2, etc.

     

     

    Yes, but I don't want to use 20+ different symbols. May I just rename

    the nets?

     

    Marco

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Marco Trapanese wrote:

    Il 07/04/2011 15:30, Chuck Huber ha scritto:

     

    >> Look in supply2.lbr.  There are several ground symbols labeled 0V, AGND,

    >> DGND, GND, GND1, GND2, etc.

     

    Yes, but I don't want to use 20+ different symbols. May I just rename

    the nets?

     

     

    Ideally yes but I have tried that with power symbols and just renaming

    in the schematic messed up the PADS netlist. So I made library parts for

    all the voltages I usually need, all with the same symbol.

     

    It's not that big a deal. For example, you could make a library

    "trapanesesupply.lib", then add a dozen grounds. A normal one, then

    ISO1, ISO2 and so on. In my experience it makes schematics easier to

    read for others if the isolated grounds have a more unusual ground

    symbol (but all of those have the same type of symbol).

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Il 10/04/2011 20:56, Joerg ha scritto:

     

    It's not that big a deal. For example, you could make a library

    "trapanesesupply.lib", then add a dozen grounds. A normal one, then

    ISO1, ISO2 and so on. In my experience it makes schematics easier to

    read for others if the isolated grounds have a more unusual ground

    symbol (but all of those have the same type of symbol).

     

     

    Yes. It's exactly what I want and what I was going to do.

    Because all of them shares the same symbol I was wondering if I may

    avoid to create n symbols, but only changing their names.

     

    Anyway the straight way seems the better one!

     

    Thanks

    Marco

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Marco Trapanese wrote:

    >Il 07/04/2011 15:30, Chuck Huber ha scritto:

    >> Look in supply2.lbr.  There are several ground symbols labeled 0V, AGND,

    >> DGND, GND, GND1, GND2, etc.

    >Yes, but I don't want to use 20+ different symbols. May I just rename

    >the nets?

     

    supply symbols use a special kind of pins that rename the net they get

    connected to.

    You can rename the net again though, but then you will get into deep

    s... really fast 8-)

     

    So the only clean way for using supply symbols is to create one for

    every separate supply net you need.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Marco Trapanese wrote:

    >Il 07/04/2011 15:30, Chuck Huber ha scritto:

    >> Look in supply2.lbr.  There are several ground symbols labeled 0V, AGND,

    >> DGND, GND, GND1, GND2, etc.

    >Yes, but I don't want to use 20+ different symbols. May I just rename

    >the nets?

     

    supply symbols use a special kind of pins that rename the net they get

    connected to.

    You can rename the net again though, but then you will get into deep

    s... really fast 8-)

     

    So the only clean way for using supply symbols is to create one for

    every separate supply net you need.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Il 11/04/2011 10:15, Lorenz ha scritto:

     

    So the only clean way for using supply symbols is to create one for

    every separate supply net you need.

     

     

    image

    Ok, thank you for the clarification!

     

    Marco