Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Internet request whenever Eagle is launched
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 580 views
  • Users 0 members are here
  • eagle
Related

Internet request whenever Eagle is launched

e14 Contributor
e14 Contributor over 15 years ago

With all of the illicit Internet activity these days, I was concerned when Eagle5.11 requested internet access whenever it was launched.  After discussions with Tech Support, I found that this is due to the "Daily" default setting in Help - Check for Updates.

 

Now that I know that this is why an Internet request was made, there are no problems.  Therefore, for the peace-of-mind of new users, I would suggest that the same "Checking for Updates" window that appears when you manually select Check-for-Updates is also launched whenever the program Automatically checks for updates.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    On 7/21/2011 7:36 PM, jhannas@jrh1.us wrote:

      With all of the illicit Internet activity these days, I was concerned when Eagle5.11 requested internet access whenever it was launched.  After discussions with Tech Support, I found that this is due to the "Daily" default setting in Help - Check for Updates.

     

    Now that I know that this is why an Internet request was made, there are no problems.  Therefore, for the peace-of-mind of new users, I would suggest that the same "Checking for Updates" window that appears when you manually select Check-for-Updates is also launched whenever the program Automatically checks for updates.

     

     

    I would rather it didn't.

    I don't like distractions.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Am 22.07.2011 17:39, schrieb Doug:

    On 7/21/2011 7:36 PM, jhannas@jrh1.us wrote:

    >> With all of the illicit Internet activity these days, I was concerned

    >> when Eagle5.11 requested internet access whenever it was launched.

    >> After discussions with Tech Support, I found that this is due to the

    >> "Daily" default setting in Help - Check for Updates.

    >>

    >> Now that I know that this is why an Internet request was made, there

    >> are no problems. Therefore, for the peace-of-mind of new users, I

    >> would suggest that the same "Checking for Updates" window that appears

    >> when you manually select Check-for-Updates is also launched whenever

    >> the program Automatically checks for updates.

    >>

    >

    I would rather it didn't.

    I don't like distractions.

     

    If you prefer you could switch off these checks. Go to the menu

    Help/Check for Update and set it to "never".

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Am 26.07.2011 09:32, schrieb Richard Hammerl:

    Am 22.07.2011 17:39, schrieb Doug:

    >> On 7/21/2011 7:36 PM, jhannas@jrh1.us wrote:

    >>> With all of the illicit Internet activity these days, I was concerned

    >>> when Eagle5.11 requested internet access whenever it was launched.

    >>> After discussions with Tech Support, I found that this is due to the

    >>> "Daily" default setting in Help - Check for Updates.

    >>>

    >>> Now that I know that this is why an Internet request was made, there

    >>> are no problems. Therefore, for the peace-of-mind of new users, I

    >>> would suggest that the same "Checking for Updates" window that appears

    >>> when you manually select Check-for-Updates is also launched whenever

    >>> the program Automatically checks for updates.

    >>>

    >>

    >> I would rather it didn't.

    >> I don't like distractions.

     

    If you prefer you could switch off these checks. Go to the menu

    Help/Check for Update and set it to "never".

     

    >

    Addition: in control panel image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Perhaps a compromise,  When the software is first installed, usually from the website, it does not have to look for updates.  Why not just leave the checkmarks OFF.  Let the user determine when to look for updates.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Perhaps a compromise,  When the software is first installed, usually from the website, it does not have to look for updates.  Why not just leave the checkmarks OFF.  Let the user determine when to look for updates.