Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Cannot backannotate VIA
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 974 views
  • Users 0 members are here
Related

Cannot backannotate VIA

e14 Contributor
e14 Contributor over 15 years ago

Hi,

 

I added a via (which came up square instead of round ??) to a board, now I cannot remove it as I get 'cannot backannotate this operation. Please do this in the schematic!'.

 

Well I added it on the board layout editor and there is NO visible via on the schematic :-O.

 

Please advise how I am supposed to remove this unwanted item ??.

 

Many Thanks

 

Graham

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    grahamst wrote:

    >I added a via (which came up square instead of round ??) to a board, now I cannot remove it

     

    undo

    ripup

    info

    change shape

     

    are some of the possibilities to get rid or modify the via

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Guys,

     

    Thanks for the help - youp I did find this out.

     

    You might guess that I am a newbie to Eagle CAD - and am finding it a little 'strange' to work with - whats its background ???, did it come from a Linux app originally maybe ??.

     

    i like the command line (once I start to learn the commands better), but the graphical UI has some very strange interpretations.

     

    I can ADD a via but I cannot DELETE one - who's idea of user-friendly' is that ???.

     

    I also tried to find a version comparison for Eagle - to see what version I have to buy for backannotate to work - can't find this anywhere :-((.

     

    Graham

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Guys,

     

    Thanks for the help - youp I did find this out.

     

    You might guess that I am a newbie to Eagle CAD - and am finding it a little 'strange' to work with - whats its background ???, did it come from a Linux app originally maybe ??.

     

    i like the command line (once I start to learn the commands better), but the graphical UI has some very strange interpretations.

     

    I can ADD a via but I cannot DELETE one - who's idea of user-friendly' is that ???.

     

    I also tried to find a version comparison for Eagle - to see what version I have to buy for backannotate to work - can't find this anywhere :-((.

     

    Graham

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Original Message -


     

    From: "grahamst" <communitymanager@premierfarnell.com>

    I can ADD a via but I cannot DELETE one - who's idea of user-friendly' is

    that ???.

     

    Its just because of the sch-brd consistancy connection. If you close your

    schematics, you can delete it, but you loose consistancy. You can also

    delete wires on a standalone board, but when you do this, you split the net

    in two different names. Same happens if you delete a via. each end of the

    via gets different netname (via is just a wire going into the screen).

     

    Now, you could suggest to Cadsoft to replace the deleted wire/via with an

    airwire. That would probably work, but also cause confusion as long as ripup

    exist and does the same. Next Q would be to merge delete with ripup... I

    won't try to defend that right now. Maybe someone can see if it will work or

    not?