Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Schematic transfer Eagle to P-CAD
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 1781 views
  • Users 0 members are here
Related

Schematic transfer Eagle to P-CAD

e14 Contributor
e14 Contributor over 15 years ago

Hello,

 

All my major clients have different CAD systems, some old, some new. So

now there is a new one and they still use P-CAD. Is there are way to

translate my Eagle schematics to P-CAD? I am using 4.16r2.

 

Not that I have high hopes that there is but it can't hurt to ask.

 

--

Regards, Joerg

 

http://www.analogconsultants.com/

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Joerg wrote:

    Hello,

     

    All my major clients have different CAD systems, some old, some new. So

    now there is a new one and they still use P-CAD. Is there are way to

    translate my Eagle schematics to P-CAD? I am using 4.16r2.

     

    Not that I have high hopes that there is but it can't hurt to ask.

     

     

    Hmm ... so I guess there ain't no way to do this.

     

    Anyhow, meantime I had to do the first review and I ended up revising

    their schematics using <ahem, cough, clears throat> ... MS-Paint image

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Joerg schrieb:

     

    >> All my major clients have different CAD systems, some old, some new. So

    >> now there is a new one and they still use P-CAD. Is there are way to

    >> translate my Eagle schematics to P-CAD? I am using 4.16r2.

    >>

    >> Not that I have high hopes that there is but it can't hurt to ask.

     

    Hmm ... so I guess there ain't no way to do this.

     

    Normally, the problem is not mainly at EAGLEs side. You can /export/ the

    complete design data in about any possible format by using ULPs. But

    does P-CAD (for example) have some interface to /import/ a complete

    schematic?

     

    However, care must be taken on different approaches regarding devices

    and how they are referenced. Maybe you'd need some database for

    translation between the two systems (the ULP could make use of that

    database, so the output file could eventually be imported to the target

    system without further modifications).

     

    As an example, Target 3001 (luckily I don't need to use that...) offers

    import of EAGLE designs by providing a specific export ULP - IIRC. The

    exported file can then be imported to Target.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Joerg schrieb:

     

    >> All my major clients have different CAD systems, some old, some new. So

    >> now there is a new one and they still use P-CAD. Is there are way to

    >> translate my Eagle schematics to P-CAD? I am using 4.16r2.

    >>

    >> Not that I have high hopes that there is but it can't hurt to ask.

     

    Hmm ... so I guess there ain't no way to do this.

     

    Normally, the problem is not mainly at EAGLEs side. You can /export/ the

    complete design data in about any possible format by using ULPs. But

    does P-CAD (for example) have some interface to /import/ a complete

    schematic?

     

    However, care must be taken on different approaches regarding devices

    and how they are referenced. Maybe you'd need some database for

    translation between the two systems (the ULP could make use of that

    database, so the output file could eventually be imported to the target

    system without further modifications).

     

    As an example, Target 3001 (luckily I don't need to use that...) offers

    import of EAGLE designs by providing a specific export ULP - IIRC. The

    exported file can then be imported to Target.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Tilmann Reh wrote:

    Joerg schrieb:

     

    >>> Then get that import format specification, take export-schematics.ulp

    >>> and modify it to match the format that P-CAD can import. image

    >> Or I could write myself a new CAD software that does it all image

     

    Of course - however, that might be a little bit more effort.

     

     

    I'll keep doing it with MS-Paint then. That is a bone-simple piece of

    software but remarkably efficient for revising graphics documents. And

    it's free, comes with the computers image

     

    What would be really nice but certainly not coming anytime soon: If you

    could load the whole JPG or whatever format into Eagle schematics as a

    "background", then draw a regular schematic on top of it. Now you could

    also draw schematics with a theme. Maybe with the Golden Gate Bridge or

    the Brandenburg Gate in the background, or Brutus the dog. Now that

    would be cool.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Joerg schrieb:

     

    >> Then get that import format specification, take export-schematics.ulp

    >> and modify it to match the format that P-CAD can import. image

     

    Or I could write myself a new CAD software that does it all image

     

    Of course - however, that might be a little bit more effort.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Tilmann Reh wrote:

    Joerg schrieb:

     

    >>> Normally, the problem is not mainly at EAGLEs side. You can /export/ the

    >>> complete design data in about any possible format by using ULPs. But

    >>> does P-CAD (for example) have some interface to /import/ a complete

    >>> schematic?

    >> I assume there must be because other CAD packages have that P-CAD

    >> linking feature:

    >>

    >> http://www.diptrace.com/releases.php

    >>

    >> Quote:

    >>

    >> # P-CAD ASCII, PADS Import/Export Improved

    >> # P-CAD ASCII, Eagle Script libraries import improved

    >> # OrCAD MIN Interchange Import/Export in PCB Layout

    >>

    >> end quote.

     

    Then get that import format specification, take export-schematics.ulp

    and modify it to match the format that P-CAD can import. image

     

     

    Or I could write myself a new CAD software that does it all image

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Joerg schrieb:

     

    >> Normally, the problem is not mainly at EAGLEs side. You can /export/ the

    >> complete design data in about any possible format by using ULPs. But

    >> does P-CAD (for example) have some interface to /import/ a complete

    >> schematic?

     

    I assume there must be because other CAD packages have that P-CAD

    linking feature:

     

    http://www.diptrace.com/releases.php

     

    Quote:

     

    1. P-CAD ASCII, PADS Import/Export Improved

    2. P-CAD ASCII, Eagle Script libraries import improved

    3. OrCAD MIN Interchange Import/Export in PCB Layout

     

    end quote.

     

    Then get that import format specification, take export-schematics.ulp

    and modify it to match the format that P-CAD can import. image

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Tilmann Reh wrote:

    Joerg schrieb:

     

    >>> All my major clients have different CAD systems, some old, some new. So

    >>> now there is a new one and they still use P-CAD. Is there are way to

    >>> translate my Eagle schematics to P-CAD? I am using 4.16r2.

    >>>

    >>> Not that I have high hopes that there is but it can't hurt to ask.

    >> Hmm ... so I guess there ain't no way to do this.

     

    Normally, the problem is not mainly at EAGLEs side. You can /export/ the

    complete design data in about any possible format by using ULPs. But

    does P-CAD (for example) have some interface to /import/ a complete

    schematic?

     

     

    I assume there must be because other CAD packages have that P-CAD

    linking feature:

     

    http://www.diptrace.com/releases.php

     

    Quote:

     

    1. P-CAD ASCII, PADS Import/Export Improved

    2. P-CAD ASCII, Eagle Script libraries import improved

    3. OrCAD MIN Interchange Import/Export in PCB Layout

     

    end quote.

     

     

    However, care must be taken on different approaches regarding devices

    and how they are referenced. Maybe you'd need some database for

    translation between the two systems (the ULP could make use of that

    database, so the output file could eventually be imported to the target

    system without further modifications).

     

    As an example, Target 3001 (luckily I don't need to use that...) offers

    import of EAGLE designs by providing a specific export ULP - IIRC. The

    exported file can then be imported to Target.

     

     

    I am aware that probably none of such routines will be perfect. But if

    it avoids redrawing only resistors, lines, capacitors and maybe diodes

    and transistors, that covers 90% plus of the grunt work that otherwise

    has to be done. Only fancy parts such as ICs or connectors would need to

    be edited in.

     

    Now I have just "winged it" with MS-Paint which looks ok on paper but

    the client has to draw it all again.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/