I added a line in the BRD: section of eagle.scr to run a ULP when a board
loads. The ULP does run.
Referring to the attached image. The ULP 'statistic-brd has run to the
dialog displaying the results but you can see the board below shows an
incomplete progress bar and a 40% figure.
Closing the ULP dialog quickly clears the 40% indication
What I would like to know what the 40% is referring to so that I can be
assurred the ULP is working with all the board data.
If the board is fully loaded/displayed, as it appears to be, then this may
be simply a delay in updating the status and could be fixed.(v5.11.1)
Thanks
Warren
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.