Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Newbie library question
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 468 views
  • Users 0 members are here
Related

Newbie library question

e14 Contributor
e14 Contributor over 14 years ago

Hi All,

After I open a new Schematics page and click on the ADD command, it is my understanding that the large library should open up. What I am getting is a box labeled ADD with only a few library parts listed in it. Not the main library as I would like. Can someone please tell me how to get the main library to open up whenever I click on or type in ADD in the schematic window?

Thanks in advance for your help.

Jeff M

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 25.09.2011 04:45, schrieb Jeff Morrissey:

    Hi All,

    After I open a new Schematics page and click on the ADD command, it is my understanding that the large library should open up. What I am getting is a box labeled ADD with only a few library parts listed in it. Not the main library as I would like. Can someone please tell me how to get the main library to open up whenever I click on or type in ADD in the schematic window?

    Thanks in advance for your help.

    Jeff M

     

    Actually there is no "THE LARGE LIBRARY" as eagle provides about 300

    libraries on installation. The path to the libraries directory is

    entered in the eagle control panel/Options/Directories. Since this is

    usually done automatically during installation, I assume you just did

    not activate them, putting them IN USE.

    In the command line at the top of your schematic just enter "USE *"

    (without the " )and hit the "Enter" Key. After that you should see all

    the libraries using the ADD command. If not, check the path as mentioned

    above.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Good Morning Joern,

    Thanks for your help with my Newbie question concerning the library. I did as instructed (USE command) and indeed it brought up the large list of libraries. In order to retrieve parts though, I next have to highlite one of the parts files, then right click and choose select. What happens next is that it automatically goes back to the schematic without the file I have chosen. If I type ADD in the sch. command line, I find the part file has been added to the screen that I thought should show up in the first place. This screen has the two smaller boxes on the right side which show symbol and package. I was thinking that all libraries should be available in this screen.

    Am I missing a step, or taking too many?

    Thanks again for your help.

     

    Jeff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 9/25/2011 9:27 AM, Jeff Morrissey wrote:

    Good Morning Joern,

    Thanks for your help with my Newbie question concerning the library. I did as instructed (USE command) and indeed it brought up the large list of libraries. In order to retrieve parts though, I next have to highlite one of the parts files, then right click and choose select. What happens next is that it automatically goes back to the schematic without the file I have chosen. If I type ADD in the sch. command line, I find the part file has been added to the screen that I thought should show up in the first place. This screen has the two smaller boxes on the right side which show symbol and package. I was thinking that all libraries should be available in this screen.

    Am I missing a step, or taking too many?

    Thanks again for your help.

     

    Jeff

     

     

    Once you have "used" all the libraries they should automatically appear

    in the list when you click the add part icon from the schematic editor.

     

     

    Note that in the add part selection you can define a search string (eg

    "soic"  which will search through all the currently used libraries for

    parts that match the search parameters.    You will often not find

    exactly the part you want so its best to make your search terms pretty

    general and refine from there.

     

    jim

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks to Joern & Jim,

    You are exactly right. My ADD library is getting larger each time I access a part in the large (USE) library. It makes sense now as to what's happening and I thank you for your help. I certainly appreciate the help. I have watched several (many) tutorials and somehow these steps you have told me about were not shown. It is very much appreciated when others will stop what they are doing and take the time to help.

     

    Jeff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 25.09.2011 15:45, schrieb Jim Littlefield:

    On 9/25/2011 9:27 AM, Jeff Morrissey wrote:

    >> Good Morning Joern,

    >> Thanks for your help with my Newbie question concerning the library. I

    >> did as instructed (USE command) and indeed it brought up the large

    >> list of libraries. In order to retrieve parts though, I next have to

    >> highlite one of the parts files, then right click and choose select.

    >> What happens next is that it automatically goes back to the schematic

    >> without the file I have chosen. If I type ADD in the sch. command

    >> line, I find the part file has been added to the screen that I thought

    >> should show up in the first place. This screen has the two smaller

    >> boxes on the right side which show symbol and package. I was thinking

    >> that all libraries should be available in this screen.

    >> Am I missing a step, or taking too many?

    >> Thanks again for your help.

    >>

    >> Jeff

    >>

    >

    Once you have "used" all the libraries they should automatically appear

    in the list when you click the add part icon from the schematic editor.

     

    >

    Note that in the add part selection you can define a search string (eg

    "soic" which will search through all the currently used libraries for

    parts that match the search parameters. You will often not find exactly

    the part you want so its best to make your search terms pretty general

    and refine from there.

     

    jim

     

    AFAIK there is no right klick needed to get a device (part) but might be

    configured. In your .sch you click on ADD and a window opens. Resize

    that to your comfort. On the left you see the names of libraries and a

    "+" in front of it. Click it i. e. on "74xx-us" to expand this library.

    Now you see a "74*00" and expand that one too. A list of different

    technologies of this device appears (74LS00,74ALS00 etc).

    Once you mark (click) on one of these, the symbol and the package will

    show in the right windows. To get this you either doubleclick the name

    or you mark it and click OK at the bottom right on this window.

    In the same moment the add window will close, you are back in your .sch

    with the part clinging on your mousepointer. With another click you

    place it on your .sch.

    A different way was descibed by Jim already.

    I suggest you work through the tutorial which comes with eagle in the

    "doc" directory. Check also the www for eagle instructions or hit F1 for

    the eagle help.

    It is better to start easy to learn to use eagle instead of constructing

    a 3000 Megawatt powerplant with frustration at the beginning image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 25.09.2011 15:45, schrieb Jim Littlefield:

    On 9/25/2011 9:27 AM, Jeff Morrissey wrote:

    >> Good Morning Joern,

    >> Thanks for your help with my Newbie question concerning the library. I

    >> did as instructed (USE command) and indeed it brought up the large

    >> list of libraries. In order to retrieve parts though, I next have to

    >> highlite one of the parts files, then right click and choose select.

    >> What happens next is that it automatically goes back to the schematic

    >> without the file I have chosen. If I type ADD in the sch. command

    >> line, I find the part file has been added to the screen that I thought

    >> should show up in the first place. This screen has the two smaller

    >> boxes on the right side which show symbol and package. I was thinking

    >> that all libraries should be available in this screen.

    >> Am I missing a step, or taking too many?

    >> Thanks again for your help.

    >>

    >> Jeff

    >>

    >

    Once you have "used" all the libraries they should automatically appear

    in the list when you click the add part icon from the schematic editor.

     

    >

    Note that in the add part selection you can define a search string (eg

    "soic" which will search through all the currently used libraries for

    parts that match the search parameters. You will often not find exactly

    the part you want so its best to make your search terms pretty general

    and refine from there.

     

    jim

     

    AFAIK there is no right klick needed to get a device (part) but might be

    configured. In your .sch you click on ADD and a window opens. Resize

    that to your comfort. On the left you see the names of libraries and a

    "+" in front of it. Click it i. e. on "74xx-us" to expand this library.

    Now you see a "74*00" and expand that one too. A list of different

    technologies of this device appears (74LS00,74ALS00 etc).

    Once you mark (click) on one of these, the symbol and the package will

    show in the right windows. To get this you either doubleclick the name

    or you mark it and click OK at the bottom right on this window.

    In the same moment the add window will close, you are back in your .sch

    with the part clinging on your mousepointer. With another click you

    place it on your .sch.

    A different way was descibed by Jim already.

    I suggest you work through the tutorial which comes with eagle in the

    "doc" directory. Check also the www for eagle instructions or hit F1 for

    the eagle help.

    It is better to start easy to learn to use eagle instead of constructing

    a 3000 Megawatt powerplant with frustration at the beginning image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks to Joern & Jim,

    You are exactly right. My ADD library is getting larger each time I access a part in the large (USE) library. It makes sense now as to what's happening and I thank you for your help. I certainly appreciate the help. I have watched several (many) tutorials and somehow these steps you have told me about were not shown. It is very much appreciated when others will stop what they are doing and take the time to help.

     

    Jeff