Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) .DRL File Eagle Freeware V5.11.0
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 1210 views
  • Users 0 members are here
Related

.DRL File Eagle Freeware V5.11.0

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

So I am attempting to use the CAM processor to generate my board files, and all of the files are processed/generated fine EXCEPT that the Excellon CAM processor I am attempting to use to generate the .drl drill file is not working properly.  Instead of producing a .drl or .drd file as it should, it keeps only creating a .dri information file instead, which the manufacturer cannot use to do their design rule check (DRC).  All of the other necessary files were successfully generated using the gerb274x.cam processor which worked perfectly, but that does not generate a .drl file as far as I know. 

 

Has anyone else encountered this problem in the freeware V5.11.0 version of EAGLE?  I have tried pretty much everything that I know of in terms of the options that are available but cannot figure it out.

 

Any help is greatly appreciated.

M

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 10/21/2011 3:53 PM, matthew mosteller wrote:

    Hi,

     

    So I am attempting to use the CAM processor to generate my board files, and all of the files are processed/generated fine EXCEPT that the Excellon CAM processor I am attempting to use to generate the .drl drill file is not working properly.  Instead of producing a .drl or .drd file as it should, it keeps only creating a .dri information file instead, which the manufacturer cannot use to do their design rule check (DRC).  All of the other necessary files were successfully generated using the gerb274x.cam processor which worked perfectly, but that does not generate a .drl file as far as I know.

     

    Has anyone else encountered this problem in the freeware V5.11.0 version of EAGLE?  I have tried pretty much everything that I know of in terms of the options that are available but cannot figure it out.

     

    Any help is greatly appreciated.

    M

     

     

    Hi Matthew,

     

    In the board editor, open the CAM processor by clicking the CAM icon.

     

    Withing the CAM dialog click File-> Open -> Job.

     

    Select excellon.cam and click open.

     

    Click process job, you will now find a drd and a dri file in the same

    directory as your board. This is all assuming that the default

    excellon.cam job has not been modified. The dri file is just a summary

    of what the CAM processor did, the drd is the file you want.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks!

     

    For some reason when I do this, I still get the same result, where it produces the .dri file but not the .drd file.

     

    I have not edited the CAM file at all (it is locked actually so that I cannot) so I am not entirely sure why this is still happening.  Any further help possible?

     

    M

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks!

     

    For some reason when I do this, I still get the same result, where it produces the .dri file but not the .drd file.

     

    I have not edited the CAM file at all (it is locked actually so that I cannot) so I am not entirely sure why this is still happening.  Any further help possible?

     

    M

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Am 24.10.2011 22:01, schrieb matthew mosteller:

    Thanks!

     

    For some reason when I do this, I still get the same result, where it produces the .dri file but not the .drd file.

     

    I have not edited the CAM file at all (it is locked actually so that I cannot) so I am not entirely sure why this is still happening.  Any further help possible?

     

    M

     

     

    Could you check the settings of your Windows Explorer? Maybe you

    hide the "known" file extensions and the extension of the drd

    file is not shown....

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 10/24/2011 4:01 PM, matthew mosteller wrote:

    Thanks!

     

    For some reason when I do this, I still get the same result, where it produces the .dri file but not the .drd file.

     

    I have not edited the CAM file at all (it is locked actually so that I cannot) so I am not entirely sure why this is still happening.  Any further help possible?

     

    M

     

     

    Hi Matt,

     

    Are you running Windows 7? Make sure that you are running EAGLE as an

    administrator. Right-click on the EAGLE icon and and then select Run as

    administrator.

     

    Try running the CAM job now and let's see what happens.

     

    Best Regards,

    Jorge