Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle schematic
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 381 views
  • Users 0 members are here
Related

Eagle schematic

e14 Contributor
e14 Contributor over 14 years ago

I'm new with Eagle and have a problem which I hope someone can help me with.

When I select a Hex INVERTER 7404N, some 74LS90N and a NE555NNE555N from tre library and puts them into the schematic, Vcc and GND will

be automatically linked. But the Vcc on the NE555NNE555N will not be automatically linked with the others Vcc. How do I connect eg. Vcc on NE555NNE555N

to the Vcc on one of the 74LS90N in schematic?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 03.11.2011 08:24, schrieb Per Ritter:

    I'm new with Eagle and have a problem which I hope someone can help me with.

    When I select a Hex INVERTER 7404N, some 74LS90N and a NE555NNE555N from tre library and puts them into the schematic, Vcc and GND will

    be automatically linked. But the Vcc on the NE555NNE555N will not be automatically linked with the others Vcc. How do I connect eg. Vcc on NE555NNE555N

    to the Vcc on one of the 74LS90N in schematic?

     

    Wellcome new user image

    I suppose the "problem" is mostly, that the name of the 555 is not "VCC"

    but something else, like V+. For eagle this are two different nets and

    therefor they are not connected together. You can connect the 555's "V+"

    to the "VCC" using the NET command. (Allways use NET to connect devices

    together, Do NOT use "Wire").

    If you use the ERC you woll get a warning that V+ and VCC are connected

    together. If this is correct (like in this case) you can just

    acknöwledge the warning, otherwise you have to take steps of course.

    (there is a tutorial in the "doc" dicectory of eagle or just hit the

    F1 key for help)

    Have fun.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag