Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) parameters file
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 884 views
  • Users 0 members are here
  • parameters
Related

parameters file

david_f
david_f over 14 years ago

Hello,

 

In the demo projects there are parameters inclued in the project (width_menu, diameter_menu...).

I found the command string to change the different values but I don't find the file where it stored.

 

Are these parameters stored in a parameter file?

 

I'd like to have the same parameters for all new projects and I wouldn't enter manualy the values each time.

 

Thanks for help.

 

David

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    david fournier wrote:

    Hello,

     

    In the demo projects there are parameters inclued in the project

    (width_menu, diameter_menu...).

    I found the command string to change the different values but I don't

    find the file where it stored.

     

    Are these parameters stored in a parameter file?

     

    I'd like to have the same parameters for all new projects and I

    wouldn't enter manualy the values each time.

     

    Thanks for help.

     

    David

     

    Eagle starts each time using a default set of settings until modified by a

    later action. You did this manually from the command line but it can be done

    for you as you open a design file.

     

    The parameters you see in the demo projects are the eagle native(default)

    ones unless modified by 'eagle.scr'

     

    Each time you open a design file the script file 'eagle.scr' is

    automatically run. It is here you place these same command lines you

    manually entered so that your wishes are implemented.

    Any eagle.scr settings change the native default settings. If nothing is

    mentioned nothing changes.

    View eagle.scr and note the different sections. Place your SET commands in

    the BRD: section

     

    e.g.

    Set Width_Menu 0 0.001 0.004 0.006 0.01 0.015 0.02 0.025 0.03 0.04 0.05 0.06

    0.08 0.1 0.15 0.2;

    Change Width 0.03;

     

    Another file interacts here, in some cases, as well. 'eaglerc.usr' . This

    stores user settings the last time you saved all /exited a file/project. and

    restores them upon opening the next design file. Sometimes it happens that a

    change to eagle.scr does not appear to work when it is 'eaglerc.usr' making

    itself felt. So during testing you need to assure that the editor you are

    working in reflects the way you want it when you close it.  That said, your

    'width_menu, diameter_menu' lists are not held there.

     

    All the best

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 03.11.2011 22:47, schrieb Warren Brayshaw:

    Each time you open a design file the script file 'eagle.scr' is

    automatically run.

     

    Please note that this eagle.scr is NOT run if you open any design saved

    as a PROJECT (the ones that have a gray or green dot in the control

    panel), which is rather confusing.

     

    Therefore, BEFORE creating designs, you should think about what you want

    or need:

      1. If you want to equip every design with its OWN settings, menus,

         etc., create your design with "new project". Its settings are

         then stored in a separate file, and your default settings from

         'eagle.scr' are ignored, as they might be replaced by your

         project's own ones.

         This might save time during design, because all settings stay

         as when last edited, BUT small mistakes (e.g., showing a

         different grid just for measuring) will NEVER be set back to

         useful defaults, so chances for mistakes are higher.

      2. If you want to open every design with some DEFAULT settings,

         menus, etc., independent of its settings when last edited, do

         NOT use projects, but 'new schematic'. This does NOT

         save any settings, so the defaults from 'eagle.scr' are used

         EVERY TIME you open the design.

         This takes some seconds longer during design, because

         previously changed settings get reset automatically, BUT at

         least one can RELY on those defaults and does not need to

         make sure that all millions of possible settings were really

         left as wanted on last exit.

     

    It's your choice how you want to work.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 03.11.2011 22:47, schrieb Warren Brayshaw:

    Each time you open a design file the script file 'eagle.scr' is

    automatically run.

     

    Please note that this eagle.scr is NOT run if you open any design saved

    as a PROJECT (the ones that have a gray or green dot in the control

    panel), which is rather confusing.

     

    Therefore, BEFORE creating designs, you should think about what you want

    or need:

      1. If you want to equip every design with its OWN settings, menus,

         etc., create your design with "new project". Its settings are

         then stored in a separate file, and your default settings from

         'eagle.scr' are ignored, as they might be replaced by your

         project's own ones.

         This might save time during design, because all settings stay

         as when last edited, BUT small mistakes (e.g., showing a

         different grid just for measuring) will NEVER be set back to

         useful defaults, so chances for mistakes are higher.

      2. If you want to open every design with some DEFAULT settings,

         menus, etc., independent of its settings when last edited, do

         NOT use projects, but 'new schematic'. This does NOT

         save any settings, so the defaults from 'eagle.scr' are used

         EVERY TIME you open the design.

         This takes some seconds longer during design, because

         previously changed settings get reset automatically, BUT at

         least one can RELY on those defaults and does not need to

         make sure that all millions of possible settings were really

         left as wanted on last exit.

     

    It's your choice how you want to work.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Andreas Weidner schrieb:

     

    >> The settings in eagle.scr are also applied when files are re-opened.

     

    Not always. I will be a bit more specific:

      - If you have NOT created a project, but just some schematics (so

        you do NOT have a *.epf file in your design directory), the

        settings from 'eagle.scr' are applied EVERY TIME you open one

        design file.

      - If you DO create a project, at the time of creation, the defaults

        are taken from 'eagle.scr' (I THINK, but I'm not 100% sure, because

        I never use projects), but then the settings are independently

        saved, and 'eagle.scr' is NOT run again at ANY time for this

        project (this NOT-running is the reason why we don't use projects

        here).

     

    It's even more complicated - if you use several design files within one

    project...

     

    That's why I don't let eagle.scr change any such settings.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 04.11.2011 11:43, schrieb Tilmann Reh:

    >> If I create a "new project", where the default settings come from?

    >> 'eagle.scr' or an other file?

     

    The settings in eagle.scr are also applied when files are re-opened.

     

    Not always. I will be a bit more specific:

      - If you have NOT created a project, but just some schematics (so

        you do NOT have a *.epf file in your design directory), the

        settings from 'eagle.scr' are applied EVERY TIME you open one

        design file.

      - If you DO create a project, at the time of creation, the defaults

        are taken from 'eagle.scr' (I THINK, but I'm not 100% sure, because

        I never use projects), but then the settings are independently

        saved, and 'eagle.scr' is NOT run again at ANY time for this

        project (this NOT-running is the reason why we don't use projects

        here).

     

    >> I want to use the same default settings (grid unit, width_menu...)

    >> for all projects and modify some settings later if I want.

     

    Since we don't use projects here, I don't know what's the best way to do

    that. Tilmann's method will surely work, and since he seems to be an

    experienced guy, I just take it for granted that that's the way to go...

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to david_f

    david fournier schrieb:

     

    If I create a "new project", where the default settings come from?

    'eagle.scr' or an other file?

     

    The settings in eagle.scr are also applied when files are re-opened.

     

    I want to use the same default settings (grid unit, width_menu...)

    for all projects and modify some settings later if I want.

     

    For this, I use my personal "defaults.scr" containing all my personal

    favorite settings (used layers, colors, grid, via size, text size etc.).

    After creating a board from a schematic, I simply run that script.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • david_f
    david_f over 14 years ago in reply to e14 Contributor

    Hello,

     

    Thanks for your help. I'm a new user of EAGLE.

     

    If I create a "new project", where the default settings come from? 'eagle.scr' or an other file?

     

    I want to use the same default settings (grid unit, width_menu...) for all projects and modify some settings later if I want.

     

    Best regards

     

    David.