Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Semi-Automatic renumbering
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 188 subscribers
  • Views 1003 views
  • Users 0 members are here
Related

Semi-Automatic renumbering

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

this is a suggestion following a question in the previous thread.

 

Often, when renumbering the parts of a circuit so that the part names

follow the structure or signal flow of the schematic, it's much work to

rename the parts manually in the desired order: you have to enter the

parts name completely, for every single part. It's also error prone,

since you easily mistype some detail.

 

Since EAGLE already has mechanisms to assign the next available/unused

part index to some part (when using ADD), it seems pretty obvious to

make this mechanism available for the user. That way, after having

renumbered the parts to some higher starting number (for which ULPs

exist), parts could be renumbered in any order by simply clicking them

one after another.

 

The related command could be "NAME AUTO" (or maybe "NAME NEXT"). It

should be rather simple to implement, since the underlying mechanism is

completely implemented already. As long as "NAME AUTO" is active, any

part clicked with the mouse should get a new name consisting of the

current prefix and the next free/unused index.

 

The command should be available in schematic, board and library editor

as well (think of renaming pads).

 

Tilmann

 

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Chuck Huber wrote:

     

    >How about reversing that... use a group to set part numbers.  i.e.

    >Enclose a set of components in a group, the say "start renumbering at

    >10".  All the R's start at 10, all the C's start at 10, and so on.

     

    also a nice method, somewhat less control over the naming, less work.

     

    Oliver

    --

    Oliver Betz, Munich

    despammed.com is broken, use Reply-To:

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Chuck Huber schrieb:

     

    How about reversing that... use a group to set part numbers.  i.e.

    Enclose a set of components in a group, the say "start renumbering at

    10".  All the R's start at 10, all the C's start at 10, and so on.

     

    This would also accommodate Morten's preference of having a refdes of

    <prefix><page#><index>.

     

    This sounds like a job for a ulp.

     

    Of course there already are ULPs for this. But those renumber strictly

    sorted by coordinates, while manual renumbering would normally do it

    another way (following circuit parts or signal flow). That's exactly why

    I posted that suggestion. I would like to be able to specify the

    numbering order by clicking the parts in exactly that order.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 11/14/2011 09:03 AM, Oliver Betz wrote:

    Since I often use part numbers to group components, I would prefer an

    implementation, where I can type a starting number somewhere.

     

    Oliver,

     

    How about reversing that... use a group to set part numbers.  i.e.

    Enclose a set of components in a group, the say "start renumbering at

    10".  All the R's start at 10, all the C's start at 10, and so on.

     

    This would also accommodate Morten's preference of having a refdes of

    .

     

    This sounds like a job for a ulp.

     

    Enjoy,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 16.11.2011 14:58, schrieb Chuck Huber:

    One other thing to consider is a conflict.  What if an R20 already

    exists, perhaps on another sheet?  In this case, the names could be swapped.

    To answer this and for completeness, that's my comment on this topic from

    the other thread:

     

    I would expect something like that in the Name dialog box:

      - "Auto increase" checkbox

      - "Resolve collisions" radio group or choice

        ("Inhibit", "Skip", "Rename other")

    Maybe a context sensitive toolbar could indicate whether the next number

    is available (green) or not (red).

    Maybe the two features could be integrated into the context sensitive

    toolbar instead or in addition to the dialog box.

     

     

    Regards,

     

    Dietmar

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 11/16/2011 02:33 AM, Tilmann Reh wrote:

    Oliver Betz schrieb:

     

    >>> The related command could be "NAME AUTO" (or maybe "NAME NEXT"). It

    >>> should be rather simple to implement, since the underlying mechanism is

    >>> completely implemented already. As long as "NAME AUTO" is active, any

    >>> part clicked with the mouse should get a new name consisting of the

    >>> current prefix and the next free/unused index.

    >>

    >> Since I often use part numbers to group components, I would prefer an

    >> implementation, where I can type a starting number somewhere.

    >>

    >> If possible, I set the numerical part of different types of components

    >> to similar numbers if they belong together

    >>

    >> R20 ... R35, C20 ... C27 and so on.

    >>

    >> Then I want to continue with R40 for another part of the circuit.

     

    You're right, I also do it that way sometimes (when circuit parts shall

    be clearly separated by the part indexes).

     

    I'll through my two cents in as well.  This would be a handy feature.

    "Name Auto 20", then start clicking away on the R's.

     

    One other thing to consider is a conflict.  What if an R20 already

    exists, perhaps on another sheet?  In this case, the names could be swapped.

     

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Morten Leikvoll schrieb:

     

    I usually don't care about refdes until components are placed. Then I run my

    own auto-numbering ULP.

     

    No problem, you don't need to use that new feature if it was

    implemented. image

     

    Tilmann

     

    P.S. Many times, my own renumbering ULPs also are sufficient for me.

    However, from time to time I really miss such a semi-automatic function

    which would save me a lot of typing...

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Oliver Betz schrieb:

     

    >>The related command could be "NAME AUTO" (or maybe "NAME NEXT"). It

    >>should be rather simple to implement, since the underlying mechanism is

    >>completely implemented already. As long as "NAME AUTO" is active, any

    >>part clicked with the mouse should get a new name consisting of the

    >>current prefix and the next free/unused index.

     

    Since I often use part numbers to group components, I would prefer an

    implementation, where I can type a starting number somewhere.

     

    If possible, I set the numerical part of different types of components

    to similar numbers if they belong together

     

    R20 ... R35, C20 ... C27 and so on.

     

    Then I want to continue with R40 for another part of the circuit.

     

    You're right, I also do it that way sometimes (when circuit parts shall

    be clearly separated by the part indexes).

     

    This could be solved by adding a starting number parameter - and EAGLE

    assigning the next free index /above that number/.

     

    So the command syntax might be:

    NAME AUTO * * *    (assign the next free index)

    NAME AUTO )

     

    "NAME @" could also be a senseful command name to avoid conflicts with

    other flavours of renaming something.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I usually don't care about refdes until components are placed. Then I run my

    own auto-numbering ULP.

    The way the ULP does it is to rename all old name/refdes's with the suffix

    "_old", then start auto numbering.

    Personally I prefer a system to the numbering, where the two last digits are

    the index within a page (sorted from left to right and down to up), while

    the other digits are page number in schematics.

    So you will have refdes that says "". That

    works nice to track components from board to schematics.

     

    On some refdes (like decoupler caps) I like to add a suffix to tell what pin

    of the IC it should be close to (wich my renumbering ULP keeps). This makes

    it easier to do the nitpick placing of decouplers and similar critical

    components.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Tilmann Reh wrote:

     

     

    >Since EAGLE already has mechanisms to assign the next available/unused

    >part index to some part (when using ADD), it seems pretty obvious to

    >make this mechanism available for the user. That way, after having

    >renumbered the parts to some higher starting number (for which ULPs

    >exist), parts could be renumbered in any order by simply clicking them

    >one after another.

    >The related command could be "NAME AUTO" (or maybe "NAME NEXT"). It

    >should be rather simple to implement, since the underlying mechanism is

    >completely implemented already. As long as "NAME AUTO" is active, any

    >part clicked with the mouse should get a new name consisting of the

    >current prefix and the next free/unused index.

     

    Since I often use part numbers to group components, I would prefer an

    implementation, where I can type a starting number somewhere.

     

    If possible, I set the numerical part of different types of components

    to similar numbers if they belong together

     

    R20 ... R35, C20 ... C27 and so on.

     

    Then I want to continue with R40 for another part of the circuit.

     

    Oliver

    --

    Oliver Betz, Munich

    despammed.com is broken, use Reply-To: