Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Semi-Automatic renumbering
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 188 subscribers
  • Views 1007 views
  • Users 0 members are here
Related

Semi-Automatic renumbering

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

this is a suggestion following a question in the previous thread.

 

Often, when renumbering the parts of a circuit so that the part names

follow the structure or signal flow of the schematic, it's much work to

rename the parts manually in the desired order: you have to enter the

parts name completely, for every single part. It's also error prone,

since you easily mistype some detail.

 

Since EAGLE already has mechanisms to assign the next available/unused

part index to some part (when using ADD), it seems pretty obvious to

make this mechanism available for the user. That way, after having

renumbered the parts to some higher starting number (for which ULPs

exist), parts could be renumbered in any order by simply clicking them

one after another.

 

The related command could be "NAME AUTO" (or maybe "NAME NEXT"). It

should be rather simple to implement, since the underlying mechanism is

completely implemented already. As long as "NAME AUTO" is active, any

part clicked with the mouse should get a new name consisting of the

current prefix and the next free/unused index.

 

The command should be available in schematic, board and library editor

as well (think of renaming pads).

 

Tilmann

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Tilmann Reh wrote:

     

     

    >Since EAGLE already has mechanisms to assign the next available/unused

    >part index to some part (when using ADD), it seems pretty obvious to

    >make this mechanism available for the user. That way, after having

    >renumbered the parts to some higher starting number (for which ULPs

    >exist), parts could be renumbered in any order by simply clicking them

    >one after another.

    >The related command could be "NAME AUTO" (or maybe "NAME NEXT"). It

    >should be rather simple to implement, since the underlying mechanism is

    >completely implemented already. As long as "NAME AUTO" is active, any

    >part clicked with the mouse should get a new name consisting of the

    >current prefix and the next free/unused index.

     

    Since I often use part numbers to group components, I would prefer an

    implementation, where I can type a starting number somewhere.

     

    If possible, I set the numerical part of different types of components

    to similar numbers if they belong together

     

    R20 ... R35, C20 ... C27 and so on.

     

    Then I want to continue with R40 for another part of the circuit.

     

    Oliver

    --

    Oliver Betz, Munich

    despammed.com is broken, use Reply-To:

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 11/14/2011 09:03 AM, Oliver Betz wrote:

    Since I often use part numbers to group components, I would prefer an

    implementation, where I can type a starting number somewhere.

     

    Oliver,

     

    How about reversing that... use a group to set part numbers.  i.e.

    Enclose a set of components in a group, the say "start renumbering at

    10".  All the R's start at 10, all the C's start at 10, and so on.

     

    This would also accommodate Morten's preference of having a refdes of

    .

     

    This sounds like a job for a ulp.

     

    Enjoy,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 11/14/2011 09:03 AM, Oliver Betz wrote:

    Since I often use part numbers to group components, I would prefer an

    implementation, where I can type a starting number somewhere.

     

    Oliver,

     

    How about reversing that... use a group to set part numbers.  i.e.

    Enclose a set of components in a group, the say "start renumbering at

    10".  All the R's start at 10, all the C's start at 10, and so on.

     

    This would also accommodate Morten's preference of having a refdes of

    .

     

    This sounds like a job for a ulp.

     

    Enjoy,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Chuck Huber wrote:

     

    >How about reversing that... use a group to set part numbers.  i.e.

    >Enclose a set of components in a group, the say "start renumbering at

    >10".  All the R's start at 10, all the C's start at 10, and so on.

     

    also a nice method, somewhat less control over the naming, less work.

     

    Oliver

    --

    Oliver Betz, Munich

    despammed.com is broken, use Reply-To:

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Chuck Huber schrieb:

     

    How about reversing that... use a group to set part numbers.  i.e.

    Enclose a set of components in a group, the say "start renumbering at

    10".  All the R's start at 10, all the C's start at 10, and so on.

     

    This would also accommodate Morten's preference of having a refdes of

    <prefix><page#><index>.

     

    This sounds like a job for a ulp.

     

    Of course there already are ULPs for this. But those renumber strictly

    sorted by coordinates, while manual renumbering would normally do it

    another way (following circuit parts or signal flow). That's exactly why

    I posted that suggestion. I would like to be able to specify the

    numbering order by clicking the parts in exactly that order.

     

    Tilmann