New to eagle along with the fact that the last time I ever laid out a board
we were still using tape and pads. :d So far things are going well but I
have a few questions.
1. Via's with SMD parts. when connecting two SMD parts on direct opposite
sides of a board and who's pads line up, in this case two 5050 LED's, can
you place a via, or the plate through hold, on the pad? I hate to loose the
lanes just to place a full via pad.
2. Polygons for power and ground on a two sided board. Can I use the
polygon to interconnect the power and grounds to components? I'd like to
know keep putting in traces and just let the polygon connect them.
3. Cutouts. I have a large hole that need to be cut in the middle of the
board so part of a component can go though it. What's the best way to do
this?
4. Can eagle panelize or is that best left to the vendor?
Thanks
John
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.