Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) MARK - Set from object 'Information'  dia log
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 269 views
  • Users 0 members are here
Related

MARK - Set from object 'Information'  dia log

e14 Contributor
e14 Contributor over 14 years ago

It would be very useful if you could set the MARK from within a information

dialog using the coordinate information of the object.

 

The attached shows an example for the wire object.

 

The mark should be set upon exiting the dialog or clicking 'apply' giving a

visual indication that the correct end of the wire had been selected.

 

I see this being useful for the wire and arc ends, and circle center.

 

Currently setting a MARK off the current grid requires you to specify the

coordinates which are usually obtained from object information dialogs.

 

Unfortunetly this takes multiple copy and pastes or hopefully you remember

the figures correctly to type. Generally the current process is painful.

 

Thank you for the consideration

Warren

 

 

Cur

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Warren Brayshaw wrote:

    It would be very useful if you could set the MARK from within a

    information dialog using the coordinate information of the object.

     

    The attached shows an example for the wire object.

     

    The mark should be set upon exiting the dialog or clicking 'apply'

    giving a visual indication that the correct end of the wire had been

    selected.

     

    I see this being useful for the wire and arc ends, and circle center.

     

    Currently setting a MARK off the current grid requires you to specify

    the coordinates which are usually obtained from object information

    dialogs.

     

    Unfortunetly this takes multiple copy and pastes or hopefully you

    remember the figures correctly to type. Generally the current process

    is painful.

     

     

    I should perhaps state my end goal rather than a solution that is v5 based.

    V6 has the potentioal to offer a better solution.

     

    The requirement is to be able to place the MARK at the exact end of a wire

    or center of a circle.

    The purpose is to be enable to use relative  and polar coordinates to

    further develop the design accurately referrenced to existing objects. .

     

    The initial method I suggested could well coexist with a more efficient

    suggestion detailed below as it would satisfy those pushing for more GUI

     

    I now suggest as the method to place the MARK at the end of a wire or

    circle center is to leverage the code that already exists.

    MARK could work similar to WIRE where, if you hold the CTL key it will snap

    you to the wire end within snap range.

    MARK currently snaps to the grid using CTL so SHIFT could be used for this

    alernate function where MARK snaps to the wire end or circle center

     

    V6 has dimension code that snaps the points to various naerby objects. I

    feel this ccould be leveaged to obtain this functionality.

     

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Warren Brayshaw wrote:

    It would be very useful if you could set the MARK from within a

    information dialog using the coordinate information of the object.

     

    The attached shows an example for the wire object.

     

    The mark should be set upon exiting the dialog or clicking 'apply'

    giving a visual indication that the correct end of the wire had been

    selected.

     

    I see this being useful for the wire and arc ends, and circle center.

     

    Currently setting a MARK off the current grid requires you to specify

    the coordinates which are usually obtained from object information

    dialogs.

     

    Unfortunetly this takes multiple copy and pastes or hopefully you

    remember the figures correctly to type. Generally the current process

    is painful.

     

     

    I should perhaps state my end goal rather than a solution that is v5 based.

    V6 has the potentioal to offer a better solution.

     

    The requirement is to be able to place the MARK at the exact end of a wire

    or center of a circle.

    The purpose is to be enable to use relative  and polar coordinates to

    further develop the design accurately referrenced to existing objects. .

     

    The initial method I suggested could well coexist with a more efficient

    suggestion detailed below as it would satisfy those pushing for more GUI

     

    I now suggest as the method to place the MARK at the end of a wire or

    circle center is to leverage the code that already exists.

    MARK could work similar to WIRE where, if you hold the CTL key it will snap

    you to the wire end within snap range.

    MARK currently snaps to the grid using CTL so SHIFT could be used for this

    alernate function where MARK snaps to the wire end or circle center

     

    V6 has dimension code that snaps the points to various naerby objects. I

    feel this ccould be leveaged to obtain this functionality.

     

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de