Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Scroll wheel with Eagle 6 on Mac
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 191 subscribers
  • Views 3222 views
  • Users 0 members are here
  • mac
  • zoom
  • mouse
Related

Scroll wheel with Eagle 6 on Mac

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I've just upgraded to Eagle 6 (I'm looking forward to  indexing the XML format files for my search engine!) - however, I can't  get the scroll wheel to work.

 

It's enabled in the options (User Interface -> Mouse wheel zoom = 1.2), but it does absolutely nothing.

 

If I load Eagle 5.11, it works fine.

 

Note that setting the zoom to 0 doesn't allow me to scroll around either.

 

This happens with both of my mice (wired and wireless mighty mouse).

 

Any ideas?

 

BTW, I'm glad the bug where my ULPs to set the print zoom, mirror, black and so forth has been fixed since 5.11 - although I still can't use the Cmd-<n> keys to switch between the windows.

  • Sign in to reply
  • Cancel
Parents
  • kcadsoft
    kcadsoft over 14 years ago

    On 12/14/11 20:29, Jason Tribbeck wrote:

    Hi,

     

    I've just upgraded to Eagle 6 (I'm looking forward to  indexing the XML format files for my search engine!) - however, I can't  get the scroll wheel to work.

     

    It's enabled in the options (User Interface ->  Mouse wheel zoom = 1.2), but it does absolutely nothing.

     

    If I load Eagle 5.11, it works fine.

     

    Note that setting the zoom to 0 doesn't allow me to scroll around either.

     

    This happens with both of my mice (wired and wireless mighty mouse).

     

    Any ideas?

     

    The next beta version 6.0.1 will have a switch in "Options/User interface"

    named "Legacy mouse wheel mode" that can be selected to switch back

    to the old mouse wheel handling under Mac OS X.

    Please watch the eagle.betatest newsgroup for the announcement of version 6.0.1.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to kcadsoft

    Hi,

     

    Many thanks for the reply. I'll look on the beta releases.

     

    Does this mean if I had a track-pad, or the new mouse, it would work fine?

     

    I do have a "Contour Design ShuttleXpress", which, after I'd posted my message, I configured the central jog wheel to send Shift-F3 and Shift-F4, and made these keys use "Window 1.2" and "Window 0.8333333" which zooms a bit - although it's central to the screen, rather than the mouse pointer position. Is there a way to get the Window command to use the mouse pointer, rather than the screen? This would be a closer workaround.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to kcadsoft

    Hi,

     

    Many thanks for the reply. I'll look on the beta releases.

     

    Does this mean if I had a track-pad, or the new mouse, it would work fine?

     

    I do have a "Contour Design ShuttleXpress", which, after I'd posted my message, I configured the central jog wheel to send Shift-F3 and Shift-F4, and made these keys use "Window 1.2" and "Window 0.8333333" which zooms a bit - although it's central to the screen, rather than the mouse pointer position. Is there a way to get the Window command to use the mouse pointer, rather than the screen? This would be a closer workaround.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • kcadsoft
    kcadsoft over 14 years ago in reply to e14 Contributor

    On 12/15/11 11:59, Jason Tribbeck wrote:

    Hi,

     

    Many thanks for the reply. I'll look on the beta releases.

     

    Does this mean if I had a track-pad, or the new mouse, it would work fine?

     

    It means that you can switch between the way things were done

    in version 5 and the new method that tries to implement the

    new two-finger-pan-gestures as used in Mac OS X 10.7. With

    a MagicTrackpad these work really nice.

     

    I do have a "Contour Design ShuttleXpress", which, after I'd posted my message, I configured the central jog wheel to send Shift-F3 and Shift-F4, and made these keys use "Window 1.2" and "Window 0.8333333" which zooms a bit - although it's central to the screen, rather than the mouse pointer position. Is there a way to get the Window command to use the mouse pointer, rather than the screen? This would be a closer workaround.

     

    You can use

     

       WINDOW (@);

     

    to move the point at the current mouse position to the

    center of the editor window. But I'm not sure if this

    will actually help here. I'm afraid simulating what the

    mouse wheel does by means of command line entries can't be

    done.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________