Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Scroll wheel with Eagle 6 on Mac
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 191 subscribers
  • Views 3235 views
  • Users 0 members are here
  • mac
  • zoom
  • mouse
Related

Scroll wheel with Eagle 6 on Mac

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I've just upgraded to Eagle 6 (I'm looking forward to  indexing the XML format files for my search engine!) - however, I can't  get the scroll wheel to work.

 

It's enabled in the options (User Interface -> Mouse wheel zoom = 1.2), but it does absolutely nothing.

 

If I load Eagle 5.11, it works fine.

 

Note that setting the zoom to 0 doesn't allow me to scroll around either.

 

This happens with both of my mice (wired and wireless mighty mouse).

 

Any ideas?

 

BTW, I'm glad the bug where my ULPs to set the print zoom, mirror, black and so forth has been fixed since 5.11 - although I still can't use the Cmd-<n> keys to switch between the windows.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I'd like to second thefool's suggestion. I have an Apple Magic Mouse and would like to be able to scroll and zoom using the touch surface. Scrolling should be the default behavior, since it is consistent with mouse usage in other applications. Zooming should be accomplished through use of an option/alt key modifier as thefool suggests.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I just installed Eagle 6.1 on my Mac (running Lion), and am very happy that pinch-to-zoom works now, and I can pan in Eagle!

     

    However, I often use an external mouse, without "pinch to zoom" functionality. I never liked the "legacy" mode, so I'm not willing to use that option, but I would like to be able to zoom with my external mouse.

    I would like to suggest the following: I have gotten very used to how Adobe allows zooming in the Creative Suite (I'm using version 3). While you press alt (option), and scroll, it zooms instead of scrolling. This would probably be a simple addition, and would greatly enhance usability when using an external mouse, and/or don't have pinch to zoom available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    The only way that I found to use zooming and panning simultaneously with the magic mouse in OSX is to activate the "Legacy mouse mode" in the Eaglecad 6.1.0 prefs and also install this app http://dangerousprototypes.com/forum/viewtopic.php?f=19&t=2097#p20115 called "Mouse Assistant" which let you the possibility to press shift key and clicking mouse to do panning simulating the "middle click" in OSX. Is also usefull for me with other apps like Sketchup.
    I hope it helps

    The only way that I found to use zooming and panning simultaneously with the magic mouse in OSX is to activate the "Legacy mouse mode" in the Eaglecad 6.1.0 prefs and also install this app http://dangerousprototypes.com/forum/viewtopic.php?f=19&t=2097#p20115 called "Mouse Assistant" which let you the possibility to press shift key and clicking mouse to do panning simulating the "middle click" in OSX. Is also usefull for me with other apps like Sketchup.

     

    I hope it helps  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I know it was fixed in 6.0.2 beta, but just in case anyone didn't try it, it's fixed in 6.1.0 (which has just been made available).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to intellijel

    On 2011-12-18 23:31:12 +0000, Danjel van Tijn said:

     

    I am not sure how this is considered an acceptable release for V6.0.

    Without zoom functionality it is totally useless. How could this have

    been tested on an OS X machine and passed?

     

    Can I also echo these sentiments.

     

    How on earth you decided to remove such key functionality is beyond me.

    As someone who switches between OS X and Linux regularly, having to

    cope with two different UI's would be ridiculous.  Thankfully you have

    an option to revert to the old behaviour.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 12/24/2011 4:34 PM, Jason Tribbeck wrote:

    Right - I've tried it in 6.0.2, and the legacy mode does seem to work.

     

    Unfortunately, there's still the issues of manual routing and the current bend/via selection not being displayed (which I've curiously not had any feedback from anyone in an official capacity yet)...

     

     

    Hi Jason,

     

    This is Jorge, sorry about that. I've actually been trying to figure out

    a nice way to illustrate the issue so that it could be resolved. I'm

    going to go to the original thread now so we can get this worked out.

     

    hth,

    Jorge

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Right - I've tried it in 6.0.2, and the legacy mode does seem to work.

     

    Unfortunately, there's still the issues of manual routing and the current bend/via selection not being displayed (which I've curiously not had any feedback from anyone in an official capacity yet)...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    warrenbrayshaw wrote on Thu, 22 December 2011 18:04

    I wrote 70 words to provide the poster with knowledge and

    understanding.

     

    No, you just wanted to push your own viewpoint of how you think things

    should be by pretending that's how they are.

     

    Quote:

    If I hadn't used the one word 'official' then  possibly you would not

    have

    responded with  401 words.

     

    You actually counted!?  Somebody needs to get a life.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    warrenbrayshaw wrote on Thu, 22 December 2011 15:29

    >> You post at Element14 which acts as a web portal to nntp

    >> 'news.cadsoft.de',

    >> the core (official) forum point.

     

    Olin Lathrop wrote:

     

     

    Clearly it's not.  Element14 is run by the owners of Cadsoft and the

    Eagle software.  The web forum is a self-contained community with a

    gateway to the old NNTP newsgroup.  Neither is more official or

    "right" than the other.  Unfortunately the gateway at element14 that

    tries to translate forum posts to newgroup messages and vice versa

    isn't what it could be, although it has been getting better and there

    seems to be real commitment lately by Farnell to make it better.

     

    Alex, there are a lot of old timers who don't like the element14

    forums because it upsets and threatens their world..........

     

     

    Thanks for the pre-Christmas entertainment Olin.

     

    I wrote 70 words to provide the poster with knowledge and understanding.

    If I hadn't used the one word 'official' then  possibly you would not have

    responded with  401 words.

     

    I used 'official' because I recall that was stated  by a CadSoft staffer,

    since Element14 kicked off.

     

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    warrenbrayshaw wrote on Thu, 22 December 2011 15:29

    You post at Element14 which acts as a web portal to nntp

    'news.cadsoft.de',

    the core (official) forum point.

     

    Clearly it's not.  Element14 is run by the owners of Cadsoft and the Eagle

    software.  The web forum is a self-contained community with a gateway to

    the old NNTP newsgroup.  Neither is more official or "right" than the

    other.  Unfortunately the gateway at element14 that tries to translate

    forum posts to newgroup messages and vice versa isn't what it could be,

    although it has been getting better and there seems to be real commitment

    lately by Farnell to make it better.

     

    Alex, there are a lot of old timers who don't like the element14 forums

    because it upsets and threatens their world.  The more people use e14 and

    the more features get added there, the less relevant the newgroup becomes.

    I think they fear that eventually the newgroup will be abandoned as the

    vast majority of users abandon it.  That may be a realistic fear, although

    there is little technical reason both couldn't exist with a good gateway

    inbetween.

     

    Don't let anyone tell you what you should use or that one is more

    "official" than the other.  Some of the old time Cadsoft staff prefer the

    newsgroup, but implying they won't look at the forums is just a weak

    argument to try to elevate the importance of newsgroup over the forum.

    Farnell owns Cadsoft now, and of course they own e14.  I really can't

    imagine they will allow their Cadsoft division to ignore data that exists

    only on the e14 forums.

     

    So continue to do what is most comfortable to you.  Cadsoft is not in a

    position to ignore the e14-only users since there are a great many of them.

    Keep in mind that the newsgroup exists and that some people therefore may

    not get all information posted on e14.  Take that for what it's worth and

    how much trouble you're willing to go thru for those people using the

    newsgroup feed.  They are a minority, but are also the experienced old

    timers for now.  Eventually there will be more experienced people on the

    forums, but that seems not to be the case at present.  However, don't let

    anyone try to misrepresent the newgroup as being the "official" place or

    whatever, or suggest that you are in the wrong place.

     

    If you find this situation uncomfortable, the most productive course of

    action is probably to complain to the e14 folks to bring the gateway to the

    newgroup to a higher level.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>