Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Scroll wheel with Eagle 6 on Mac
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 191 subscribers
  • Views 3221 views
  • Users 0 members are here
  • mac
  • zoom
  • mouse
Related

Scroll wheel with Eagle 6 on Mac

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I've just upgraded to Eagle 6 (I'm looking forward to  indexing the XML format files for my search engine!) - however, I can't  get the scroll wheel to work.

 

It's enabled in the options (User Interface -> Mouse wheel zoom = 1.2), but it does absolutely nothing.

 

If I load Eagle 5.11, it works fine.

 

Note that setting the zoom to 0 doesn't allow me to scroll around either.

 

This happens with both of my mice (wired and wireless mighty mouse).

 

Any ideas?

 

BTW, I'm glad the bug where my ULPs to set the print zoom, mirror, black and so forth has been fixed since 5.11 - although I still can't use the Cmd-<n> keys to switch between the windows.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to alexwhittemore

    Alex Whittemore wrote:

    No no, you're correct, see my edit. That IS the intended and

    desirable behavior. Like I said, the only problem is that on the old

    style trackpad, zoom isn't tied to any physical gesture or button. So

    the switch you implemented in the beta is perfect.

     

    FYI Alex

     

    You post at Element14 which acts as a web portal to nntp 'news.cadsoft.de',

    the core (official) forum point.

      'edits' and 'inline' images do not reach the nntp which is the 'goto

    place' for cadsoft staff.

     

    So do not 'edit', just reply to your posting and when passing an image, use

    the attach method which does get through.

    A fix for the 'inline' images is promised soon.

     

    HTH

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • alexwhittemore
    alexwhittemore over 14 years ago in reply to kcadsoft

    No no, you're correct, see my edit. That IS the intended and desirable behavior. Like I said, the only problem is that on the old style trackpad, zoom isn't tied to any physical gesture or button. So the switch you implemented in the beta is perfect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kcadsoft
    kcadsoft over 14 years ago in reply to alexwhittemore

    On 19.12.2011 21:54, Alex Whittemore wrote:

    ...

    Klaus: I finally got around to testing this at work where I HAVE a magic trackpad (external) and it still doesn't work as intended. Two finger swipes on the external multitouch trackpad behave in exactly the same way as two finger swipes on the built-in non-multiouch trackpad (which is, they scroll left/right when the view is zoomed in enough that it doesn't all fit on one screen).

     

    But that is the intended behavior, isn't it?

    Two finger swipes on the Magic Trackpad scroll (or "pan") a scrollable

    window left/right and up/down. It's the same as, for instance, in

    the Safari browser.

    Or am I missing something?

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • alexwhittemore
    alexwhittemore over 14 years ago in reply to intellijel

    I also had problems with this, and the beta mentioned works fine (switches between old=works method and new=doesn't method). However, I'd like to update with new info for Klaus.

     

    Klaus: I finally got around to testing this at work where I HAVE a magic trackpad (external) and it still doesn't work as intended. Two finger swipes on the external multitouch trackpad behave in exactly the same way as two finger swipes on the built-in non-multiouch trackpad (which is, they scroll left/right when the view is zoomed in enough that it doesn't all fit on one screen).

     

    EGAD: Pardon me, just a case of user error. I'm not used to pan/zoom enough. Zoom does work, and pan works once zoomed in enough.

     

    So obviously, the only thing missing from the normal non-multitouch trackpad is zoom. So the switch, as implemented in the beta, is perfect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • intellijel
    intellijel over 14 years ago in reply to e14 Contributor

    I am not sure how this is considered an acceptable release for V6.0. Without zoom functionality it is totally useless. How could this have been tested on an OS X machine and passed?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Can someone clarify the Magic Mouse gesture behavior in v6.0? I couldn't find it in the help documentation. I really like how you pan using the touch surface, but I haven't been able to figure out how to zoom. I've tried holding the Command key while using a single finger up/down motion and also a two finger up/down gesture, but neither worked. Is it no longer possible to zoom without clicking on the zoom button or using F3? Mind you, I don't want to revert back to the old behavior, as I really prefer being able to pan using the mouse surface, I'd just like to be able to zoom somehow too.

     

    mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kcadsoft
    kcadsoft over 14 years ago in reply to e14 Contributor

    On 12/15/11 11:59, Jason Tribbeck wrote:

    Hi,

     

    Many thanks for the reply. I'll look on the beta releases.

     

    Does this mean if I had a track-pad, or the new mouse, it would work fine?

     

    It means that you can switch between the way things were done

    in version 5 and the new method that tries to implement the

    new two-finger-pan-gestures as used in Mac OS X 10.7. With

    a MagicTrackpad these work really nice.

     

    I do have a "Contour Design ShuttleXpress", which, after I'd posted my message, I configured the central jog wheel to send Shift-F3 and Shift-F4, and made these keys use "Window 1.2" and "Window 0.8333333" which zooms a bit - although it's central to the screen, rather than the mouse pointer position. Is there a way to get the Window command to use the mouse pointer, rather than the screen? This would be a closer workaround.

     

    You can use

     

       WINDOW (@);

     

    to move the point at the current mouse position to the

    center of the editor window. But I'm not sure if this

    will actually help here. I'm afraid simulating what the

    mouse wheel does by means of command line entries can't be

    done.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to kcadsoft

    Hi,

     

    Many thanks for the reply. I'll look on the beta releases.

     

    Does this mean if I had a track-pad, or the new mouse, it would work fine?

     

    I do have a "Contour Design ShuttleXpress", which, after I'd posted my message, I configured the central jog wheel to send Shift-F3 and Shift-F4, and made these keys use "Window 1.2" and "Window 0.8333333" which zooms a bit - although it's central to the screen, rather than the mouse pointer position. Is there a way to get the Window command to use the mouse pointer, rather than the screen? This would be a closer workaround.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kcadsoft
    kcadsoft over 14 years ago

    On 12/14/11 20:29, Jason Tribbeck wrote:

    Hi,

     

    I've just upgraded to Eagle 6 (I'm looking forward to  indexing the XML format files for my search engine!) - however, I can't  get the scroll wheel to work.

     

    It's enabled in the options (User Interface ->  Mouse wheel zoom = 1.2), but it does absolutely nothing.

     

    If I load Eagle 5.11, it works fine.

     

    Note that setting the zoom to 0 doesn't allow me to scroll around either.

     

    This happens with both of my mice (wired and wireless mighty mouse).

     

    Any ideas?

     

    The next beta version 6.0.1 will have a switch in "Options/User interface"

    named "Legacy mouse wheel mode" that can be selected to switch back

    to the old mouse wheel handling under Mac OS X.

    Please watch the eagle.betatest newsgroup for the announcement of version 6.0.1.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<