somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires
5.11 didnt do this... i have messed with alot of settings, nothing seems to help
somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires
5.11 didnt do this... i have messed with alot of settings, nothing seems to help
Am 16.12.2011 18:55, schrieb Mitch Solomon:
somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires
5.11 didnt do this... i have messed with alot of settings, nothing seems to help
Gentlemen, so far I have followed all this postings and noticed that
there is is very little information about what machine and operating
system you are using.
I think to mention this would be a great help for cadsoft in eliminating
these errors.
I don't have this error on my windows xp sp3.
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
Am 16.12.2011 18:55, schrieb Mitch Solomon:
somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires
5.11 didnt do this... i have messed with alot of settings, nothing seems to help
Gentlemen, so far I have followed all this postings and noticed that
there is is very little information about what machine and operating
system you are using.
I think to mention this would be a great help for cadsoft in eliminating
these errors.
I don't have this error on my windows xp sp3.
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
On 12/01/2012 13:36, Joern Paschedag wrote:
Am 16.12.2011 18:55, schrieb Mitch Solomon:
>> somethings changed, when i manually route and click on the destination
>> pad, if i dont click dead center now... im left with tiny tiny airwires
>> 5.11 didnt do this... i have messed with alot of settings, nothing
>> seems to help
>>
>
Gentlemen, so far I have followed all this postings and noticed that
there is is very little information about what machine and operating
system you are using.
I think to mention this would be a great help for cadsoft in eliminating
these errors.
I don't have this error on my windows xp sp3.
Using the files linked-to in this thread I can reproduce the fault under
Eagle 6.0.0 and Eagle 6.0.2 in Windows 7 x64.
I was also seeing this leftover airwires problem on Linux x64 (but with
a different (production!) board) using 6.0.0.
The exchange of messages in this thread, between Jorge Garcia and Jason
Tribbeck, suggests that the developers have all they need to be able to
reproduce this.
Hopefully 6.1 will nail it. Hopefully soon!
Andrew
0xADF