Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) in V6.0.0 manual routing got really hard
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 190 subscribers
  • Views 4688 views
  • Users 0 members are here
Related

in V6.0.0 manual routing got really hard

e14 Contributor
e14 Contributor over 14 years ago

somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires

5.11 didnt do this... i have messed with alot of settings, nothing seems to help

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 1/13/2012 7:08 AM, Andrew Feldhaus wrote:

    On 13/01/2012 11:19, Jason Tribbeck wrote:

    >> Oh. Maybe I was a bit hasty in thinking that my example worked

    >> then...

    >>

    >> I was using the bend style 0 (I think - Mac OS STILL doesn't show

    >> the current bend state), and while I didn't click to finish it, it

    >> did appear to snap.

    >

    >> I'll re-verify this tonight then.

    >>

    >

    According to Walter Spermann in eagle.betatest (replying to the thread

    "Possible routing bug"):

     

    On 13/01/2012 11:06, wsp@cadsoft.de wrote:

    > We fixed this meanwhile, but it's not included in 6.1 yet.

    > It'll go into next beta (6.1.1).

     

    So hopefully Cadsoft have squashed this bug and the fix will be out soon.

     

    >

    Andrew

    0xADF

     

    Thanks Andrew,

     

    I was about to quote Walter as well. The fix for this bug didn't make it

    into this release but it will be in the next beta 6.1.1.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 13/01/2012 11:19, Jason Tribbeck wrote:

    Oh. Maybe I was a bit hasty in thinking that my example worked

    then...

     

    I was using the bend style 0 (I think - Mac OS STILL doesn't show

    the current bend state), and while I didn't click to finish it, it

    did appear to snap.

    >

    I'll re-verify this tonight then.

     

     

    According to Walter Spermann in eagle.betatest (replying to the thread

    "Possible routing bug"):

     

    On 13/01/2012 11:06, wsp@cadsoft.de wrote:

    > We fixed this meanwhile, but it's not included in 6.1 yet.

    > It'll go into next beta (6.1.1).

     

    So hopefully Cadsoft have squashed this bug and the fix will be out soon.

     

     

    Andrew

    0xADF

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Oh. Maybe I was a bit hasty in thinking that my example worked then...

     

    I was using the bend style 0 (I think - Mac OS STILL doesn't show the current bend state), and while I didn't click to finish it, it did appear to snap.

     

    I'll re-verify this tonight then.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 13/01/2012 08:16, Jason Tribbeck wrote:

    Ok, im testing the new version 6.1.0 right now.

    > The problem still exists in my opinion.

     

    I agree.  I have tested 6.1.0 in Windows 7 x64 with the example project

    you kindly posted earlier in this thread -

    http://www.tribbeck.com/misc/Test5_11_0.zip

     

    Steps to reproduce:

     

    Load Example.brd

    ROTATE =MR45 Q1

    ROUTE

    Click SV1 pad 1 to start routing*

    Hover over Q1 pad 1

    The end of the track being placed does not snap to the target pad.

    Hit 'Esc' to cancel the current routing operation

    Click SV1 pad 1 to try again

    Hover over Q1 pad 1

    Now the track snaps to the pin as it should.

     

     

    There are various other situations where the routed track fails to snap

    to the target pad, but the steps above seem to work consistently for me.

     

    Andrew

    0xADF

     

     

    • I'm  a 25mil grid and Wire_Bend style '1' (horizontal-then-45-degree)

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Przemyslaw Zur wrote:

     

    Ok, im testing the new version 6.1.0 right now. The problem still exists in my opinion.

    When trying to route im pulling a connection from one pad to another, at the other pad the connection just doesn't "snap". However when You press esc button and try to route once more TADA it connects like a charm. What gives? When you move a elemenet and try to connect it again the problem still remains... press ESC and you can connect with noproblems. Come on I started projects in v6 I can't go back to 5. FIX THIS please.

    That's a shame. I only tried it on my example that I provided earlier, and it worked (I had to get up early today, so didn't have any time to play).

     

    It's possible that they've only used my example and not actually used it after fixing that example.

     

    I'll have more time over the weekend to give it a more thorough test. And if it's not working, I'll come up with another example.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Ok, im testing the new version 6.1.0 right now. The problem still exists in my opinion.

    When trying to route im pulling a connection from one pad to another, at the other pad the connection just doesn't "snap". However when You press esc button and try to route once more TADA it connects like a charm. What gives? When you move a elemenet and try to connect it again the problem still remains... press ESC and you can connect with noproblems. Come on I started projects in v6 I can't go back to 5. FIX THIS please.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Sorry for not writing about about OS that I use. The broblem I think is platform and OS independent. I notised that the same problem occurs On Windows XP SP3, Windows 7 32bit Vista 64bit.

    I haven't tested the version 6.1 yet hope it works better (fingers crossed).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to dukepro

    Hi Chuck,

     

    By default, you should receive email notifications for any discussion thread that you have posted in.  On this page, there is a Actions widget near the top on the right hand side where you can disable email notifications for this thread.  Additionally, you can view all your email notifications and disable as desired by clicking 'Manage email notifications' in the Actions widget on your profile page.

     

    There had been an issue with delivery of email from element14 that impacted some users.  This issue was resolved recently, and, thus, you may now be receiving notifications that you had not previously.

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 14 years ago in reply to e14 Contributor

    Why am I suddenly receiving email copies of posts?

     

     

    On 01/12/2012 01:49 PM, Jason Tribbeck wrote:

    Just downloaded 6.1.0, and my test example isn't failing as before.

     

    So, 6.1.0 looks like it may have fixed it (I'll need to do some more tests though).

     

    Yay!

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Just downloaded 6.1.0, and my test example isn't failing as before.

     

    So, 6.1.0 looks like it may have fixed it (I'll need to do some more tests though).

     

    Yay!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>