Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) in V6.0.0 manual routing got really hard
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 190 subscribers
  • Views 4650 views
  • Users 0 members are here
Related

in V6.0.0 manual routing got really hard

e14 Contributor
e14 Contributor over 14 years ago

somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires

5.11 didnt do this... i have messed with alot of settings, nothing seems to help

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Sorry for not writing about about OS that I use. The broblem I think is platform and OS independent. I notised that the same problem occurs On Windows XP SP3, Windows 7 32bit Vista 64bit.

    I haven't tested the version 6.1 yet hope it works better (fingers crossed).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Sorry for not writing about about OS that I use. The broblem I think is platform and OS independent. I notised that the same problem occurs On Windows XP SP3, Windows 7 32bit Vista 64bit.

    I haven't tested the version 6.1 yet hope it works better (fingers crossed).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Ok, im testing the new version 6.1.0 right now. The problem still exists in my opinion.

    When trying to route im pulling a connection from one pad to another, at the other pad the connection just doesn't "snap". However when You press esc button and try to route once more TADA it connects like a charm. What gives? When you move a elemenet and try to connect it again the problem still remains... press ESC and you can connect with noproblems. Come on I started projects in v6 I can't go back to 5. FIX THIS please.