Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Moving a package reference point - custom library edit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 506 views
  • Users 0 members are here
Related

Moving a package reference point - custom library edit

e14 Contributor
e14 Contributor over 14 years ago

Greetings all - I have not been able to find the answer to this - when I

copy/paste a package

into a new package (that I am going to edit to make a new package based on

the old one),

when you "paste" it into the library window, you can move it around to put

it where you want

it on the reference "+" for the package (and use the "alt" key to get finer

resolution).  If you

don't manage to get it where you want it etc, is there a way to move that

reference point

in the component (to get it on the same grid for example) or do you have to

start over

again - pointers to where that is documented in the manual are fine - I was

not able to

discover the answer to this one

 

Thanks !!

--

 

Mikey aka "mr.gadget"

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    "Mike Fields" <spam_me_not_mr.gadget2@comcast.net> wrote in message

    news:jcmnsg$o56$1@cheetah.cadsoft.de...

    Greetings all - I have not been able to find the answer to this - when I

    copy/paste a package

    into a new package (that I am going to edit to make a new package based on

    the old one),

    when you "paste" it into the library window, you can move it around to put

    it where you want

    it on the reference "+" for the package (and use the "alt" key to get

    finer resolution).  If you

    don't manage to get it where you want it etc, is there a way to move that

    reference point

    in the component (to get it on the same grid for example) or do you have

    to start over

    again - pointers to where that is documented in the manual are fine - I

    was not able to

    discover the answer to this one

     

    Thanks !!

     

    Mikey aka "mr.gadget"

     

     

    Perhaps a different part of the same question is - when I dropped a package

    into a new window with the mouse click (copy/paste), it ended up with

    everything on a grid offset by .05  (.15, .25 etc) is there an easy way to

    move the package to align with the 0.1 inch grid instead of being offset by

    0.5" ?  If the answer is obvious, please point me to the doc - I am more

    than

    happy to read !!

     

    mikey

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Mike Fields schrieb:

     

    >> Greetings all - I have not been able to find the answer to this - when I

    >> copy/paste a package

    >> into a new package (that I am going to edit to make a new package based on

    >> the old one),

    >> when you "paste" it into the library window, you can move it around to put

    >> it where you want

    >> it on the reference "+" for the package (and use the "alt" key to get

    >> finer resolution).  If you

    >> don't manage to get it where you want it etc, is there a way to move that

    >> reference point

    >> in the component (to get it on the same grid for example) or do you have

    >> to start over

    >> again - pointers to where that is documented in the manual are fine - I

    >> was not able to

    >> discover the answer to this one

     

    First GROUP everything, then simply MOVE it.

     

    Perhaps a different part of the same question is - when I dropped a package

    into a new window with the mouse click (copy/paste), it ended up with

    everything on a grid offset by .05  (.15, .25 etc) is there an easy way to

    move the package to align with the 0.1 inch grid instead of being offset by

    0.5" ?  If the answer is obvious, please point me to the doc - I am more

    than happy to read !!

     

    Select the proper reference coordinate after COPY (CUT with V5) and/or

    PASTE it to a useful position.

    If you let EAGLE automatically choose the reference coordinate, it will

    be centered and thus often will be exactly half-grid (depending on the

    package).

     

    Take a look into HELP and the manual on how to exactly use these

    commands and their options.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

     

    --

     

    Mikey aka "mr.gadget"

    Retirement is not all that it's cracked up to be

                  ( It's actually much better. )

    Retirement is a gift of time - Don't waste it!

      ---

     

    "Tilmann Reh" <usenet2007nospam@autometer.de> wrote in message

    news:jcmrd2$c68$1@cheetah.cadsoft.de...

    Mike Fields schrieb:

     

    >>> Greetings all - I have not been able to find the answer to this - when I

    >>> copy/paste a package

    >>> into a new package (that I am going to edit to make a new package based

    >>> on

    >>> the old one),

    >>> when you "paste" it into the library window, you can move it around to

    >>> put

    >>> it where you want

    >>> it on the reference "+" for the package (and use the "alt" key to get

    >>> finer resolution).  If you

    >>> don't manage to get it where you want it etc, is there a way to move

    >>> that

    >>> reference point

    >>> in the component (to get it on the same grid for example) or do you have

    >>> to start over

    >>> again - pointers to where that is documented in the manual are fine - I

    >>> was not able to

    >>> discover the answer to this one

     

    First GROUP everything, then simply MOVE it.

     

    >> Perhaps a different part of the same question is - when I dropped a

    >> package

    >> into a new window with the mouse click (copy/paste), it ended up with

    >> everything on a grid offset by .05  (.15, .25 etc) is there an easy way

    >> to

    >> move the package to align with the 0.1 inch grid instead of being offset

    >> by

    >> 0.5" ?  If the answer is obvious, please point me to the doc - I am more

    >> than happy to read !!

     

    Select the proper reference coordinate after COPY (CUT with V5) and/or

    PASTE it to a useful position.

    If you let EAGLE automatically choose the reference coordinate, it will

    be centered and thus often will be exactly half-grid (depending on the

    package).

     

    Take a look into HELP and the manual on how to exactly use these

    commands and their options.

     

    Tilmann

     

    OK, thanks - that was basically what I ended up doing - by using the ALT

    key, I can

    place the grouped object on the finer grid which (as you pointed out) is

    often off by

    1/2 a grid line.  I was used to other cad type programs etc where you can

    hold

    down the CTL key for example which temporarily turns off the "snap to grid"

    and

    you can place the object exactly as wanted.

     

    One warning for others experimenting with version 6 and 5 at the same time -

    if

    you have defined multiple library paths (as suggested by Cadsoft) that use

    the

    installed library as well as one you have defined in another path, when you

    install the two versions, while the two versions get installed in separate

    paths,

    apparently, the library paths are in the registry since version 6 comes up

    looking at the same extra user defined library even though I did not tell 6

    that

    I had an extra library path. (my test library is now version 6 only - it got

    converted).

     

    mikey

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

     

    --

     

    Mikey aka "mr.gadget"

    Retirement is not all that it's cracked up to be

                  ( It's actually much better. )

    Retirement is a gift of time - Don't waste it!

      ---

     

    "Tilmann Reh" <usenet2007nospam@autometer.de> wrote in message

    news:jcmrd2$c68$1@cheetah.cadsoft.de...

    Mike Fields schrieb:

     

    >>> Greetings all - I have not been able to find the answer to this - when I

    >>> copy/paste a package

    >>> into a new package (that I am going to edit to make a new package based

    >>> on

    >>> the old one),

    >>> when you "paste" it into the library window, you can move it around to

    >>> put

    >>> it where you want

    >>> it on the reference "+" for the package (and use the "alt" key to get

    >>> finer resolution).  If you

    >>> don't manage to get it where you want it etc, is there a way to move

    >>> that

    >>> reference point

    >>> in the component (to get it on the same grid for example) or do you have

    >>> to start over

    >>> again - pointers to where that is documented in the manual are fine - I

    >>> was not able to

    >>> discover the answer to this one

     

    First GROUP everything, then simply MOVE it.

     

    >> Perhaps a different part of the same question is - when I dropped a

    >> package

    >> into a new window with the mouse click (copy/paste), it ended up with

    >> everything on a grid offset by .05  (.15, .25 etc) is there an easy way

    >> to

    >> move the package to align with the 0.1 inch grid instead of being offset

    >> by

    >> 0.5" ?  If the answer is obvious, please point me to the doc - I am more

    >> than happy to read !!

     

    Select the proper reference coordinate after COPY (CUT with V5) and/or

    PASTE it to a useful position.

    If you let EAGLE automatically choose the reference coordinate, it will

    be centered and thus often will be exactly half-grid (depending on the

    package).

     

    Take a look into HELP and the manual on how to exactly use these

    commands and their options.

     

    Tilmann

     

    OK, thanks - that was basically what I ended up doing - by using the ALT

    key, I can

    place the grouped object on the finer grid which (as you pointed out) is

    often off by

    1/2 a grid line.  I was used to other cad type programs etc where you can

    hold

    down the CTL key for example which temporarily turns off the "snap to grid"

    and

    you can place the object exactly as wanted.

     

    One warning for others experimenting with version 6 and 5 at the same time -

    if

    you have defined multiple library paths (as suggested by Cadsoft) that use

    the

    installed library as well as one you have defined in another path, when you

    install the two versions, while the two versions get installed in separate

    paths,

    apparently, the library paths are in the registry since version 6 comes up

    looking at the same extra user defined library even though I did not tell 6

    that

    I had an extra library path. (my test library is now version 6 only - it got

    converted).

     

    mikey