Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 6.0 crashes when deletibg a net ... sometimes
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 189 subscribers
  • Views 2623 views
  • Users 0 members are here
  • eagle
  • crash
  • bug
  • schematic
Related

Eagle 6.0 crashes when deletibg a net ... sometimes

wayne2056
wayne2056 over 14 years ago

Here is a capture of an error I have received a number of times now.  It occurs occasionally when I delete a net.

After you click OK the program crashes and all work prior to last save is lost..

 

 

 

image

  • Sign in to reply
  • Cancel
Parents
  • scottyhomer
    scottyhomer over 14 years ago

    I am also hitting this problem with Eagle 6.0.0 on Linux.  It only seems to hit specific nets, and it is extremely consistent about aborting on deleting those nets.  Steps to recreate the problem are simple - Start a new schematic.  Add a component (DS1307 for example).  Run a wire from pin 8 out 1 and up 1 ( a right-angle wire).  Add a VCC symbol to the end of that wire.  Add junction dots where the wire meets pin 8 and the VCC symbol.  Delete the vertical segment of the wire.  Now delete the horizontal segment.  It will abort every time at this point.  Alternatively, you can delete the horizontal segment of the wire first (successfully), and then have it fail when you try to delete the vertical segment.  It only happens if you have the junctions.  If you never add the junctions, then it doesn't fail.

     

    It doesn't seem to matter what symbols/components are involved.  The main things are that the wire has a right-angle bend, and that the junction dots are in place.  So far it only seems to happen with wires, not parts.  But even if I delete the part, deleting the remaining wire(s) cause the problem.

     

    As you can see in the picture, both wires were deleted from the image, but the crash happened immediately after the horizontal wire was removed from the schematic.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to scottyhomer

    Also happens on MacOS too, so probably happens on Windows as well (just read the original posted message, so definitely so!)

     

    Although I've never seen the point of junction dots at those locations myself image Seems a bit ... superflouous...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to scottyhomer

    Also happens on MacOS too, so probably happens on Windows as well (just read the original posted message, so definitely so!)

     

    Although I've never seen the point of junction dots at those locations myself image Seems a bit ... superflouous...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Just confirmed that my test sequence doesn't fail in 6.1.0.

     

    I'm guessing this was the problem:

     

    - Fixed a crash if deleting a group containing a net wire and a junction in special constellation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 1/5/2012 1:41 PM, Jason Tribbeck wrote:

    Okay - here's a short video on reproducing it:

     

    >

     

    http://www.youtube.com/watch?v=sLp8WIgC-bY

     

    And an Eagle 6.0.0 file is available from http://www.tribbeck.com/misc/TakeObject.sch.zip

     

     

    Awesome Jason,

     

    Our developers really appreciate this, and I'm positive your fellow

    EAGLE brethren appreciate it even more.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Okay - here's a short video on reproducing it:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    http://www.youtube.com/watch?v=sLp8WIgC-bY

     

    And an Eagle 6.0.0 file is available from http://www.tribbeck.com/misc/TakeObject.sch.zip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to billpenner

    On 03.01.2012 21:58, billpenner wrote:

    The error is created when a junction is placed on a pin manually.  It will happen with either a wire or a net. Use net instead of wire. It works for me. Hope it will for you.

    Bill.

     

     

    I can't reproduce this. It's possible to place junctions manually on

    nets pin connections, not matter whether I use NET or WIRE.

    Using SuSE 12.1

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billpenner
    billpenner over 14 years ago in reply to e14 Contributor

    The error is created when a junction is placed on a pin manually.  It will happen with either a wire or a net. Use net instead of wire. It works for me. Hope it will for you.

    Bill.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Do you use NET or WIRE? With net the junctions are placed automatically. See

    the manual/online-help for details.

    r

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Guest wrote:

     

    Am 02.01.2012 15:34, schrieb Jason Tribbeck:

    Also happens on MacOS too, so probably happens on Windows as well.

     

    Although I've never seen the point of junction dots at those locations myself image Seems a bit ... superflouous...

     

     

    No crashes on my windows xp. Are those junctions placed by hand?

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    Yes - you need to manually create them (which is why I've never seen it crash, as I never create joins manually).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 02.01.2012 15:34, schrieb Jason Tribbeck:

    Also happens on MacOS too, so probably happens on Windows as well.

     

    Although I've never seen the point of junction dots at those locations myself image Seems a bit ... superflouous...

     

     

    No crashes on my windows xp. Are those junctions placed by hand?

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag