I cannot figure out how to use meander, can anyone help! If I have 2 traces, 1 trace is 5 inches, and the other is 4 inches, how do I make the second trace 5 inches long?
I cannot figure out how to use meander, can anyone help! If I have 2 traces, 1 trace is 5 inches, and the other is 4 inches, how do I make the second trace 5 inches long?
Hi Craig,
simply invoke Meander with parameter giving the desired length (here 5 in), click on the shorter track and the window with desired length and the actual percentage of itappears. Now simply move the pointer to place the meander as desired. Well desribed in help.
I am confused, I click on the meander icon, and there is no popup for a desired length? How do I enter the parameter?
I am confused, I click on the meander icon, and there is no popup for a desired length? How do I enter the parameter?
You can simplu type the length after selecting the command (same way as with for example wire width while routing). I am using text commands, not the icons, but with icon it works the same way - click on icon, then type the parameter.
Craig Beiferman wrote:
I am confused, I click on the meander icon, and there is no popup for
a desired length? How do I enter the parameter?
Hmmm! Does it not work how the manual describes?
Manual is found in the doc folder of your installation.
HTH
Warren
--
Viewed / responded via the newsgroup at
news.cadsoft.de