Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Magnetic attach while manually routing
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 750 views
  • Users 0 members are here
Related

Magnetic attach while manually routing

e14 Contributor
e14 Contributor over 14 years ago

Hello

 

There seems to be a problem in v6.1 Layout Editor. The mechanism for

automatically attaching a track to a near pad or track frequently does

not work even when very close. I have noticed that when the problem

occurs, if I undo the track which I have just laid and then try again

then the mechanism usually works fine.  It is as though something is

being disabled.

 

A second similar but possibly unrelated problem occurs in the Schematic

Editor. When a component is Cut into the Past buffer and then Pasted so

that it has a terminal end on the end of an existing wire the terminal

fails to join to the wire.  However if a similar operation is performed

using the Copy command then the component terminal joins correctly.

 

Regards

Stephen Dickinson

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Il 24/01/2012 11:52, Stephen Dickinson ha scritto:

     

    A second similar but possibly unrelated problem occurs in the Schematic

    Editor. When a component is Cut into the Past buffer and then Pasted so

    that it has a terminal end on the end of an existing wire the terminal

    fails to join to the wire. However if a similar operation is performed

    using the Copy command then the component terminal joins correctly.

     

     

    Yes, I confirm this behavior. In my experience the join will fail

    because the component is moved away if it has one or more pin on the end

    of existing wire. You have to select again the component(s) and move

    another time at the desired position.

     

    I'm going to try the beta.... sigh

     

    Marco

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    This is a really irritating bug, when will the fix be released? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 24/01/2012 10:52, Stephen Dickinson wrote:

    There seems to be a problem in v6.1 Layout Editor. The mechanism for

    automatically attaching a track to a near pad or track frequently does

    not work even when very close. I have noticed that when the problem

    occurs, if I undo the track which I have just laid and then try again

    then the mechanism usually works fine. It is as though something is

    being disabled.

     

    This is a known issue which Cadsoft has said is fixed in Beta 6.1.1 --

    the "in V6.0.0 manual routing got really hard" thread has more details

    about the bug.  Hopefully this beta will be released soon.

     

    I can't shed any light on your second problem, though.

     

     

    Andrew

    0xADF