Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Magnetic attach while manually routing
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 753 views
  • Users 0 members are here
Related

Magnetic attach while manually routing

e14 Contributor
e14 Contributor over 14 years ago

Hello

 

There seems to be a problem in v6.1 Layout Editor. The mechanism for

automatically attaching a track to a near pad or track frequently does

not work even when very close. I have noticed that when the problem

occurs, if I undo the track which I have just laid and then try again

then the mechanism usually works fine.  It is as though something is

being disabled.

 

A second similar but possibly unrelated problem occurs in the Schematic

Editor. When a component is Cut into the Past buffer and then Pasted so

that it has a terminal end on the end of an existing wire the terminal

fails to join to the wire.  However if a similar operation is performed

using the Copy command then the component terminal joins correctly.

 

Regards

Stephen Dickinson

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 24/01/2012 10:52, Stephen Dickinson wrote:

    There seems to be a problem in v6.1 Layout Editor. The mechanism for

    automatically attaching a track to a near pad or track frequently does

    not work even when very close. I have noticed that when the problem

    occurs, if I undo the track which I have just laid and then try again

    then the mechanism usually works fine. It is as though something is

    being disabled.

     

    This is a known issue which Cadsoft has said is fixed in Beta 6.1.1 --

    the "in V6.0.0 manual routing got really hard" thread has more details

    about the bug.  Hopefully this beta will be released soon.

     

    I can't shed any light on your second problem, though.

     

     

    Andrew

    0xADF

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    This is a really irritating bug, when will the fix be released? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    This is a really irritating bug, when will the fix be released?