EAGLE User Support (English) Eagle 6.1 Crashes trying to make Gerber Output
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
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 399 views
  • Users 0 members are here
  • eagle
  • crash
  • output
  • bug
  • gerber
Related

Eagle 6.1 Crashes trying to make Gerber Output

Former Member
Former Member over 14 years ago

I am trying to get a board out to be fabbed and frelling new Eagle keeps crashing when I try and create the gerber output.

 

I am using Eagle 6.1.0 under Windows 7 x 64 Pro.   The CAM file device I have selected is GERBER_RS274X. 

 

When I press the Process Job button the CAM starts to make output, the .gpi and .gbr files are created in

the directory, but they are zero bytes and then the program crashed and closes.   If I use the Process Section

button I get the same result.

 

I am a long time user of Eagle under windows (from version 4 on) so I think I know what I am doing with the software.

 

I hope it is something I am doing wrong because to release software that will not make output is unacceptable.

 

Now I have to go back to version 5 and hope I can open the files to create the output I need.

 

Any help would be appreciated, if you need more info on my particular setup just ask.

 

Regards

Darren

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 13 years ago in reply to ericwertz +1
    On 15.02.2012 07:31, Eric Wertz wrote: I am also having the same problem running 6.1.0 Light. I have verified that "pos. Coord" is set in all of my layers. I see the crash on two different machines, one…
Parents
  • Former Member
    Former Member over 13 years ago

    On 02.02.2012 22:51, Darren Carpenter wrote:

    I am trying to get a board out to be fabbed and frelling new Eagle keeps crashing when I try and create the gerber output.

     

    I am using Eagle 6.1.0 under Windows 7 x 64 Pro.   The CAM file device I have selected is GERBER_RS274X.

     

    When I press the Process Job button the CAM starts to make output, the .gpi and .gbr files are created in

    the directory, but they are zero bytes and then the program crashed and closes.   If I use the Process Section

    button I get the same result.

     

    I am a long time user of Eagle under windows (from version 4 on) so I think I know what I am doing with the software.

     

    I hope it is something I am doing wrong because to release software that will not make output is unacceptable.

     

    Now I have to go back to version 5 and hope I can open the files to create the output I need.

     

    Any help would be appreciated, if you need more info on my particular setup just ask.

     

    Regards

    Darren

     

     

    Hi,

     

    could you please check whether there is the "pos. coords." flag is set

    on in all sections? It should not be switched off in 6.1.0.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ericwertz
    ericwertz over 13 years ago in reply to Former Member

    I am also having the same problem running 6.1.0 Light.  I have verified that "pos. Coord" is set in all of my layers.

     

    I see the crash on two different machines, one running XP on an Athlon XP-M, and another running Windows7 on an AMD E-350.

    Both machines can successfully run the CAM job with 6.0.0 Light.

     

    My workaround is to run 6.0.0, I suppose.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to ericwertz

    On 15.02.2012 07:31, Eric Wertz wrote:

    I am also having the same problem running 6.1.0 Light.  I have verified that "pos. Coord" is set in all of my layers.

     

    I see the crash on two different machines, one running XP on an Athlon XP-M, and another running Windows7 on an AMD E-350.

    Both machines can successfully run the CAM job with 6.0.0 Light.

     

    My workaround is to run 6.0.0, I suppose.

     

     

    Don't use 6.0.0, but try our new beta 6.1.2.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 13 years ago in reply to ericwertz

    On 15.02.2012 07:31, Eric Wertz wrote:

    I am also having the same problem running 6.1.0 Light.  I have verified that "pos. Coord" is set in all of my layers.

     

    I see the crash on two different machines, one running XP on an Athlon XP-M, and another running Windows7 on an AMD E-350.

    Both machines can successfully run the CAM job with 6.0.0 Light.

     

    My workaround is to run 6.0.0, I suppose.

     

     

    Don't use 6.0.0, but try our new beta 6.1.2.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ericwertz
    ericwertz over 13 years ago in reply to Former Member

    I've verified that the beta 6.1.2 doesn't crash when running the same CAM job over the same BRD file.

    Any idea when a production-ready version will be available?  Not crashing is nice, but supported output is nice too... :-|

     

    Since the fix, and presumably the problem, is known, is there a workaround within 6.1 that will generate correct/supported output?

     

    thanks!

    -e