Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Electrical test errors
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 226 views
  • Users 0 members are here
Related

Electrical test errors

rickford66
rickford66 over 14 years ago

I get electrical test errors and warnings such as "OUTPUT and SUPPLY pins mixed on net DGND (sup)" when I run an Erc.  In the libraries, the device pin is defined as PWR and the DGND pin is defined as SUP, so why does it flag an error when I connect the device pin to DGND?

Thanks.

  • Sign in to reply
  • Cancel
  • rickford66
    rickford66 over 14 years ago in reply to e14 Contributor

    I guess that makes sense.  Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    rickford66 wrote on Wed, 29 February 2012 11:26

    I get electrical test errors and warnings such as "OUTPUT and SUPPLY

    pins mixed on net DGND (sup)" when I run an Erc.  In the libraries, the

    device pin is defined as PWR and the DGND pin is defined as SUP, so why

    does it flag an error when I connect the device pin to DGND?

     

     

    The Supply direction is only meant for the special case of supply symbols.

    That type of pin will cause any net connected to it to be named the same as

    the pin name (i.e. V3V3 or GND).

     

    You can either setup power input pins to be the direction of "power" or as

    "input".  If it's a power direction then the ERC will complain when the net

    name connected to the pin doesn't match the pin name.  That is kind of

    annoying, but I've also caught a few issues with that e.g. GND vs GNDA.

    With the input direction you don't get that extra check.

     

    Hope that helps.  The manual describes the direction parameter in the

    symbol section.

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.