Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) No air wires connected to some parts.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 189 subscribers
  • Views 1096 views
  • Users 0 members are here
Related

No air wires connected to some parts.

rickford66
rickford66 over 14 years ago

I just created a board yesterday from the schematic.  I have placed about 70% of the parts on the PCB, but have noticed that some parts don't have air wires connected to them.  Upon launching it this morning, I get an error saying that the PCB and schematic are not consistent.  Run an ERC.  I run it and get the following error.

Different connections on C12 pin + and pad + (+12V/none)

There are others for other caps, but they are the same error.  These caps do not have air wires connecting to them on the PCB, but the parts are connected in the schematic.  Did I do something wrong?  Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 3/1/2012 9:37 AM, rickford66 wrote:

    I just created a board yesterday from the schematic.  I have placed about 70% of the parts on the PCB, but have noticed that some parts don't have air wires connected to them.  Upon launching it this morning, I get an error saying that the PCB and schematic are not consistent.  Run an ERC.  I run it and get the following error.

    Different connections on C12 pin + and pad + (+12V/none)

    There are others for other caps, but they are the same error.  These caps do not have air wires connecting to them on the PCB, but the parts are connected in the schematic.  Did I do something wrong?  Thanks.

     

    Marco is right.  I had the same thing happen to me.  The only way I

    could recover was to delete the parts and re-add them.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 3/1/2012 9:37 AM, rickford66 wrote:

    I just created a board yesterday from the schematic.  I have placed about 70% of the parts on the PCB, but have noticed that some parts don't have air wires connected to them.  Upon launching it this morning, I get an error saying that the PCB and schematic are not consistent.  Run an ERC.  I run it and get the following error.

    Different connections on C12 pin + and pad + (+12V/none)

    There are others for other caps, but they are the same error.  These caps do not have air wires connecting to them on the PCB, but the parts are connected in the schematic.  Did I do something wrong?  Thanks.

     

    Marco is right.  I had the same thing happen to me.  The only way I

    could recover was to delete the parts and re-add them.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rickford66
    rickford66 over 14 years ago in reply to e14 Contributor

    No, that's not it.  I'm aware that they both have to be open.  From the schematic, I created the board.  As I moved the parts onto the board, a few caps didn't have air wires attached.  I thought that was weird, and thought I'll have to go back to the schematic and make sure these parts are really connected there.  I saved it and closed it last night.  I did not do anything in the schematic after closing the PCB, as it was late.  I closed one, then the other.  When I opened them this morning, I had this problem.