Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 6.1.0 Unattended Install
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 188 subscribers
  • Views 1677 views
  • Users 0 members are here
Related

Eagle 6.1.0 Unattended Install

e14 Contributor
e14 Contributor over 14 years ago

I maintain the installs on our University owned machines.  I need to deploy this software to around 50 machines, and will periodically need to update this to newer versions.  I have the license and the installer already, but I'm running into issues automating the install process.

 

I noticed that your self extracting exe unzips and then runs "bin/eagle.exe --setup", which is fine, but I'm not able to figure out how to pass any of the inputs for scripted installs.  It appears that all the --setup command does, is take a couple of inputs, and then copies itself into the target location, and create two files: eagle.key, and uninstall.lst.

 

I have a feeling that I could install it onto one computer, and then copy the install onto other computers, while adding the 4 Registry keys, and the 5 start menu shortcuts, but I'd rather do it through officially supported means.

 

Is there any method provided by CadSoft for unattended/silent installs?

 

Thanks,
ECEHelp

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 08.03.2012 18:21, schrieb ECE Help:

    I have a feeling that I could install it onto one computer, and then copy the install onto other computers, while adding the 4 Registry keys, and the 5 start menu shortcuts, but I'd rather do it through officially supported means.

     

    As a matter of fact, that is EXACTLY what can be done (we do this since

    years):

       1. Install it on ONE machine (your reference).

       2. Afterwards, just deploy EAGLE by copying all the reference

          files to other machines (prefereably into a folder where

          the user has WRITE access, otherwise there'll be problems

          when running EAGLE later).

       3. (Cannot be avoided) When starting EAGLE the first time, every

          user must enter your license key.

       -


       4. Adding registry keys is ONLY necessary if the users like to

          be able to double-click on EAGLE files to open them.

       5. Same is valid for the menu shortcuts.

     

    This even works for multiple operating systems: All EAGLE files for

    Windows, Linux and Mac can reside on ONE system (we use a samba server

    here), even without any useless duplication of libraries etc.

     

    Additionally, in order to keep already existing EAGLE installations

    up-to-date, I can provide you with an update program (for all three OSs)

    that the users can start themselves: This program can check a (remote)

    server for your reference installation and then update all local files

    with newer ones from the reference repository.

     

    If you're interested in this, send me a valid e-mail address, and I can

    give you more details.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 08.03.2012 18:21, schrieb ECE Help:

    I have a feeling that I could install it onto one computer, and then copy the install onto other computers, while adding the 4 Registry keys, and the 5 start menu shortcuts, but I'd rather do it through officially supported means.

     

    As a matter of fact, that is EXACTLY what can be done (we do this since

    years):

       1. Install it on ONE machine (your reference).

       2. Afterwards, just deploy EAGLE by copying all the reference

          files to other machines (prefereably into a folder where

          the user has WRITE access, otherwise there'll be problems

          when running EAGLE later).

       3. (Cannot be avoided) When starting EAGLE the first time, every

          user must enter your license key.

       -


       4. Adding registry keys is ONLY necessary if the users like to

          be able to double-click on EAGLE files to open them.

       5. Same is valid for the menu shortcuts.

     

    This even works for multiple operating systems: All EAGLE files for

    Windows, Linux and Mac can reside on ONE system (we use a samba server

    here), even without any useless duplication of libraries etc.

     

    Additionally, in order to keep already existing EAGLE installations

    up-to-date, I can provide you with an update program (for all three OSs)

    that the users can start themselves: This program can check a (remote)

    server for your reference installation and then update all local files

    with newer ones from the reference repository.

     

    If you're interested in this, send me a valid e-mail address, and I can

    give you more details.

     

    Andreas Weidner