Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) grab part in PCB 6.10
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 638 views
  • Users 0 members are here
Related

grab part in PCB 6.10

rickford66
rickford66 over 14 years ago

I'm wondering if there is a special command to grab a part in PCB.  For example, I would type SHOW U1 and Eagle would highlight U1 so I could find it.  Rather than hunt for every part to move them onto the PCB, is there a command that will cause the part to become attached to my mouse pointer as if I was moving it?  I've used FIND U1 before.  That actually works sometimes.  I haven't figured out why it only works simetimes, but Eagle complains everytime that it's not a valid command.  Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 16.03.2012 16:51, rickford66 wrote:

    I'm wondering if there is a special command to grab a part in PCB.  For example, I would type SHOW U1 and Eagle would highlight U1 so I could find it.  Rather than hunt for every part to move them onto the PCB, is there a command that will cause the part to become attached to my mouse pointer as if I was moving it?  I've used FIND U1 before.  That actually works sometimes.  I haven't figured out why it only works simetimes, but Eagle complains everytime that it's not a valid command.  Thanks.

     

     

     

    Try   SHOW @ U1   and EAGLE points to the part.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 16.03.2012 16:51, rickford66 wrote:

    I'm wondering if there is a special command to grab a part in PCB.  For example, I would type SHOW U1 and Eagle would highlight U1 so I could find it.  Rather than hunt for every part to move them onto the PCB, is there a command that will cause the part to become attached to my mouse pointer as if I was moving it?  I've used FIND U1 before.  That actually works sometimes.  I haven't figured out why it only works simetimes, but Eagle complains everytime that it's not a valid command.  Thanks.

     

     

     

    Try   SHOW @ U1   and EAGLE points to the part.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/