Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) VALUE attribute also used to update the Value
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 694 views
  • Users 0 members are here
Related

VALUE attribute also used to update the Value

e14 Contributor
e14 Contributor over 14 years ago

Currently, the VALUE attribute is always used to initialize the Value of a part in a schematic, whatever its status (ON / OFF).Very well!

 

The problem is that it only happens the first time the part is added in the schematic.

If I replace the part or if I change its technology, its VALUE is not updated.

The VALUE of the part remain this one of its first placement.

 

It is not only very annoying but it is also a source of errors!

 

This is why I propose that the VALUE attribute (if exist) is also used to update the VALUE in the replacements and changes of technology.

 

Christian Bohrer

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 03.04.2012 10:27, schrieb Andreas Weidner:

    Therefore, you type 'a ad797s' and get this opamp in the

    SO-8 package. Quick and simple. BUT under normal circumstances,

    the device value now shows 'AD797S', and my students often

    ask me to buy this AD797S, because the stock is empty. It

    ISN'T empty, of course, but this IC is NOT labelled 'AD797S'

    by Analog Devices, but 'AD797ARZ'.

     

    As a matter of fact, about one minute ago, a student did INDEED ask

    EXACTLY that question: It was about the 'S' suffix in some (old)

    schematic, and it was even the AD797. Strange...

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to CSWalt

    Am 02.04.2012 17:27, schrieb Walter Spermann:

    To make things simpler I tend to say that in any case (change package, technology

    and replace) the values get overridden if there's a VALUE attribute in the new device.

     

    THAT of course is also possible. It's perhaps not as nice as one wishes,

    but it's still MUCH nicer than apparently implemented now, and it has

    the benefit of simplicity. Yes, please.

     

    Originally we thought that a device's value is something that should be defined in the

    schematic or board.

     

    Yes: For devices with VALUE=ON, that's nearly always the case.

     

    No: For devices with VALUE=OFF, the value comes from the LIBRARY and is

    automatically created by a mathematical construct, which, QUITE often,

    does NOT yield the desired text.

     

    Examples:

      1. Manufacturer's IC suffixes are not standardised and therefore

         rather confusing. In order to not having to memorise all

         thousands of suffixes, our libraries use the suffix 'S' for

         (standard) SMD packages - independent of manufacturer.

         Therefore, you type 'a ad797s' and get this opamp in the

         SO-8 package. Quick and simple. BUT under normal circumstances,

         the device value now shows 'AD797S', and my students often

         ask me to buy this AD797S, because the stock is empty. It

         ISN'T empty, of course, but this IC is NOT labelled 'AD797S'

         by Analog Devices, but 'AD797ARZ'. Therefore, one wishes for

         an EAGLE value of either 'AD797' (ignoring the suffix, because

         one SEES what package is necessary) or 'AD797ARZ' (which is

         the manufacturer's code).

      2. The diode 1N4148 has about 24 different packages in our

         library: Pad distances of 0.1", 0.2",..., 1.2", each with

         large pads (easily solderable for our students) and smaller

         pads (for dense layouts). WITHOUT default values in the

         library, you would get either NO value at all (VALUE=ON) or

         values like '1N4148-01N', '1N4148-02N',... (VALUE=OFF).

         Here, for ALL cases, one would like to see JUST '1N4148'

         as value.

      3. All ICs in our libraries have SEVERAL flavours of DIP

         packages: One with large pads (easily solderable), one with

         long pads (easily solderable, through-pin routing possible)

         and one with reduced pads (for dense layouts). The value

         of ICs using EITHER of these packages should be the SAME,

         because it will be the SAME component (just the board copper

         changes).

     

    Supporting value definition in the library by an attribute VALUE

    is more like a workaround and no standard case.

     

    As shown above, the possibility of DEFAULT values in libraries does NOT

    seem to be a workaround for me, but a QUITE valuable addition, because

    ALL devices (defined with VALUE=OFF) in ALL my libraries will be

    equipped with such a thing...

     

    And since we have THOUSANDS of devices with VALUE=OFF, but only a

    limited number with VALUE=ON, the 'workaround' with the value attribute

    will become OUR standard (at the moment, I simulate this with a

    self-made attribute called TYPE, but this doesn't work anymore in

    version 6 in case variants are used).

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • CSWalt
    CSWalt over 14 years ago in reply to e14 Contributor

    Hello,

     

    On 04/02/12 10:29, Andreas Weidner wrote:

    Am 30.03.2012 16:45, schrieb Christian Bohrer:

    >> Currently, the VALUE attribute is always used to initialize the Value

    >> of a part in a schematic, whatever its status (ON / OFF).Very well!

     

    YES!

     

    >> The problem is that it only happens the first time the part is added

    >> in the schematic.

    >> If I replace the part or if I change its technology, its VALUE is not

    >> updated.

    >> The VALUE of the part remain this one of its first placement.

     

    That's NOT so nice...

     

    >> It is not only very annoying but it is also a source of errors!

     

    YES, that's quite definitely a source of errors!

     

    >> This is why I propose that the VALUE attribute (if exist) is also used

    >> to update the VALUE in the replacements and changes of technology.

     

    YES, please! The algorithm could look a little bit more sophisticated,

    e.g. as follows:

    1. If the component is REPLACED, the current value is ALWAYS replaced

        by the VALUE attribute of the NEW component (in case such an

        attribute exists). If NO such attribute exists, proceed as

        currently implemented.

    2. If the component PACKAGE is changed AND the new package contains

        a VALUE attribute AND the current component's value has NOT been

        changed from its default, change the component's value to the

        new package's VALUE attribute. Otherwise, proceed as currently

        implemented.

    3. Same as (2), but for changing the TECHNOLOGY.

     

    The above would assure that component default values UNCHANGED by the

    user would automatically be changed to their new counterparts, and, in

    case the user DID change something, this change would NOT be destroyed.

     

    Andreas Weidner

     

     

    Thanks for your ideas !

    Currently nothing in this direction happens, it was like this also in V5.

     

    This is a tricky and confusing topic. There are at least 2 more cases:

    1. The existing part/element's device has no attribute VALUE, but the new device has one.

    2. The existing part/element's device has no attribute VALUE and also no user defineable value.

     

    To make things simpler I tend to say that in any case (change package, technology

    and replace) the values get overridden if there's a VALUE attribute in the new device.

    In both case I would prefer to update the value by the VALUE attribute.

     

    So the general rule would be:

    If a user uses devices with an attribute VALUE by whatever command, he gets the

    value of VALUE as part/element value.

     

    This can be compared with the behaviour of other attributes:

    If a user has a part/element with a device with library attributes and changes this with

    replace/change package or technology, all attributes get replaced by the new

    package's or technology's attributes and their values.

    This is for library attributes, not for schematic or board attributes !

    These attributes will be kept in any case.

     

    Originally we thought that a device's value is something that should be defined in the

    schematic or board. Supporting value definition in the library by an attribute VALUE

    is more like a workaround and no standard case.

     

    Regards,

    Walter Spermann

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

     

    "Andreas Weidner" <andreas.weidner@aei.mpg.de> a écrit dans le message de news:

    jlbo1v$v68$1@cheetah.cadsoft.de...

    Am 30.03.2012 16:45, schrieb Christian Bohrer:

    >> Currently, the VALUE attribute is always used to initialize the Value of a part in a schematic,

    >> whatever its status (ON / OFF).Very well!

     

    YES!

     

    >> The problem is that it only happens the first time the part is added in the schematic.

    >> If I replace the part or if I change its technology, its VALUE is not updated.

    >> The VALUE of the part remain this one of its first placement.

     

    That's NOT so nice...

     

    >> It is not only very annoying but it is also a source of errors!

     

    YES, that's quite definitely a source of errors!

     

    >> This is why I propose that the VALUE attribute (if exist) is also used to update the VALUE in

    >> the replacements and changes of technology.

     

    YES, please! The algorithm could look a little bit more sophisticated,

    e.g. as follows:

    1. If the component is REPLACED, the current value is ALWAYS replaced

        by the VALUE attribute of the NEW component (in case such an

        attribute exists). If NO such attribute exists, proceed as

        currently implemented.

    2. If the component PACKAGE is changed AND the new package contains

        a VALUE attribute AND the current component's value has NOT been

        changed from its default, change the component's value to the

        new package's VALUE attribute. Otherwise, proceed as currently

        implemented.

    3. Same as (2), but for changing the TECHNOLOGY.

     

    The above would assure that component default values UNCHANGED by the

    user would automatically be changed to their new counterparts, and, in

    case the user DID change something, this change would NOT be destroyed.

     

    Andreas Weidner

     

    Thanks Andreas for your support.

     

    may be the diagram below would help to understand the problem (in red).

     

     

    begin 666 ScreenShot314.png

    MB5!.1PT*&@H````-24A$4@```N$```%'" (```" CP6K```>7$E$051XG.W=

    MX;&C1A8&4-B:0"84A)0)A2'XE F$T/;)8%A! T</OV.>5R:?0D!.K6Y:-I

    MH?[U>G4``,'\YD5``!8\>/I%2BI[_NG5Z$R1M&I8\=DZ^GZ0G?JKH/:.YO

    ME6KN5!FEZ[K7Z_?3JU"-OO_Y]"I421_[5M:>IB?LEZ /:.[]"C:W<ST`0$0R

    M"@`0D8P"`$0DHP``$<DH`$!$,@H`$)&,`@!$),``!') ! 1#(*`!"1C (`

    M1)3M]WJ@4LM?N#CP^R!]_].OBJ0Q=HG7Z_?8LIHX\V]2D:!$:%:?!M>4KP

    MLVV,IJT_MJPFSDISO-<#R31/%6)K-X.M[6Q"EI[@W&4: .TZ'@[M^Z-MRY

    MK&6S!W][)]',6F?6[LM&?-<]9H?F8U]:?16>HKE',@H$,JTI[\[[3(>"5T]:

    MSQZ\?,SVG00W:[YE(PX]9-G*^D"-&F]N&04"V9@H-XLO&_7E8]W9.-(BOEG[

    MIM[NWLLZ0.1-=[<,@J$LUITIH_&_] BH].[G7T@;HTU=PR"F2S>F*(JFT<

    M*.]O[O&\0%?;CJHUFGLDHVQ9GN:?/6#_7V>+W?E(FK4Q?GO^V@GOSB7IAT&L

    M3CLXO]B/R]$''J&Y-_2OUOI=2BF[_NR[_BR";>O8+'_A:'KX11L%?U_<],

    MK7/XGULLN2?PXUE\%V=C;<R3[!M1TX1OS6\XTDK9TZ[K"9.7^#G<6/U"

    MQT9SC[8?MO$]D>)J[P.:RL%F]LXREO2=1'Z<N5A%4B6"UGTSO_.H!'Q\

    M?2<1K,Z._'A[>R&KAT;Z0 2:>Y5KN)VUD6H__G6I[W\._TWOF=UOA@$`+3".

    MLFX:.6\;"_GXQ??9;9JU[!CPT>R02>?)+4=SRRB/6?:>\U]\IQ&Z!,?H.4U)

    MT-PRREM7GU)Y]Y6-2U\4`&HAHZSX'6>G7_Z->-!PLK`#1.1CFE8$ I^+JD

    MY+(Z.:P>?GS5E"<__JI'$.<_T2TTI8PRMSI-M9OTIW>SD)9?NMF^AMOJQ<Z7

    MWA9/K*%?LG2<G+2(Y?5X;S9)?B_>K?F9<V0!O'F4]TUTQ3RBASVU]2_^J)

    M!Q[Y<2'V-%"UPQ5F?/"9G=/)IQ-'(TTIHT#U5J]0N1R6$W#CV[[8Z/*1JRV^

    M_SK"VY<>GGFE^/V7*GQ[2>AW5Z1=/F#ZIRI:4T:!NKFL3AJK3;G:B-/S1,L6

    M7][HUOK Q@+?W>EJ"#?8WRY3>YKOJP4&(:- 35Q6)[?MBU:OWNZT>,WV?*)G

    M-KFMY.O]S_X3(U,1E=7*F3/&#"0)%7?R$[U\Y/[G5M&4,@K4S65U*,BD

    MD\=]]8G>/KLW/J;>-O6;@M *":8B9XZ/3[[NZ_5[^&]Z?R/?(JG"ZH55-EKG

    M79MN+#"._O5Z/;T.Q?1]7UU(?%#?_\S4^O=XL(_MF=4_,SNB>G#-\_6TDSUA

    M^]LZW:MNLD1\_C/[7W5ZG<WMO_9?I2J2LSU=X'KOC@[_]$?VR[C5ZQ>L_'

    M%3BI8'/*.VJO6H\0A\[(&5/R]H3-JXJ)J,\O18'G;E2W(E7-/<SO4`\('9

    MLCS"G%D`_C$[-6 :2@+-GUJ30Z040#XG^5LV6?6@WJ;43G>@" B&04`" B

    M&04`B$A&`0`BDE$`@(AD% `@(AD%`(A(1@$`(LKV>SU/KT)E,K7^/?2Q8_+U

    M-#WA6U7W`<W]+;\I6).^]SYS.=V,3C=H3/KF=JX'`(A(1@$`(I)1`("(9!0`

    M("(9!0"(2$8!`"*240" B&04`" B&04`B$A&`0`BDE$`@(AD% `@(AD%`(A(

    M1@$`(I)1`("(9!0`("(9!0"(2$8!`"*240" B&04`""B'T^O`%!,W_=/KP+/

    MTPU(0T:!)%ZOU].KP//ZOM<32,.Y'@`@(AD%`(A(1@$`(I)1`("(9!0`("(9

    M!0"(2$:YQ/;U"5R]```^DE&N\BZ(""@`L(>,<HGM:RBYPA)0BE%;$I-1+K2L

    M#NH%4)Q16[24:XUK1'J!5"<45L2DU&N,I:&(9J,`47)`(HS:DM,@I !D9M

    MR<<O9%YH62:\V\ 55D.)@D/MC-<2($`@,-D%("$'".1@(QRK6F94# BR@O

    MI"2C```1R2@`&1BU)1\9Y7)#L5 R`. K,@H`$)'KHUQK=M$"[S9P$=6&?'X\

    MO0)IC?7B[]__5(H_?O;#G6H'4-!06(92
    ?/?KBAVI" <93RENEDZH^??K@'

    M&.:3E8-!4>UH5(R2DG;Z61X0#.^)A.IA0<*B6C%/-5R1@H',"W#I2:P1\_

    M%7PJXWL]!?1]?ZQJC>-_4@IL$??]P?2R?3IJ@T5$:M/V7]R9YM)L"VP\,G

    M2T9PJ86,<E"I=#(EJ0!!=/)E*1"?#UZY()U,!S"X)U,3A$)J-\YX:2

    M,5 XH&6WE9J!Z;3$9,[L7H<GQAYC.BTTZ^3$V,,OJMH0C>S\V=4G=[:9I +M

    MN'GX9$:U(1H99<NSZ63J1_([=ET,J/@$(2,\E:HDC%0.""?@5FH.#P.+\I

    MN")LR?C[]\L/$T(:84O-Z._?K[YW*,MCS)G]/S=/C#W@[]\OTVFA=L/G-VR=

    M&8RKI]KP% 'Y'W&FGNQG@AO4*'XZ65)M>(2,4F4ZF7+.&&H1?)AV#P6'.[6>

    M414C('"`9&E34#!8=[M#L?)?[4DZ^8I (Q53'UY(!A.NW3:T%R+8ZCU'YR

    M9YO3QA#$>!3TQ\^$&:53;;A>6QDE=SJ9,A(STHY=K)*4N$ZK624=M)E*0"

    M]\MT$GD_284K-)%1VBP9(TD%[M%XJ1DH.!24?,YLLHFQQYA."U?+.C'V&--I

    M27M.$J;)W>V.;Z!XM)/C#W&J1^2)A1I)-MD@H488SV(TF%DU)E%.ED/TD%

    MSG!F9S])A</R9!3'--]2.. `I>: X4280R.^E6'.K(FQQ_@)9?B*B;&'C6_:

    M,)U6P6&GNL=1G-PIQ9@*;# QMJ!Q3$6UX:-:>XET<@4CL3!CC/8BCHO8H\J,

    MHFI<2E!3IVYA:3"MLHRBN&3>R@<-&Z<=^+DSM7&:M,I."Q4DU&DD_M)C3(

    MU)-'^.(/JRK(*-+)LR05&B&=/,YT6F9"=P7I) ['-R1FZDDHCHL8QSX<EEZJGNCAAL*!\J]VL[JLU.DDIZ_[GSQ?J^'P]KZOHD[#&]

    MEG-!U;U18..S0TW&_K>'FL[D/TD6HS&O-W[]?JDU-V64!.ED5A%N.. H

    M7H#N-$TJ3Z\+#1G3R;CK>GJ-CE!MOC*.8Z+\KDCHU1Z<N<K8Q$I<G#SQ\^

    MZI(Q,J#";:;I),?'YQW59I6DDM/2Y?>0CJYPGBJ^.D56#<EJ$S.&=,<<N)

    ML0K.?BFK3?=OKU!P:G=51DF93L;K/JT.O3HWO$%2X2*SB;%I/C6JS6&22B;E

    M,TK=+)M_P3[[3^E)ZE0T.RL8U\K%2;G69)1;6I5.'Y*+5/C/WHY"6TWYU(

    MWEYFCF'8D>FTG)1C8NQ'JLUYOF98NV+ILIWADX73MI_B:2=S\WZEKJ2"MJ

    M\9IL9Z@VI;B22J49)1VT@E7D%38H[5TPA4DE>J<RBC2":5(KPCG5"6I%*1

    M@QE%.N$*D@HS]5[/GN!4FRH<R2A1)3K))NRI_R=I!PA32E)G>1,8Y"(,F.

    M;'SCL2!)A5(RG>M)7V3,1R&$9.EDD+Y\W$]2X8Q,Z620OLB<NC[*Z_4:WITJ

    M?O'A\!J.3WQP&\^L?/#6&5=O[$[PSM!)@G?I3K6)9[IB2DU%"ES#K:ZD,C6[

    MKM&[AQWX/8L[KU2]\5KC]3=C_LJ:=,(QM225*=7F0=))O8I=9W::5$HMLZ#Q

    MER\.\'P<EG2"2>%3BJ31RSX9-G5X8#"O]>S] )JCAG/'3<:349O]PXO7-Y

    M.>KQ_G>W9TOK)F5T]3V9_G7C]NK2ME\K9A,<*QFK/_$SSHA2?=I42\%1;>YW

    M9NJ):A-'X=_K&40[]?/'VN]63'_I8_K_Z>=P>3 TNW_ZL1QOSWY#9'L(=/;7

    MU;6:C1)/R\&[UWKW#CSKS,F=U<</=RH9C0MUZD>U>;S:G)]ZHMK$4?YWCP?C

    M\<WRTQ7<[#!B]J$]MB';I7/VUW$%5HO=SC69'8H]_OZ7&FY-/XF=PVH94YE2

    M;<HZ,W:RI-I$<%5&&<1)*L\>8.W_A(_WO/NHKQY4[?SK(\J>#'Z]7AN%PV L

    M0P]Y]E.@VCRB^+P3U2:":S/8)I4[N_-RQ>-,ZP;79D,S,]C?WM7V\VGMDI

    MN,QWA6-ZIP.@ECU8<%2;1Y0=/IE2;1YWR7R45:'.&4_-SK^>7,[VTO8,PVX/

    MNKY;PO51X4CG4D^('PI'\<622<R"H]J4=7[JR4>JS;,>"(!W7IUV.<5]

    M.4U].GEM.<UM^Y_394Z/169#H*O/6EW)U=NCY>K-7NO=ZMU9.(J/N(YFQRO#

    M/\<[`Q[9!%D-[IFDHMIT-U:;Z\9.!K54F_1%YK'-<QW]?*Y+)X/EIW'Z%<$X

    M56,49#48U#6=EG>N3B>#6JI-^B+S\.:I&CE<G4X&VR>&XU2-49#58.30J';W

    ME)JNGFJ3OLB$V#Q)I6K7S3N9>C>+?E8L5A_SE/3EHU*22HWN&3X95%1MTA>9

    M0)LGJ53GMF.:2J4O'U53<&IQ9SJI3OHB<\=WCW>J\1),S9).J)V"$Y]T0L0(

    M9B0V,NEDO_2'.#DH. %))SNE+S)Q-\_Q3332R;?2EX],))4XE)K]TA>9Z)LG

    MJ01QS\389-7CWPDE6<9/OE6B)3Q9)@]R3'-8O*1E8)S/GDF/1%IJ;-

    M4SAN)IV<E+Y\)&9 Y3;2R1GIBTQEFZ=PW$,Z*2)]4A/P;F4=')>B)3Y>89

    M4F.=%)0^O1"$GE"@)$>F3,6;)ZD49V)L6>G1U,DE5DDX+2%YGJ-T]2

    M<PR172EX\&22IG2"?%I2\R239/4CE,.KE.^O1)C'E`.GD(NF+3K-Z_M>

    MU=A/.KE:O+1,DEE)GD4NF3;-,Z"RAW1RC_3E`TEEPS2==*K--=(7F9R;

    M)ZF\(YW<7WY8""I+!DN4?Z(I-Y\R25&5_;N5GZ\L%HC"E=\S5'.KE3B3

    M?/,Z2:7K.L,G#TE?/IAI/*E()_=+7V22;]ZHV:0BG3PH??E@58.G?J23IZ0O

    M,LDW;ZJUF"*=/"Y]^6!#(TG%Q-AGI2\RR3=OJ86D(IT$D;Y
    %'NI&+XY''I

    MBTSRS7LG<5(Q,3:.].6#/5).4I%.@DA?9))OWK9D2<7P233IRP?[I4DJTDDH

    MZ8M,\LW[,=(K'024_KRP;>JCC224#IBTSRS=NIW@$5Z22R].6#8ZIB;&

    MAI6R"3?O*_4E52DD_C2EP\.JC4C&3R-(7F>2;=T 52<7$V"JD+Q<%#RI

    M2"?QI2\RR3?OL!)Q?!)1=*7#XH(F%2DDUJDS+)-^^,:.>,I9/JI"\?%!0D

    MJ9AZ4I?T12;YYIT7(:E()Y57SXHZ]F8(IW4'V12;YYI3QUZD<ZJ5KZ\L$5

    M'DDJ3NY4GV12;YY9=V<5$R,K5WZ\L%U;DLJTDG5TA>9Y)MWA1N2BN&3'-7

    M#ZYV:5*13A)(7V22;]Y%KIND(IUDDKY\<(_B2<74DS32%YGDFW>ILDE%.LDG

    M??G@-J5BBG223/HBDWSS;G#^U(]TDE7Z\L'-3B85)W?R25]DDF_>;0XG%1-C

    M$TM?/GC$@:0BG625OL@DW[R;?954#)DE[Y
    *"=244ZR2U]D4F
    >??;,TE%

    M.FE$O+!LZ8QI5O4'%-/6I"R"3?O*>\2RK225/2EP\B6"85Z:0=Z8M,\LU[

    MUC2I2"<-2E\^B&.65 :Z7WKIBTSRS8M@K!W>ZM:D+Q]$H]JT)GV1^<_3*Y#?

    MT(%R=R,@`M6&9&04`" B&04`B$A&`0`BDE$`@(AD% `@(AD%`(A(1@$`(I)1

    M`("(9!0`("(9!0"(2$8!`"+Z\?0*M&OVZU]# RXB&I#I8RC/&;VZU]# RX

    MB&I#I624*-_Q#80A&I#9SK>=K]7I7):#L89G@<-4&VHDHX0PJQW3?PZW

    MQWO&V@%P@&I#1624A[T[N'E7'1S6`,>H-E1'1@EJ5AV&XK*\'^ DU8:PS)FM

    MQNOU&FL'P'54&X*04:(;RH1B`5Q-M2$:YWH>-A:%Z;#J] AF-M/>Z"MPC&I#

    M=624A[VK`LLSQ+>L#I"6:D-UG.L!`"*240" B&04`" B&04`B$A&`0`BDE$N

    ML7V!`9<?`("/9)2KO LB`DIBLBE 03+*);8O,.#R`XG)IL!U6CL0DE$NM.PN

    M3H04]T=Y5.X%2FCH0DE&N->TT3L0'VEWH)36!NEEEO,?OEB8L8)":7

    M<)O6!O_I6AJDEU&@)-F4S4U,^@D4%Z&>56=E1 669!M::I`R$9Y4(I>PP'

    MZ G<+/&!-4V14: PB81'R"4MRUIV9)1K3?M-UCX$/*NIP7^ZEEI61H'R9%.

    M\V04@(2$X]P:.1"242XW])[$?0AXG I#2C>7H&[/36M[/[75;.>]7J]K[7

    M"@"'Y<\HLW#PUNOAU;D;K,-;WQG*9N2WA"+Q]O/K@PW:.% *&U&&3K[822

    MF=F&MU:\9--!(\T-$3QR+'3SB]Y<4A)FE*'!VMDG[32^(;FO/BF;-IY-X6;3

    MB-!"V9EN[PU5)=4PD72RWY_]GUVN_9;6WY:OQ5F5?O _"(=#W;]5I;NRL"3I

    MS?9/Q38;VG]_7*T>(WR702VV5ZDX"Q=5U@RG.OIUYW.69XW^H]\%(LOC6V

    M>-?P/N8V_S<J_NO7<RMRB9O'_"-0<-ZYKK#4NG,:"2A%_-G_65U/T/0GU=CH

    M5?C?'!TN>2=_M\MS=JCI)/]RHZI5)Q1=)JRZCH+( 4(::4]<]Q9#/19&D(

    M\DZE6IS0G:4FM&T6DN$GG)9N655<V#4LZF<J45.QK#BNR-ZDRH@TEXH<

    M4S3]12(W>G#2R3NU)Q6'0^>=/P2JZ/82]T@YAYTU\J9J,'U_>]=+*M__6K

    MQGZEVA1TIK94]IN"LT]_GK]%>VKDIK:@$;/3@!98_7KU_5]2O5IJPSM:6R

    MC$;E(Q[B"G["2C[U1535)LK'XM-6447>=.<797VOU.<=H],@'E6[7$%-7F

    M.L=J2S491=>YG]T5+ DHQ]024PBECHPBH#SE\9BBZ>_W>*-')J"<$3RFJ#97

    M.U!;ZL@HM$G)>(J8LDI .2]L3%%M[O%M;:D@H^@ZS[*[@DY 2=L3"&@"C(

    M;9)-GR6;T@[5YDY?U9;H&477B<#NBL891"G+4 H[1<\HM$DVC4 VI06JS?WV

    MUY8?5Z_*&2>[SO!+`=WD!Q>6]PQWSOZY?,SVTE85[/3C&LY6]4Y#EZKQFM:C

    M97L=>S//M,P#A^[%J'$'$3I?_TN%;[#4,I59>4)46FN,SC*$-C3)MD><^>

    M9WU<VO3&^,\]IAUZ(_&,`67G8K]]<#07'=8LF^G8NW1FW5:?NZ=;/L502DS]

    M7>GDMA=Z2MEJH\CLM[.V9,XH>PQQM?@>_;I=+ 5=T?1[5)T@6W/=(,J9W7_5

    M(RBC%F:E*#(GQ3W74R3>#OUC>G;FZCW]QDO,1MN&?TY#TNR<SCADMWHV:KJ0

    MV>W9TI8O?4R"TSU+RQXRO?_=[8]G#Y=W;KSHU.HIQ6EGZ-;&<NL=R&W9Z]>O

    M(:9,`\<87,:_F]/%S)=PFQI[Y[2_7N>:/O5QW_6?EI<8K,&7$SR@W&)MQH

    MSJ^6MN>UQMO3%YW>7N:5U>5,%S\Z5VLN3FEG?3@_7E&[5LH-GIN>4;N_/=

    M7NURJRO03K#[(6N;M^4V32(9;88HL/L]C0ES!#NRBS\919\EC>&&_/7CJ?

    MZN-(C-;PXUI>F,4M9JI)C]=>=RIIU@UF6/=8XTXWY7^_A&O1NY73W@V+.H

    MZ1.7C;OG,?M?D6_=,UMV&1%6'_"M=^>20B6/E#-GMRDR7\F?4:;A=/G6WSD3

    MY<$=2?"QDSAF;]1VY]FYD(TQTN62[Y]AQ-FYUS>#9]\N]@@*8091>8K3/*

    M.]N#8!\??.;E'/7&<</)KWE3X9=)6&>$O'O8F;#"LQ29,X)^KZ?X]\'.

    M])9^<E_>>M7_Y!Y[U;CG;2SO9*?Z^)NH-Y\>WDZEWR[J\$(*;G(518?!

    M..>CX *[M1!S/M:D#$;W5!M%9MO'?4K0$X'%>\^[P:Z=B?+

    5YI.<1W_
    M.IL#NWRYU3&]Y539Z9+?/>

    N8/_L_K^LSEU:-93-MM-'L[7WW3FXTQ_[E3U]B

    M8S[3]EL]IF<OW;8ZT75I-NMV=<1E]:M W=K7A99/V3G2<U_Z]?]

    MO>N:J/('+!=6UK))12;T;A#!F%ZZ3)*!RP75N"GNL!`!HGHP``$<DH`$!$

    M,@H`$)&,`@!$E"JC;']_^-LOET\O>G-\G7:\T$7:N52&=G_V%8F@R"5,4EX'

    M)8BG\IV"DNJC/Q6GO#C>E[O>?J.F<N_K9<VCV:VE%I]^5TY3M;$S>0@H

    M%SEP$+7]R82]",\GJ]GJVV9;\W?_\/`5[TO?_T%\G0[JO2M_NJU^M5RVZ[

    MR'5<GKH8S",71^ENW,L4_U2F*2S=CMJ2ZO=ZIM?1FUW%=7;G[)'=I\OVK?X0

    MY?839R\TO7/GY0*7FS![_,8U`5=?\;J+SY;R>KT.7%A)N[];C5K:G='TNJZS

    MV^-E89?7GUV](NUT(=O7G[WG8K()O/M8K5:>;L<'?UDN%):9/!EE-@ZVNM_J

    MUBX8WRVZR&H3=HO=WO83_UK[M<GE#O=TZ>O..T*T\6.MS^NQOVQY>NA7;?

    M6(WE[33MGM7LO3]6LY8O3$\999%7FN_GSR[O5P([ZQK#:.?SX6G(U/L<(R

    MR)-1IB%Q1Z].R!>YLJ/C]G8F7U<P6=>YZ^['][EOS1_C6/3+M_*T>[-V66

    M,]X]H-LW%K+QTS]BR@&KE6?Y@&[?!U9AF<F344[:?ZN[@7/O.[7CL^\EW:

    MO>*ET]/N;!A./M9U$N1CS@BU.4]-1AD<.[E\QL</;%.%Y<\=$]WB9I0[>\_)

    MMKG.SO1]S_KOZ4_G:?>NR7:GB-5Y)P3Q>,$)55AV"OJ]GAL<>.NW6^[=`O<?

    MJ:^7,&]]?3LZ?9)Z;=-UZ:4/K%7).=C]QXS,8]>Q;":/:QVO@TO?L`AS

    M?<_'%_JXP!H+2Q_Y".FKXF-:0>K=[Z;[/?;#[4<E6W7^CCT[?MG!XQFR2U

    MNKO==*W'4]K]PV)VSVLT_WC)-+9M-C-[[7\V[JZ_)9&]_KV9[U4MRS)WK^

    MMQI?#MPN/U;CN9N_S]6JX^<FIUWMOXIXW7G3V]RUM80F>4[OO>PT5NWE%I

    M]R $E.Z)C+R#O>FAWM4FE&6MN?,LFIG;6GW7 _ 'A5=STB00)*%^"2H0W:

    M?_ 3/:/H/1'<?S"MW2,PB!$F21[9ENPF%QO]<#$,2S7T)VEN=J9[Y.Z"S/

    MM[XZ(DCM(YI'[:4P?3VOU9!E& QU6040`>9U9**=$&408.BN[Q[<%/'1E%

    M[WGLP?3VOTI!E%6B2GGQ0PH`P7G:@<2QT9I=-[GA!A1Z7=[Q>AW<,24\Z(

    M'%"(J9J,TME=W<N."E:)<=4$5#L9:YS;)]24T:A3:K&G633/<24;U414 8

    MSA4.%Y;*,HK><X]H.RKM?H]H[1Z9F)?10%EH."4=::P1\6_BH72K]4V!V5

    M=K]4V':/,)E\H.KJ",^K[O7/[DG"'JG>D`56:4SN[J,L%W5-K](L';/;)A

    M3R:I+/WS4X65]RLUY[ B5:76C-()N:6=#[SW4#*$U#.DU2F<J23D9IS0FJ

    M4G%&&>@]1=2UEQ)/2ZDEF-9"4DF63D9JSGYEJTKU&:434TZK*Z",M/M)E;9[

    M?,/K&LIK(S3AW/W*$EEVQ7'/!DR2J?K'%7[8;1V/Z;V=J_%&%:ZC'EEK6F

    MIOJ2LK-T74E)DE$&NLY^F?92VGV_3.U>EVE>R:'Q7C0V:,N59_R&]G6=(55&

    M&=AC;<NZE]NV[V.SQKFCY;J#_3\?<4$\29I2!D#MS0^"-0O/--+N$$&^

    MT;EFRM)VHPRFG6:=G9=LLDIF_H&>T:W=@4SR9Y29%GNH66W:;=`:K3

    L7$8!`I0V6\`@"-D%$`@(AD% `@HO\"RY=4&>T-=BL`````245.1*Y"8((`

    `

    end

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 30.03.2012 16:45, schrieb Christian Bohrer:

    Currently, the VALUE attribute is always used to initialize the Value of a part in a schematic, whatever its status (ON / OFF).Very well!

     

    YES!

     

    The problem is that it only happens the first time the part is added in the schematic.

    If I replace the part or if I change its technology, its VALUE is not updated.

    The VALUE of the part remain this one of its first placement.

     

    That's NOT so nice...

     

    It is not only very annoying but it is also a source of errors!

     

    YES, that's quite definitely a source of errors!

     

    This is why I propose that the VALUE attribute (if exist) is also used to update the VALUE in the replacements and changes of technology.

     

    YES, please! The algorithm could look a little bit more sophisticated,

    e.g. as follows:

      1. If the component is REPLACED, the current value is ALWAYS replaced

         by the VALUE attribute of the NEW component (in case such an

         attribute exists). If NO such attribute exists, proceed as

         currently implemented.

      2. If the component PACKAGE is changed AND the new package contains

         a VALUE attribute AND the current component's value has NOT been

         changed from its default, change the component's value to the

         new package's VALUE attribute. Otherwise, proceed as currently

         implemented.

      3. Same as (2), but for changing the TECHNOLOGY.

     

    The above would assure that component default values UNCHANGED by the

    user would automatically be changed to their new counterparts, and, in

    case the user DID change something, this change would NOT be destroyed.

     

    Andreas Weidner