Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) VALUE attribute also used to update the Value
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 696 views
  • Users 0 members are here
Related

VALUE attribute also used to update the Value

e14 Contributor
e14 Contributor over 14 years ago

Currently, the VALUE attribute is always used to initialize the Value of a part in a schematic, whatever its status (ON / OFF).Very well!

 

The problem is that it only happens the first time the part is added in the schematic.

If I replace the part or if I change its technology, its VALUE is not updated.

The VALUE of the part remain this one of its first placement.

 

It is not only very annoying but it is also a source of errors!

 

This is why I propose that the VALUE attribute (if exist) is also used to update the VALUE in the replacements and changes of technology.

 

Christian Bohrer

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 30.03.2012 16:45, schrieb Christian Bohrer:

    Currently, the VALUE attribute is always used to initialize the Value of a part in a schematic, whatever its status (ON / OFF).Very well!

     

    YES!

     

    The problem is that it only happens the first time the part is added in the schematic.

    If I replace the part or if I change its technology, its VALUE is not updated.

    The VALUE of the part remain this one of its first placement.

     

    That's NOT so nice...

     

    It is not only very annoying but it is also a source of errors!

     

    YES, that's quite definitely a source of errors!

     

    This is why I propose that the VALUE attribute (if exist) is also used to update the VALUE in the replacements and changes of technology.

     

    YES, please! The algorithm could look a little bit more sophisticated,

    e.g. as follows:

      1. If the component is REPLACED, the current value is ALWAYS replaced

         by the VALUE attribute of the NEW component (in case such an

         attribute exists). If NO such attribute exists, proceed as

         currently implemented.

      2. If the component PACKAGE is changed AND the new package contains

         a VALUE attribute AND the current component's value has NOT been

         changed from its default, change the component's value to the

         new package's VALUE attribute. Otherwise, proceed as currently

         implemented.

      3. Same as (2), but for changing the TECHNOLOGY.

     

    The above would assure that component default values UNCHANGED by the

    user would automatically be changed to their new counterparts, and, in

    case the user DID change something, this change would NOT be destroyed.

     

    Andreas Weidner

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 30.03.2012 16:45, schrieb Christian Bohrer:

    Currently, the VALUE attribute is always used to initialize the Value of a part in a schematic, whatever its status (ON / OFF).Very well!

     

    YES!

     

    The problem is that it only happens the first time the part is added in the schematic.

    If I replace the part or if I change its technology, its VALUE is not updated.

    The VALUE of the part remain this one of its first placement.

     

    That's NOT so nice...

     

    It is not only very annoying but it is also a source of errors!

     

    YES, that's quite definitely a source of errors!

     

    This is why I propose that the VALUE attribute (if exist) is also used to update the VALUE in the replacements and changes of technology.

     

    YES, please! The algorithm could look a little bit more sophisticated,

    e.g. as follows:

      1. If the component is REPLACED, the current value is ALWAYS replaced

         by the VALUE attribute of the NEW component (in case such an

         attribute exists). If NO such attribute exists, proceed as

         currently implemented.

      2. If the component PACKAGE is changed AND the new package contains

         a VALUE attribute AND the current component's value has NOT been

         changed from its default, change the component's value to the

         new package's VALUE attribute. Otherwise, proceed as currently

         implemented.

      3. Same as (2), but for changing the TECHNOLOGY.

     

    The above would assure that component default values UNCHANGED by the

    user would automatically be changed to their new counterparts, and, in

    case the user DID change something, this change would NOT be destroyed.

     

    Andreas Weidner

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • CSWalt
    CSWalt over 14 years ago in reply to e14 Contributor

    Hello,

     

    On 04/02/12 10:29, Andreas Weidner wrote:

    Am 30.03.2012 16:45, schrieb Christian Bohrer:

    >> Currently, the VALUE attribute is always used to initialize the Value

    >> of a part in a schematic, whatever its status (ON / OFF).Very well!

     

    YES!

     

    >> The problem is that it only happens the first time the part is added

    >> in the schematic.

    >> If I replace the part or if I change its technology, its VALUE is not

    >> updated.

    >> The VALUE of the part remain this one of its first placement.

     

    That's NOT so nice...

     

    >> It is not only very annoying but it is also a source of errors!

     

    YES, that's quite definitely a source of errors!

     

    >> This is why I propose that the VALUE attribute (if exist) is also used

    >> to update the VALUE in the replacements and changes of technology.

     

    YES, please! The algorithm could look a little bit more sophisticated,

    e.g. as follows:

    1. If the component is REPLACED, the current value is ALWAYS replaced

        by the VALUE attribute of the NEW component (in case such an

        attribute exists). If NO such attribute exists, proceed as

        currently implemented.

    2. If the component PACKAGE is changed AND the new package contains

        a VALUE attribute AND the current component's value has NOT been

        changed from its default, change the component's value to the

        new package's VALUE attribute. Otherwise, proceed as currently

        implemented.

    3. Same as (2), but for changing the TECHNOLOGY.

     

    The above would assure that component default values UNCHANGED by the

    user would automatically be changed to their new counterparts, and, in

    case the user DID change something, this change would NOT be destroyed.

     

    Andreas Weidner

     

     

    Thanks for your ideas !

    Currently nothing in this direction happens, it was like this also in V5.

     

    This is a tricky and confusing topic. There are at least 2 more cases:

    1. The existing part/element's device has no attribute VALUE, but the new device has one.

    2. The existing part/element's device has no attribute VALUE and also no user defineable value.

     

    To make things simpler I tend to say that in any case (change package, technology

    and replace) the values get overridden if there's a VALUE attribute in the new device.

    In both case I would prefer to update the value by the VALUE attribute.

     

    So the general rule would be:

    If a user uses devices with an attribute VALUE by whatever command, he gets the

    value of VALUE as part/element value.

     

    This can be compared with the behaviour of other attributes:

    If a user has a part/element with a device with library attributes and changes this with

    replace/change package or technology, all attributes get replaced by the new

    package's or technology's attributes and their values.

    This is for library attributes, not for schematic or board attributes !

    These attributes will be kept in any case.

     

    Originally we thought that a device's value is something that should be defined in the

    schematic or board. Supporting value definition in the library by an attribute VALUE

    is more like a workaround and no standard case.

     

    Regards,

    Walter Spermann

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

     

    "Andreas Weidner" <andreas.weidner@aei.mpg.de> a écrit dans le message de news:

    jlbo1v$v68$1@cheetah.cadsoft.de...

    Am 30.03.2012 16:45, schrieb Christian Bohrer:

    >> Currently, the VALUE attribute is always used to initialize the Value of a part in a schematic,

    >> whatever its status (ON / OFF).Very well!

     

    YES!

     

    >> The problem is that it only happens the first time the part is added in the schematic.

    >> If I replace the part or if I change its technology, its VALUE is not updated.

    >> The VALUE of the part remain this one of its first placement.

     

    That's NOT so nice...

     

    >> It is not only very annoying but it is also a source of errors!

     

    YES, that's quite definitely a source of errors!

     

    >> This is why I propose that the VALUE attribute (if exist) is also used to update the VALUE in

    >> the replacements and changes of technology.

     

    YES, please! The algorithm could look a little bit more sophisticated,

    e.g. as follows:

    1. If the component is REPLACED, the current value is ALWAYS replaced

        by the VALUE attribute of the NEW component (in case such an

        attribute exists). If NO such attribute exists, proceed as

        currently implemented.

    2. If the component PACKAGE is changed AND the new package contains

        a VALUE attribute AND the current component's value has NOT been

        changed from its default, change the component's value to the

        new package's VALUE attribute. Otherwise, proceed as currently

        implemented.

    3. Same as (2), but for changing the TECHNOLOGY.

     

    The above would assure that component default values UNCHANGED by the

    user would automatically be changed to their new counterparts, and, in

    case the user DID change something, this change would NOT be destroyed.

     

    Andreas Weidner

     

    Thanks Andreas for your support.

     

    may be the diagram below would help to understand the problem (in red).

     

     

    begin 666 ScreenShot314.png

    MB5!.1PT*&@H````-24A$4@```N$```%'" (```" CP6K```>7$E$051XG.W=

    MX;&C1A8&4-B:0"84A)0)A2'XE F$T/;)8%A! T</OV.>5R:?0D!.K6Y:-I

    MH?[U>G4``,'\YD5``!8\>/I%2BI[_NG5Z$R1M&I8\=DZ^GZ0G?JKH/:.YO

    ME6KN5!FEZ[K7Z_?3JU"-OO_Y]"I421_[5M:>IB?LEZ /:.[]"C:W<ST`0$0R

    M"@`0D8P"`$0DHP``$<DH`$!$,@H`$)&,`@!$),``!') ! 1#(*`!"1C (`

    M1)3M]WJ@4LM?N#CP^R!]_].OBJ0Q=HG7Z_?8LIHX\V]2D:!$:%:?!M>4KP

    MLVV,IJT_MJPFSDISO-<#R31/%6)K-X.M[6Q"EI[@W&4: .TZ'@[M^Z-MRY

    MK&6S!W][)]',6F?6[LM&?-<]9H?F8U]:?16>HKE',@H$,JTI[\[[3(>"5T]:

    MSQZ\?,SVG00W:[YE(PX]9-G*^D"-&F]N&04"V9@H-XLO&_7E8]W9.-(BOEG[

    MIM[NWLLZ0.1-=[<,@J$LUITIH_&_] BH].[G7T@;HTU=PR"F2S>F*(JFT<

    M*.]O[O&\0%?;CJHUFGLDHVQ9GN:?/6#_7V>+W?E(FK4Q?GO^V@GOSB7IAT&L

    M3CLXO]B/R]$''J&Y-_2OUOI=2BF[_NR[_BR";>O8+'_A:'KX11L%?U_<],

    MK7/XGULLN2?PXUE\%V=C;<R3[!M1TX1OS6\XTDK9TZ[K"9.7^#G<6/U"

    MQT9SC[8?MO$]D>)J[P.:RL%F]LXREO2=1'Z<N5A%4B6"UGTSO_.H!'Q\

    M?2<1K,Z._'A[>R&KAT;Z0 2:>Y5KN)VUD6H__G6I[W\._TWOF=UOA@$`+3".

    MLFX:.6\;"_GXQ??9;9JU[!CPT>R02>?)+4=SRRB/6?:>\U]\IQ&Z!,?H.4U)

    MT-PRREM7GU)Y]Y6-2U\4`&HAHZSX'6>G7_Z->-!PLK`#1.1CFE8$ I^+JD

    MY+(Z.:P>?GS5E"<__JI'$.<_T2TTI8PRMSI-M9OTIW>SD)9?NMF^AMOJQ<Z7

    MWA9/K*%?LG2<G+2(Y?5X;S9)?B_>K?F9<V0!O'F4]TUTQ3RBASVU]2_^J)

    M!Q[Y<2'V-%"UPQ5F?/"9G=/)IQ-'(TTIHT#U5J]0N1R6$W#CV[[8Z/*1JRV^

    M_SK"VY<>GGFE^/V7*GQ[2>AW5Z1=/F#ZIRI:4T:!NKFL3AJK3;G:B-/S1,L6

    M7][HUOK Q@+?W>EJ"#?8WRY3>YKOJP4&(:- 35Q6)[?MBU:OWNZT>,WV?*)G

    M-KFMY.O]S_X3(U,1E=7*F3/&#"0)%7?R$[U\Y/[G5M&4,@K4S65U*,BD

    MD\=]]8G>/KLW/J;>-O6;@M *":8B9XZ/3[[NZ_5[^&]Z?R/?(JG"ZH55-EKG

    M79MN+#"._O5Z/;T.Q?1]7UU(?%#?_\S4^O=XL(_MF=4_,SNB>G#-\_6TDSUA

    M^]LZW:MNLD1\_C/[7W5ZG<WMO_9?I2J2LSU=X'KOC@[_]$?VR[C5ZQ>L_'

    M%3BI8'/*.VJO6H\0A\[(&5/R]H3-JXJ)J,\O18'G;E2W(E7-/<SO4`\('9

    MLCS"G%D`_C$[-6 :2@+-GUJ30Z040#XG^5LV6?6@WJ;43G>@" B&04`" B

    M&04`B$A&`0`BDE$`@(AD% `@(AD%`(A(1@$`(LKV>SU/KT)E,K7^/?2Q8_+U

    M-#WA6U7W`<W]+;\I6).^]SYS.=V,3C=H3/KF=JX'`(A(1@$`(I)1`("(9!0`

    M("(9!0"(2$8!`"*240" B&04`" B&04`B$A&`0`BDE$`@(AD% `@(AD%`(A(

    M1@$`(I)1`("(9!0`("(9!0"(2$8!`"*240" B&04`""B'T^O`%!,W_=/KP+/

    MTPU(0T:!)%ZOU].KP//ZOM<32,.Y'@`@(AD%`(A(1@$`(I)1`("(9!0`("(9

    M!0"(2$:YQ/;U"5R]```^DE&N\BZ(""@`L(>,<HGM:RBYPA)0BE%;$I-1+K2L

    M#NH%4)Q16[24:XUK1'J!5"<45L2DU&N,I:&(9J,`47)`(HS:DM,@I !D9M

    MR<<O9%YH62:\V\ 55D.)@D/MC-<2($`@,-D%("$'".1@(QRK6F94# BR@O

    MI"2C```1R2@`&1BU)1\9Y7)#L5 R`. K,@H`$)'KHUQK=M$"[S9P$=6&?'X\

    MO0)IC?7B[]__5(H_?O;#G6H'4-!06(92
    ?/?KBAVI" <93RENEDZH^??K@'

    M&.:3E8-!4>UH5(R2DG;Z61X0#.^)A.IA0<*B6C%/-5R1@H',"W#I2:P1\_

    M%7PJXWL]!?1]?ZQJC>-_4@IL$??]P?2R?3IJ@T5$:M/V7]R9YM)L"VP\,G

    M2T9PJ86,<E"I=#(EJ0!!=/)E*1"?#UZY()U,!S"X)U,3A$)J-\YX:2

    M,5 XH&6WE9J!Z;3$9,[L7H<GQAYC.BTTZ^3$V,,OJMH0C>S\V=4G=[:9I +M

    MN'GX9$:U(1H99<NSZ63J1_([=ET,J/@$(2,\E:HDC%0.""?@5FH.#P.+\I

    MN")LR?C[]\L/$T(:84O-Z._?K[YW*,MCS)G]/S=/C#W@[]\OTVFA=L/G-VR=

    M&8RKI]KP% 'Y'W&FGNQG@AO4*'XZ65)M>(2,4F4ZF7+.&&H1?)AV#P6'.[6>

    M414C('"`9&E34#!8=[M#L?)?[4DZ^8I (Q53'UY(!A.NW3:T%R+8ZCU'YR

    M9YO3QA#$>!3TQ\^$&:53;;A>6QDE=SJ9,A(STHY=K)*4N$ZK624=M)E*0"

    M]\MT$GD_284K-)%1VBP9(TD%[M%XJ1DH.!24?,YLLHFQQYA."U?+.C'V&--I

    M27M.$J;)W>V.;Z!XM)/C#W&J1^2)A1I)-MD@H488SV(TF%DU)E%.ED/TD%

    MSG!F9S])A</R9!3'--]2.. `I>: X4280R.^E6'.K(FQQ_@)9?B*B;&'C6_:

    M,)U6P6&GNL=1G-PIQ9@*;# QMJ!Q3$6UX:-:>XET<@4CL3!CC/8BCHO8H\J,

    MHFI<2E!3IVYA:3"MLHRBN&3>R@<-&Z<=^+DSM7&:M,I."Q4DU&DD_M)C3(

    MU)-'^.(/JRK(*-+)LR05&B&=/,YT6F9"=P7I) ['-R1FZDDHCHL8QSX<EEZJGNCAAL*!\J]VL[JLU.DDIZ_[GSQ?J^'P]KZOHD[#&]

    MEG-!U;U18..S0TW&_K>'FL[D/TD6HS&O-W[]?JDU-V64!.ED5A%N.. H

    M7H#N-$TJ3Z\+#1G3R;CK>GJ-CE!MOC*.8Z+\KDCHU1Z<N<K8Q$I<G#SQ\^

    MZI(Q,J#";:;I),?'YQW59I6DDM/2Y?>0CJYPGBJ^.D56#<EJ$S.&=,<<N)

    ML0K.?BFK3?=OKU!P:G=51DF93L;K/JT.O3HWO$%2X2*SB;%I/C6JS6&22B;E

    M,TK=+)M_P3[[3^E)ZE0T.RL8U\K%2;G69)1;6I5.'Y*+5/C/WHY"6TWYU(

    MWEYFCF'8D>FTG)1C8NQ'JLUYOF98NV+ILIWADX73MI_B:2=S\WZEKJ2"MJ

    M\9IL9Z@VI;B22J49)1VT@E7D%38H[5TPA4DE>J<RBC2":5(KPCG5"6I%*1

    M@QE%.N$*D@HS]5[/GN!4FRH<R2A1)3K))NRI_R=I!PA32E)G>1,8Y"(,F.

    M;'SCL2!)A5(RG>M)7V3,1R&$9.EDD+Y\W$]2X8Q,Z620OLB<NC[*Z_4:WITJ

    M?O'A\!J.3WQP&\^L?/#6&5=O[$[PSM!)@G?I3K6)9[IB2DU%"ES#K:ZD,C6[

    MKM&[AQWX/8L[KU2]\5KC]3=C_LJ:=,(QM225*=7F0=))O8I=9W::5$HMLZ#Q

    MER\.\'P<EG2"2>%3BJ31RSX9-G5X8#"O]>S] )JCAG/'3<:349O]PXO7-Y

    M.>KQ_G>W9TOK)F5T]3V9_G7C]NK2ME\K9A,<*QFK/_$SSHA2?=I42\%1;>YW

    M9NJ):A-'X=_K&40[]?/'VN]63'_I8_K_Z>=P>3 TNW_ZL1QOSWY#9'L(=/;7

    MU;6:C1)/R\&[UWKW#CSKS,F=U<</=RH9C0MUZD>U>;S:G)]ZHMK$4?YWCP?C

    M\<WRTQ7<[#!B]J$]MB';I7/VUW$%5HO=SC69'8H]_OZ7&FY-/XF=PVH94YE2

    M;<HZ,W:RI-I$<%5&&<1)*L\>8.W_A(_WO/NHKQY4[?SK(\J>#'Z]7AN%PV L

    M0P]Y]E.@VCRB^+P3U2:":S/8)I4[N_-RQ>-,ZP;79D,S,]C?WM7V\VGMDI

    MN,QWA6-ZIP.@ECU8<%2;1Y0=/IE2;1YWR7R45:'.&4_-SK^>7,[VTO8,PVX/

    MNKY;PO51X4CG4D^('PI'\<622<R"H]J4=7[JR4>JS;,>"(!W7IUV.<5]

    M.4U].GEM.<UM^Y_394Z/169#H*O/6EW)U=NCY>K-7NO=ZMU9.(J/N(YFQRO#

    M/\<[`Q[9!%D-[IFDHMIT-U:;Z\9.!K54F_1%YK'-<QW]?*Y+)X/EIW'Z%<$X

    M56,49#48U#6=EG>N3B>#6JI-^B+S\.:I&CE<G4X&VR>&XU2-49#58.30J';W

    ME)JNGFJ3OLB$V#Q)I6K7S3N9>C>+?E8L5A_SE/3EHU*22HWN&3X95%1MTA>9

    M0)LGJ53GMF.:2J4O'U53<&IQ9SJI3OHB<\=WCW>J\1),S9).J)V"$Y]T0L0(

    M9B0V,NEDO_2'.#DH. %))SNE+S)Q-\_Q3332R;?2EX],))4XE)K]TA>9Z)LG

    MJ01QS\389-7CWPDE6<9/OE6B)3Q9)@]R3'-8O*1E8)S/GDF/1%IJ;-

    M4SAN)IV<E+Y\)&9 Y3;2R1GIBTQEFZ=PW$,Z*2)]4A/P;F4=')>B)3Y>89

    M4F.=%)0^O1"$GE"@)$>F3,6;)ZD49V)L6>G1U,DE5DDX+2%YGJ-T]2

    M<PR172EX\&22IG2"?%I2\R239/4CE,.KE.^O1)C'E`.GD(NF+3K-Z_M>

    MU=A/.KE:O+1,DEE)GD4NF3;-,Z"RAW1RC_3E`TEEPS2==*K--=(7F9R;

    M)ZF\(YW<7WY8""I+!DN4?Z(I-Y\R25&5_;N5GZ\L%HC"E=\S5'.KE3B3

    M?/,Z2:7K.L,G#TE?/IAI/*E()_=+7V22;]ZHV:0BG3PH??E@58.G?J23IZ0O

    M,LDW;ZJUF"*=/"Y]^6!#(TG%Q-AGI2\RR3=OJ86D(IT$D;Y
    %'NI&+XY''I

    MBTSRS7LG<5(Q,3:.].6#/5).4I%.@DA?9))OWK9D2<7P233IRP?[I4DJTDDH

    MZ8M,\LW[,=(K'024_KRP;>JCC224#IBTSRS=NIW@$5Z22R].6#8ZIB;&

    MAI6R"3?O*_4E52DD_C2EP\.JC4C&3R-(7F>2;=T 52<7$V"JD+Q<%#RI

    M2"?QI2\RR3?OL!)Q?!)1=*7#XH(F%2DDUJDS+)-^^,:.>,I9/JI"\?%!0D

    MJ9AZ4I?T12;YYIT7(:E()Y57SXHZ]F8(IW4'V12;YYI3QUZD<ZJ5KZ\L$5

    M'DDJ3NY4GV12;YY9=V<5$R,K5WZ\L%U;DLJTDG5TA>9Y)MWA1N2BN&3'-7

    M#ZYV:5*13A)(7V22;]Y%KIND(IUDDKY\<(_B2<74DS32%YGDFW>ILDE%.LDG

    M??G@-J5BBG223/HBDWSS;G#^U(]TDE7Z\L'-3B85)W?R25]DDF_>;0XG%1-C

    M$TM?/GC$@:0BG625OL@DW[R;?954#)DE[Y
    *"=244ZR2U]D4F
    >??;,TE%

    M.FE$O+!LZ8QI5O4'%-/6I"R"3?O*>\2RK225/2EP\B6"85Z:0=Z8M,\LU[

    MUC2I2"<-2E\^B&.65 :Z7WKIBTSRS8M@K!W>ZM:D+Q]$H]JT)GV1^<_3*Y#?

    MT(%R=R,@`M6&9&04`" B&04`B$A&`0`BDE$`@(AD% `@(AD%`(A(1@$`(I)1

    M`("(9!0`("(9!0"(2$8!`"+Z\?0*M&OVZU]# RXB&I#I8RC/&;VZU]# RX

    MB&I#I624*-_Q#80A&I#9SK>=K]7I7):#L89G@<-4&VHDHX0PJQW3?PZW

    MQWO&V@%P@&I#1624A[T[N'E7'1S6`,>H-E1'1@EJ5AV&XK*\'^ DU8:PS)FM

    MQNOU&FL'P'54&X*04:(;RH1B`5Q-M2$:YWH>-A:%Z;#J] AF-M/>Z"MPC&I#

    M=624A[VK`LLSQ+>L#I"6:D-UG.L!`"*240" B&04`" B&04`B$A&`0`BDE$N

    ML7V!`9<?`("/9)2KO LB`DIBLBE 03+*);8O,.#R`XG)IL!U6CL0DE$NM.PN

    M3H04]T=Y5.X%2FCH0DE&N->TT3L0'VEWH)36!NEEEO,?OEB8L8)":7

    M<)O6!O_I6AJDEU&@)-F4S4U,^@D4%Z&>56=E1 669!M::I`R$9Y4(I>PP'

    MZ G<+/&!-4V14: PB81'R"4MRUIV9)1K3?M-UCX$/*NIP7^ZEEI61H'R9%.

    M\V04@(2$X]P:.1"242XW])[$?0AXG I#2C>7H&[/36M[/[75;.>]7J]K[7

    M"@"'Y<\HLW#PUNOAU;D;K,-;WQG*9N2WA"+Q]O/K@PW:.% *&U&&3K[822

    MF=F&MU:\9--!(\T-$3QR+'3SB]Y<4A)FE*'!VMDG[32^(;FO/BF;-IY-X6;3

    MB-!"V9EN[PU5)=4PD72RWY_]GUVN_9;6WY:OQ5F5?O _"(=#W;]5I;NRL"3I

    MS?9/Q38;VG]_7*T>(WR702VV5ZDX"Q=5U@RG.OIUYW.69XW^H]\%(LOC6V

    M>-?P/N8V_S<J_NO7<RMRB9O'_"-0<-ZYKK#4NG,:"2A%_-G_65U/T/0GU=CH

    M5?C?'!TN>2=_M\MS=JCI)/]RHZI5)Q1=)JRZCH+( 4(::4]<]Q9#/19&D(

    M\DZE6IS0G:4FM&T6DN$GG)9N655<V#4LZF<J45.QK#BNR-ZDRH@TEXH<

    M4S3]12(W>G#2R3NU)Q6'0^>=/P2JZ/82]T@YAYTU\J9J,'U_>]=+*M__6K

    MQGZEVA1TIK94]IN"LT]_GK]%>VKDIK:@$;/3@!98_7KU_5]2O5IJPSM:6R

    MC$;E(Q[B"G["2C[U1535)LK'XM-6447>=.<797VOU.<=H],@'E6[7$%-7F

    M.L=J2S491=>YG]T5+ DHQ]024PBECHPBH#SE\9BBZ>_W>*-')J"<$3RFJ#97

    M.U!;ZL@HM$G)>(J8LDI .2]L3%%M[O%M;:D@H^@ZS[*[@DY 2=L3"&@"C(

    M;9)-GR6;T@[5YDY?U9;H&477B<#NBL891"G+4 H[1<\HM$DVC4 VI06JS?WV

    MUY8?5Z_*&2>[SO!+`=WD!Q>6]PQWSOZY?,SVTE85[/3C&LY6]4Y#EZKQFM:C

    M97L=>S//M,P#A^[%J'$'$3I?_TN%;[#4,I59>4)46FN,SC*$-C3)MD><^>

    M9WU<VO3&^,\]IAUZ(_&,`67G8K]]<#07'=8LF^G8NW1FW5:?NZ=;/L502DS]

    M7>GDMA=Z2MEJH\CLM[.V9,XH>PQQM?@>_;I=+ 5=T?1[5)T@6W/=(,J9W7_5

    M(RBC%F:E*#(GQ3W74R3>#OUC>G;FZCW]QDO,1MN&?TY#TNR<SCADMWHV:KJ0

    MV>W9TI8O?4R"TSU+RQXRO?_=[8]G#Y=W;KSHU.HIQ6EGZ-;&<NL=R&W9Z]>O

    M(:9,`\<87,:_F]/%S)=PFQI[Y[2_7N>:/O5QW_6?EI<8K,&7$SR@W&)MQH

    MSJ^6MN>UQMO3%YW>7N:5U>5,%S\Z5VLN3FEG?3@_7E&[5LH-GIN>4;N_/=

    M7NURJRO03K#[(6N;M^4V32(9;88HL/L]C0ES!#NRBS\919\EC>&&_/7CJ?

    MZN-(C-;PXUI>F,4M9JI)C]=>=RIIU@UF6/=8XTXWY7^_A&O1NY73W@V+.H

    MZ1.7C;OG,?M?D6_=,UMV&1%6'_"M=^>20B6/E#-GMRDR7\F?4:;A=/G6WSD3

    MY<$=2?"QDSAF;]1VY]FYD(TQTN62[Y]AQ-FYUS>#9]\N]@@*8091>8K3/*

    M.]N#8!\??.;E'/7&<</)KWE3X9=)6&>$O'O8F;#"LQ29,X)^KZ?X]\'.

    M])9^<E_>>M7_Y!Y[U;CG;2SO9*?Z^)NH-Y\>WDZEWR[J\$(*;G(518?!

    M..>CX *[M1!S/M:D#$;W5!M%9MO'?4K0$X'%>\^[P:Z=B?+

    5YI.<1W_
    M.IL#NWRYU3&]Y539Z9+?/>

    N8/_L_K^LSEU:-93-MM-'L[7WW3FXTQ_[E3U]B

    M8S[3]EL]IF<OW;8ZT75I-NMV=<1E]:M W=K7A99/V3G2<U_Z]?]

    MO>N:J/('+!=6UK))12;T;A#!F%ZZ3)*!RP75N"GNL!`!HGHP``$<DH`$!$

    M,@H`$)&,`@!$E"JC;']_^-LOET\O>G-\G7:\T$7:N52&=G_V%8F@R"5,4EX'

    M)8BG\IV"DNJC/Q6GO#C>E[O>?J.F<N_K9<VCV:VE%I]^5TY3M;$S>0@H

    M%SEP$+7]R82]",\GJ]GJVV9;\W?_\/`5[TO?_T%\G0[JO2M_NJU^M5RVZ[

    MR'5<GKH8S",71^ENW,L4_U2F*2S=CMJ2ZO=ZIM?1FUW%=7;G[)'=I\OVK?X0

    MY?839R\TO7/GY0*7FS![_,8U`5=?\;J+SY;R>KT.7%A)N[];C5K:G='TNJZS

    MV^-E89?7GUV](NUT(=O7G[WG8K()O/M8K5:>;L<'?UDN%):9/!EE-@ZVNM_J

    MUBX8WRVZR&H3=HO=WO83_UK[M<GE#O=TZ>O..T*T\6.MS^NQOVQY>NA7;?

    M6(WE[33MGM7LO3]6LY8O3$\999%7FN_GSR[O5P([ZQK#:.?SX6G(U/L<(R

    MR)-1IB%Q1Z].R!>YLJ/C]G8F7U<P6=>YZ^['][EOS1_C6/3+M_*T>[-V66

    M,]X]H-LW%K+QTS]BR@&KE6?Y@&[?!U9AF<F344[:?ZN[@7/O.[7CL^\EW:

    MO>*ET]/N;!A./M9U$N1CS@BU.4]-1AD<.[E\QL</;%.%Y<\=$]WB9I0[>\_)

    MMKG.SO1]S_KOZ4_G:?>NR7:GB-5Y)P3Q>,$)55AV"OJ]GAL<>.NW6^[=`O<?

    MJ:^7,&]]?3LZ?9)Z;=-UZ:4/K%7).=C]QXS,8]>Q;":/:QVO@TO?L`AS

    M?<_'%_JXP!H+2Q_Y".FKXF-:0>K=[Z;[/?;#[4<E6W7^CCT[?MG!XQFR2U

    MNKO==*W'4]K]PV)VSVLT_WC)-+9M-C-[[7\V[JZ_)9&]_KV9[U4MRS)WK^

    MMQI?#MPN/U;CN9N_S]6JX^<FIUWMOXIXW7G3V]RUM80F>4[OO>PT5NWE%I

    M]R $E.Z)C+R#O>FAWM4FE&6MN?,LFIG;6GW7 _ 'A5=STB00)*%^"2H0W:

    M?_ 3/:/H/1'<?S"MW2,PB!$F21[9ENPF%QO]<#$,2S7T)VEN=J9[Y.Z"S/

    MM[XZ(DCM(YI'[:4P?3VOU9!E& QU6040`>9U9**=$&408.BN[Q[<%/'1E%

    M[WGLP?3VOTI!E%6B2GGQ0PH`P7G:@<2QT9I=-[GA!A1Z7=[Q>AW<,24\Z(

    M'%"(J9J,TME=W<N."E:)<=4$5#L9:YS;)]24T:A3:K&G633/<24;U414 8

    MSA4.%Y;*,HK><X]H.RKM?H]H[1Z9F)?10%EH."4=::P1\6_BH72K]4V!V5

    M=K]4V':/,)E\H.KJ",^K[O7/[DG"'JG>D`56:4SN[J,L%W5-K](L';/;)A

    M3R:I+/WS4X65]RLUY[ B5:76C-()N:6=#[SW4#*$U#.DU2F<J23D9IS0FJ

    M4G%&&>@]1=2UEQ)/2ZDEF-9"4DF63D9JSGYEJTKU&:434TZK*Z",M/M)E;9[

    M?,/K&LIK(S3AW/W*$EEVQ7'/!DR2J?K'%7[8;1V/Z;V=J_%&%:ZC'EEK6F

    MIOJ2LK-T74E)DE$&NLY^F?92VGV_3.U>EVE>R:'Q7C0V:,N59_R&]G6=(55&

    M&=AC;<NZE]NV[V.SQKFCY;J#_3\?<4$\29I2!D#MS0^"-0O/--+N$$&^

    MT;EFRM)VHPRFG6:=G9=LLDIF_H&>T:W=@4SR9Y29%GNH66W:;=`:K3

    L7$8!`I0V6\`@"-D%$`@(AD% `@HO\"RY=4&>T-=BL`````245.1*Y"8((`

    `

    end