Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Library Problems
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 371 views
  • Users 0 members are here
Related

Library Problems

e14 Contributor
e14 Contributor over 14 years ago

I have a library (lib file) that I am adding parts to.  It was

originally created under Eagle 5.

 

I added a new IC to this library file, during a trip, using Eagle 6.1.0

Professional on a laptop running Windows 7 32 bit.

 

Now, when back at work, I copy the library file to my desktop computer

running Eagle 6.1.0 or 6.2.0 Professional, the new I.C. is not visible,

but all the older parts are still there in the library.  The desktop

computer is running Windows 7, 64 bit.

 

When I look in 6.1.0 on the laptop, in the same file, the new part is

there.  When I look in 6.1.0 or 6.2.0 on the desktop computer, the new

part is not there.

 

This is a large IC, that took several hours to create the footprint,

symbol, part, etc.

 

I have already spent several hours more going back and forth from the

laptop to the desktop to make sure that I have the correct version of

the file, and copying several times, to the lib file inside of the

Program files folder as well as trying to put it in the lib file in

the %appdata% folder.

 

How do I get my new part to be usable on my desktop Windows 7 64 computer?

 

--- Graham

 

==

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I have sorted out the problem.

     

    There are now two copies of the library file in the laptop.

     

    The original unmodified copy of the library is (still) located at:

    C:\Program Files\EAGLE-6.2.0\lbr

     

    The modified copy of the library is located at

    C:\Users\UsersName\AppData\Local\VirtualStore\Program Files\EAGLE-6.2.0\lbr

     

    When Eagle modifies a library, it generates a changed copy, but

    does not put the "lock" symbol on the file to warn you that it is using

    the copy in the virtual store, rather than the original.  And it does

    not remove or destroy the original, or tell you which one it is using.

     

    I now have things working.

     

    Thanks,

    --- Graham

     

    ==

     

    On 4/23/2012 12:53 PM, Graham wrote:

    I have a library (lib file) that I am adding parts to. It was originally

    created under Eagle 5.

     

    I added a new IC to this library file, during a trip, using Eagle 6.1.0

    Professional on a laptop running Windows 7 32 bit.

     

    Now, when back at work, I copy the library file to my desktop computer

    running Eagle 6.1.0 or 6.2.0 Professional, the new I.C. is not visible,

    but all the older parts are still there in the library. The desktop

    computer is running Windows 7, 64 bit.

     

    When I look in 6.1.0 on the laptop, in the same file, the new part is

    there. When I look in 6.1.0 or 6.2.0 on the desktop computer, the new

    part is not there.

     

    This is a large IC, that took several hours to create the footprint,

    symbol, part, etc.

     

    I have already spent several hours more going back and forth from the

    laptop to the desktop to make sure that I have the correct version of

    the file, and copying several times, to the lib file inside of the

    Program files folder as well as trying to put it in the lib file in

    the %appdata% folder.

     

    How do I get my new part to be usable on my desktop Windows 7 64 computer?

     

    --- Graham

     

    ==

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robotonics
    robotonics over 14 years ago in reply to e14 Contributor

    Hi Graham

     

    Thanks for the info, I am upgrading to 64 bit soon, so will at least know what to look out for! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to robotonics

    Best I can tell, Eagle 6.2.0, both 32 bit and 64 bit now conform to the

    Windows 7 security mechanism, such that programs without administrator

    privileges can not modify files in the Program Files area.  I find the

    method that Microsoft used to enable this convoluted, and the (hidden)

    location where it puts the modified files quite obscure.

     

    Since I need to routinely move files between machines, particularly

    when they are actively being built and tested, I would rather see Eagle

    place the lib, cam, dru, scr and ulp files in the same location in the

    eagle documents as the projects.  Any files that a user would normally

    be expected to modify.  Everything except the binaries and Docs.

     

    Nothing that a user would normally be expected to modify should be

    located in the Windows system security protected area.

     

    --- Graham

     

    ==

     

    On 4/24/2012 2:36 AM, David Cotterill-Drew wrote:

    Hi Graham

     

    Thanks for the info, I am upgrading to 64 bit soon, so will at least know what to look out for! image

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to robotonics

    Best I can tell, Eagle 6.2.0, both 32 bit and 64 bit now conform to the

    Windows 7 security mechanism, such that programs without administrator

    privileges can not modify files in the Program Files area.  I find the

    method that Microsoft used to enable this convoluted, and the (hidden)

    location where it puts the modified files quite obscure.

     

    Since I need to routinely move files between machines, particularly

    when they are actively being built and tested, I would rather see Eagle

    place the lib, cam, dru, scr and ulp files in the same location in the

    eagle documents as the projects.  Any files that a user would normally

    be expected to modify.  Everything except the binaries and Docs.

     

    Nothing that a user would normally be expected to modify should be

    located in the Windows system security protected area.

     

    --- Graham

     

    ==

     

    On 4/24/2012 2:36 AM, David Cotterill-Drew wrote:

    Hi Graham

     

    Thanks for the info, I am upgrading to 64 bit soon, so will at least know what to look out for! image