How would one change the default shape of a via?
The user manual describes some properties in .eaglerc, but I have not
found one related to the default via shape.
Thanks,
- Chuck
How would one change the default shape of a via?
The user manual describes some properties in .eaglerc, but I have not
found one related to the default via shape.
Thanks,
- Chuck
On 4/24/2012 11:13 AM, Chuck Huber wrote:
How would one change the default shape of a via?
The user manual describes some properties in .eaglerc, but I have not
found one related to the default via shape.
Thanks,
- Chuck
Hi Chuck,
Use the eagle.scr file found under the scripts tree in the control
panel. Go ahead and open it and on the next line after BRD: type in the
following.
CHANGE SHAPE ROUND;
Instead of round you can put SQUARE, OCTAGON, etc.
Save the eagle.scr file. This script file is special because it runs
every time a new editor is opened, so it's good for setting up defaults
like this. By putting it after the BRD: heading it will only affect the
board.
hth,
Jorge Garcia
On 04/24/2012 01:27 PM, Jorge Garcia wrote:
On 4/24/2012 11:13 AM, Chuck Huber wrote:
>> How would one change the default shape of a via?
>>
Hi Chuck,
Use the eagle.scr file found under the scripts tree in the control
panel.
...
This script file is special because it runs
every time a new editor is opened, so it's good for setting up defaults
like this.
Good morning, Jorge,
Thanks for the tip. It worked exactly as described.
Do you know of a user-specific file that could be edited in a similar
manner, perhaps a file that doesn't get overwritten on each update/upgrade?
Thanks,
- Chuck
Chuck Huber wrote:
Do you know of a user-specific file that could be edited in a similar
manner, perhaps a file that doesn't get overwritten on each
update/upgrade?
Thanks,
- Chuck
You can place your preferences into a script and give it a unique name.
Locate it in a personal path for scripts.
Then in eagle.scr add the line to call your script.
In this way should the next versin of eagle overwrite eagle.scr all you have
to do is add one line to the new eagle.scr to call your script
Remember eagle.scr is not run in all cases when opening a design file. Some
people add a custom menu item in the text command menu so that with one
click you can run that script and get back your default settings
HTH
Warren
--
Viewed / responded via the newsgroup at
news.cadsoft.de
I added
CHANGE SHAPE ROUND;
to the BRD section of my eagle.scr file, but it didn't set the default via to round. Is there a way to verify if the eagle.scr file is used when I open eagle? I've got the Eagle Scripts directory setup like this (I'm on a mac):
$EAGLEDIR/scr:/Users/Scott/Documents/Eagle/scr
The path + filename is:
/Users/Scott/Documents/Eagle/scr/eagle.scr
I'm on Eagle ver 7.3.0
I added
CHANGE SHAPE ROUND;
to the BRD section of my eagle.scr file, but it didn't set the default via to round. Is there a way to verify if the eagle.scr file is used when I open eagle? I've got the Eagle Scripts directory setup like this (I'm on a mac):
$EAGLEDIR/scr:/Users/Scott/Documents/Eagle/scr
The path + filename is:
/Users/Scott/Documents/Eagle/scr/eagle.scr
I'm on Eagle ver 7.3.0