While reflecting why I actually wanna have the "attributes" in the
property dialogue of a part editable directly in the property dialogue
itself, I actually found out what annoys me most on the current
"attribute" dialogue.
That is, for simply changing a value in an already populated list, you
have to select the line with the value you wanna change in it,
doubleclick it, which leads to the opening of a sub dialog where I again
have to select the value, edit it, select if I wanna have it visible or
not and so on.
This would be much more easy if you could just type directly in the
dialog and just tick the corresponding checkboxes if you wish to have
them visible.
I made a mockup dialogue how I imagine this could look like.
Maybe there could be a "All Names visible" and "All Values visible"
button to check/uncheck all boxes in the corresponding columns.
95% of all time I edit attribute values that have been pre-created for
each part with a script in advance, so the focus of the dialogue should
be more on make changes easy, than on make creation of the attribute
structure easy (e.g. add new attributes).
Markus Rudolf