EAGLE User Support (English) New installation of Eagle 6.2.0 crashing
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
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 704 views
  • Users 0 members are here
Related

New installation of Eagle 6.2.0 crashing

Former Member
Former Member over 13 years ago

I've put a new instalation of Eagle 6.2.0 on a windows 7 PC.

It will bring up a project, but will crash on the first interaction with the design. It quietly closes out without warning or error message.

 

Being new to Eagle (but a user of many other CAD systems) I don't know where to start looking for a fix, so I've posted this message here.

 

Any clues?

 

Thank you,

David

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 13 years ago

    On 5/21/2012 5:32 PM, David Johnston wrote:

    I've put a new instalation of Eagle 6.2.0 on a windows 7 PC.

    It will bring up a project, but will crash on the first interaction with the design. It quietly closes out without warning or error message.

     

    Being new to Eagle (but a user of many other CAD systems) I don't know where to start looking for a fix, so I've posted this message here.

     

    Any clues?

     

    Thank you,

    David

     

     

    The output of the system log show a memory fault:

    -

     

    Or in the 'friendly' window:

    Faulting application name: eagle.exe, version: 0.0.0.0, time stamp:

    0x4f86f08b

    Faulting module name: eagle.exe, version: 0.0.0.0, time stamp: 0x4f86f08b

    Exception code: 0xc0000005

    Fault offset: 0x0024527e

    Faulting process id: 0x568

    Faulting application start time: 0x01cd37b6f8429ace

    Faulting application path: C:\Program Files (x86)\EAGLE-6.2.0\bin\eagle.exe

    Faulting module path: C:\Program Files (x86)\EAGLE-6.2.0\bin\eagle.exe

    Report Id: 4128e86b-a3aa-11e1-9e9a-68b599eefd97

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    On 22.05.2012 03:11, David Johnston wrote:

    On 5/21/2012 5:32 PM, David Johnston wrote:

    >> I've put a new instalation of Eagle 6.2.0 on a windows 7 PC.

    >> It will bring up a project, but will crash on the first interaction

    >> with the design. It quietly closes out without warning or error message.

    >>

    >> Being new to Eagle (but a user of many other CAD systems) I don't know

    >> where to start looking for a fix, so I've posted this message here.

    >>

    >> Any clues?

    >>

    >> Thank you,

    >> David

    >>

    >

     

    Or in the 'friendly' window:

    Faulting application name: eagle.exe, version: 0.0.0.0, time stamp:

    0x4f86f08b

    Faulting module name: eagle.exe, version: 0.0.0.0, time stamp: 0x4f86f08b

    Exception code: 0xc0000005

    Fault offset: 0x0024527e

    Faulting process id: 0x568

    Faulting application start time: 0x01cd37b6f8429ace

    Faulting application path: C:\Program Files (x86)\EAGLE-6.2.0\bin\eagle.exe

    Faulting module path: C:\Program Files (x86)\EAGLE-6.2.0\bin\eagle.exe

    Report Id: 4128e86b-a3aa-11e1-9e9a-68b599eefd97

     

     

    These error messages do not help much. Was there already an older EAGLE

    version installed on this computer? Is there already a file named

    eaglerc.usr on the system?

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    On 22.05.2012 03:11, David Johnston wrote:

    On 5/21/2012 5:32 PM, David Johnston wrote:

    >> I've put a new instalation of Eagle 6.2.0 on a windows 7 PC.

    >> It will bring up a project, but will crash on the first interaction

    >> with the design. It quietly closes out without warning or error message.

    >>

    >> Being new to Eagle (but a user of many other CAD systems) I don't know

    >> where to start looking for a fix, so I've posted this message here.

    >>

    >> Any clues?

    >>

    >> Thank you,

    >> David

    >>

    >

     

    Or in the 'friendly' window:

    Faulting application name: eagle.exe, version: 0.0.0.0, time stamp:

    0x4f86f08b

    Faulting module name: eagle.exe, version: 0.0.0.0, time stamp: 0x4f86f08b

    Exception code: 0xc0000005

    Fault offset: 0x0024527e

    Faulting process id: 0x568

    Faulting application start time: 0x01cd37b6f8429ace

    Faulting application path: C:\Program Files (x86)\EAGLE-6.2.0\bin\eagle.exe

    Faulting module path: C:\Program Files (x86)\EAGLE-6.2.0\bin\eagle.exe

    Report Id: 4128e86b-a3aa-11e1-9e9a-68b599eefd97

     

     

    These error messages do not help much. Was there already an older EAGLE

    version installed on this computer? Is there already a file named

    eaglerc.usr on the system?

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    On 5/23/2012 2:40 AM, Richard Hammerl wrote:

    On 22.05.2012 03:11, David Johnston wrote:

     

    >> Exception code: 0xc0000005

    >> Fault offset: 0x0024527e

     

    >

    These error messages do not help much. Was there already an older EAGLE

    version installed on this computer? Is there already a file named

    eaglerc.usr on the system?

     

    >

     

    There was no older Eagle system. It was freshly purchased, downloaded

    and installed.

     

    The two numbers above tell you that the eagle executable is making an

    access to an illegal memory address (generally due to bad pointer

    arithmetic). The offset tells you where in your code the erroneous

    access is happening. Only you can determine what the offset refers to

    because it's your code. No one else can.

     

    As is stands, it is wasted money. The software doesn't even begin to work.

     

    I since decided to try and run it on Linux. After fixing your broken library build script to get 32 bit libraries built so eagle would link the shared libraries, I get this:

      # /usr/local/eagle-6.2.0/bin/eagle

      Segmentation fault

     

    I'm starting to see a pattern here. Regardless of the machine or the operating system, your software segfaults. You need to improve your Q&A or give me a refund.

     

    Message was edited by: David Johnston

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Do you have any update for me?

     

    It is still segfaulting. It is still useless. I'm rapidly turning into a very annoyed customer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    On 5/25/2012 2:25 PM, David Johnston wrote:

    Do you have any update for me?

     

      It is still segfaulting. It is still useless. I'm rapidly turning into a very annoyed customer.

     

     

    Hi David,

     

    Try downloading it again, in the error message you posted it doesn't

    specify a version for the executable of EAGLE which leads me to believe

    that the exe is somehow corrupt or missing code.

     

    How big was the file? It should be in the neighborhood of 40MB.

     

    Word to the wise, the Program Files(x86) folder has some restrictions

    that mess with EAGLE so let EAGLE install into the Documents folder to

    avoid issues.

     

    hth,

     

    Jorge Garcia

    Cadsoft Support