Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Multiple(non standart) footprints
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 603 views
  • Users 0 members are here
Related

Multiple(non standart) footprints

e14 Contributor
e14 Contributor over 14 years ago

Good Day.

I have a two questions:

1) I want to put several different footprints on the PCB for one part on the scheme.  For example ATmega32U4 in QFN/TQFP package or a trimmer in vertical/horizontal package.

How can I do this?

 

2) In my scheme I have a  transistor which I need put on the big heat sink. Transistor will be connected  to the connector on PCB.

How can I add a part on the scheme but hide them on the PCB?

  • Sign in to reply
  • Cancel
  • dukepro
    dukepro over 13 years ago

    On 05/25/2012 03:10 PM, Nifril wrote:

    Good Day.

    I have a two questions:

    1) I want to put several different footprints on the PCB for one part on the scheme.  For example ATmega32U4 in QFN/TQFP package or a trimmer in vertical/horizontal package.

    How can I do this?

     

    I have done the same thing on several occasions.  Once you have your

    part established with the desired footprints in the library, you need to

    add the part to the schematic twice - once for each footprint.  You can

    place both symbols directly on top of each other do that all connections

    will be identical.  I smash the symbol and move each reference (U1, U2,

    or R1, R2) so they don't overlap.  I then add a note to the schematic

    that only one of the two parts will be populated.

     

    2) In my scheme I have a  transistor which I need put on the big heat sink. Transistor will be connected  to the connector on PCB.

    How can I add a part on the scheme but hide them on the PCB?

     

    There are a couple of ways to approach this determined by whether or not

    you want to show the connector in the schematic for BOM purposes or not.

     

    If you want to show the connector, the add the connector as expected in

    your schematic.  In your library create a device that has just the

    symbol of the transistor - no packages defined.  Then add that device to

    your schematic.

     

    In the case where you do not want to show the connector, you can create

    a variant of the transistor device that has the connector's footprint,

    then add that device/package to your schematic.

     

    HTH,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    On 25.05.2012 21:10, Nifril wrote:

    Good Day. I have a two questions: 1) I want to put several different

    footprints on the PCB for one part on the scheme.  For example

    ATmega32U4 in QFN/TQFP package or a trimmer in vertical/horizontal

    package. How can I do this?

     

     

    Hi,

     

    when you create a Device in the library you can assign different

    package variants. Therefore you have to click onto the "New" button

    and choose a package from the list. Be sure to type in a variant

    name, as well. Then click OK and the package available. When you

    click onto "New" again, you can select another package.

     

     

     

     

    2) In my scheme I have a  transistor which I need put on the big heat

    sink. Transistor will be connected  to the connector on PCB. How can

    I add a part on the scheme but hide them on the PCB?

     

     

    You could define a kind of dummy part that has no real pins in the

    symbol. So you do not have to assign a package. You could place vias

    in the layout then for connecting the transistor with the board.

    Alternatively use a transistor symbol and assign it to a connector

    package.

     

    Hope this helps.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/