Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Multiple(non standart) footprints
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 603 views
  • Users 0 members are here
Related

Multiple(non standart) footprints

e14 Contributor
e14 Contributor over 14 years ago

Good Day.

I have a two questions:

1) I want to put several different footprints on the PCB for one part on the scheme.  For example ATmega32U4 in QFN/TQFP package or a trimmer in vertical/horizontal package.

How can I do this?

 

2) In my scheme I have a  transistor which I need put on the big heat sink. Transistor will be connected  to the connector on PCB.

How can I add a part on the scheme but hide them on the PCB?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    On 25.05.2012 21:10, Nifril wrote:

    Good Day. I have a two questions: 1) I want to put several different

    footprints on the PCB for one part on the scheme.  For example

    ATmega32U4 in QFN/TQFP package or a trimmer in vertical/horizontal

    package. How can I do this?

     

     

    Hi,

     

    when you create a Device in the library you can assign different

    package variants. Therefore you have to click onto the "New" button

    and choose a package from the list. Be sure to type in a variant

    name, as well. Then click OK and the package available. When you

    click onto "New" again, you can select another package.

     

     

     

     

    2) In my scheme I have a  transistor which I need put on the big heat

    sink. Transistor will be connected  to the connector on PCB. How can

    I add a part on the scheme but hide them on the PCB?

     

     

    You could define a kind of dummy part that has no real pins in the

    symbol. So you do not have to assign a package. You could place vias

    in the layout then for connecting the transistor with the board.

    Alternatively use a transistor symbol and assign it to a connector

    package.

     

    Hope this helps.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    On 25.05.2012 21:10, Nifril wrote:

    Good Day. I have a two questions: 1) I want to put several different

    footprints on the PCB for one part on the scheme.  For example

    ATmega32U4 in QFN/TQFP package or a trimmer in vertical/horizontal

    package. How can I do this?

     

     

    Hi,

     

    when you create a Device in the library you can assign different

    package variants. Therefore you have to click onto the "New" button

    and choose a package from the list. Be sure to type in a variant

    name, as well. Then click OK and the package available. When you

    click onto "New" again, you can select another package.

     

     

     

     

    2) In my scheme I have a  transistor which I need put on the big heat

    sink. Transistor will be connected  to the connector on PCB. How can

    I add a part on the scheme but hide them on the PCB?

     

     

    You could define a kind of dummy part that has no real pins in the

    symbol. So you do not have to assign a package. You could place vias

    in the layout then for connecting the transistor with the board.

    Alternatively use a transistor symbol and assign it to a connector

    package.

     

    Hope this helps.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/