Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Pad Dimension Errors - New User
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 436 views
  • Users 0 members are here
  • clearance
Related

Pad Dimension Errors - New User

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I'm new to Eagle.  I've searched for an answer to this, but maybe I don't know enough to search for the correct terms.

 

I built a package in the library for a through hole header with 1.27 mm spacing and 0.7 mm holes, as per the manufacturer's datasheet.

 

If I allow Eagle to set the pad size, it sets it to 1.2 mm.  That leaves only 0.07 mm of spacing between pads -- not enough.

 

If I manually set the pad size to 1.0 mm in the library, it does not change in the board and I stll get DRC errors.

 

I've gone through the DRC dimensions and sizes and don't see anything that would cause this.  Besides, it seems to be elsewhere because the change in the board occurs before I do a DRC.

 

Can anyone give me pointers or direct me to documentation that would help me?

 

Thanks!

 

Dave

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Do not use the "auto"-parameter for the pad-diameter. The DRC changes all

    auto pads image

    Always set your own pad diameter.

    r

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Do not use the "auto"-parameter for the pad-diameter. The DRC changes all

    auto pads image

    Always set your own pad diameter.

    r

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for the reply.  But I said:

     

    "If I manually set the pad size to 1.0 mm in the library, it does not change in the board and I stll get DRC errors."

     

    So setting the pad size manually doesn't work for those dimensions.

     

    Dave