Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) High Current Traces
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 190 subscribers
  • Views 4408 views
  • Users 0 members are here
  • current
  • trace
  • width
  • high
Related

High Current Traces

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I'm a new Eagle user, but I suspect this is actually a more complicated question.

 

I have traces that will carry up to 2 amps.  Those traces also control various FETs and other signals.  If I set that net node to the trace width for the high current, all of the net gets set to that width and I don't have room to route my board.  I've already re-arranged all my components so that the wide traces are short and the pins near each other.  I've even gone from 4 layers to 6 layers.  (The board routes just fine with 4 layers by 7 mil traces.)

 

I don't see a way to set the width of signals before routing, and after routing is too late.  One idea is to isolate the low current part of the net from the high current with a 0 ohm resistor, then after routing fill in will a trace.  But even that seems a little clumsy.

 

I'm considering going to thicker copper layers so that I can reduce the trace width, but I haven't tried that yet.

 

Does anyone have any ideas on how I might solve this problem?

 

Thanks,

 

Dave

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 6/9/2012 2:59 PM, Dave Wills wrote:

    Hi,

     

    I'm a new Eagle user, but I suspect this is actually a more complicated question.

     

    I have traces that will carry up to 2 amps.  Those traces also control various FETs and other signals.  If I set that net node to the trace width for the high current, all of the net gets set to that width and I don't have room to route my board.  I've already re-arranged all my components so that the wide traces are short and the pins near each other.  I've even gone from 4 layers to 6 layers.  (The board routes just fine with 4 layers by 7 mil traces.)

     

    I don't see a way to set the width of signals before routing, and after routing is too late.  One idea is to isolate the low current part of the net from the high current with a 0 ohm resistor, then after routing fill in will a trace.  But even that seems a little clumsy.

     

    I'm considering going to thicker copper layers so that I can reduce the trace width, but I haven't tried that yet.

     

    Does anyone have any ideas on how I might solve this problem?

     

    Thanks,

     

    Dave

     

     

     

    Help -> Net Class

     

    You can create net classes with all the traces in the same class having

    various common properties including width and clearance from other

    conductive elements.    Good for high(er) current and also high voltage.

     

    Jim

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Jim,

     

    I've done that.  I have a separate net class for the high current traces.  The problem is one net goes to a few high current nodes (output of high current supply, connector, resistor, FET) but it also goes to a bunch of places that are not high current (but still the same node).  So the high current pins on the node need to be connected with wide traces, but the signal level pins do not.  If I allow all of the pins to be high current traces, I can't get it to route.

     

    That's why I said I could split the high current and signal level pins on the net with a 0 ohm resistor.  Then Eagle wouldn't automatically make all the traces high current traces.  But that sounds like a clumsy solution.  Seems better to make the copper thicker then make all the traces less wide.

     

    Thanks for the suggestion.

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Dave Wills wrote:

    Hi Jim,

     

    I've done that. I have a separate net class for the high current

    traces. The problem is one net goes to a few high current nodes

    (output of high current supply, connector, resistor, FET) but it also

    goes to a bunch of places that are not high current (but still the

    same node). So the high current pins on the node need to be connected

    with wide traces, but the signal level pins do not. If I allow all of

    the pins to be high current traces, I can't get it to route.

     

    That's why I said I could split the high current and signal level

    pins on the net with a 0 ohm resistor. Then Eagle wouldn't

    automatically make all the traces high current traces. But that

    sounds like a clumsy solution. Seems better to make the copper

    thicker then make all the traces less wide.

     

    Thanks for the suggestion.

     

    Dave

     

     

    If you have organised the positions of the high current points then you

    should manually route them with the desired width and then let the auto

    router do the remaining unrouted nets narrower.

     

    Using the autorouter entirely, you could route with the setting you mention.

    At this point all you wide traces are complete. Then ripup every thing

    except the wide net name. Then ripup any remaining wide traces that should

    be narrow. Next change the class width to narrow and run the autorouter

    again

     

    HTH

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Ivan,

     

    Thanks for the suggestions.  Yes, that's pretty much what I thought

    needed to be done.  But as my initial report said, I'm a new user so

    I'm still learning a lot.  One thing that stops me from manually

    routing is I ran into a roadblock adding vias.  I couldn't figure out

    how to make the corresponding hole in the ground plane to run the via through.

     

    In the meantime, I figure I can go to 2 oz copper and thinner

    traces.  I'm pretty close in routing everything (3 wires out of 350),

    so figure I can get there with some care.

     

    Not sure about some manual routing.  I don't know enough about Eagle yet.

     

    Thanks again!!!

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Dave,

     

    If you insist in 0-ohm "bridges", you might (most likely, according to your description how this is becoming complicated) want to add more than one split-resistor per net.

     

    To get a good estimation about number of 0-ohm resistors needed, perform the following steps: (1) run autorouter, (2) highlight trace of interest, (3) count number of trace branches mixing high and low current flows. These joints are initial candidates for your 0-ohm resistors location.

     

     

    BTW: I prefer (at least) partial manual routing.

     

     

    Best wishes,  Ivan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Morosh

    Hi Morosh,

     

    Yes, that is where I started in my original post.  I tried doing it and it got complicated.  Maybe I'll try again.

     

    Thanks,

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Morosh
    Morosh over 14 years ago in reply to e14 Contributor

    On 10/06/2012 09:10, Dave Wills wrote:

    My apologies if I'm being dense.

     

    I don't appear to be able to change the width on any unrouted traces.  Am I missing something?

     

    Manually routing some nodes doesn't seem like a good option.  If I tweak anything and need to start over, it takes a lot of time.

     

    I could route the wide traces first, but I can't rip some of the traces on a node and leave others alone, then auto routed the ripped wide traces with a smaller width.  At least, not without a lot of manual work.  Seems I'd need to route wide traces, rip the ones that don't need to be wide, then change the width of the signals on that net, and finally continue routing with the new widths.  Again, this is a lot of manual work.

     

    To give an idea, here are my high current nodes:

     

    N$61  C21      1        P$1        3 *** up to 1 amp

              C22      1        P$1        3 *** up to 1 amp

              L3        2        2          3 *** up to 2 amps

              R24      1        P$1        3 signal level

              R25      2        P$2        3 signal level

              R26      C        P$2        3 *** up to 2 amps

              R27      2        P$2        3 signal level

              U4       9        VON        3 signal level

     

    N$60   C19      2        P$2        3 signal level

              L3        1        1            3 *** up to 2 amps

              U4       11       SW         3 *** up to 1 amp

              U4       12       SW         3 *** up to 1 amp

              U4       13       SW         3 *** up to 1 amp

              U4       14       SW         3 *** up to 1 amp

              U4       15       SW         3 *** up to 1 amp

              U4       16       SW         3 *** up to 1 amp

     

    N$62   Q8       4        S          3 *** up to 2 amps

              R26      A        P$1        3 *** up to 2 amps

              U5       6        -IN        3 signal level

              U7       6        -IN        3 signal level

     

    N$63   Q10      4        S          3 *** up to 2 amps

              Q11      4        S          3 *** up to 2 amps

              Q8       1        D          3 *** up to 2 amps

              Q8       2        D          3 *** up to 2 amps

              Q8       5        D          3 *** up to 2 amps

              Q8       6        D          3 *** up to 2 amps

     

    You can see that there are low current (skinny traces) mixed in with high current (wide) traces.  Even though the traces that need to be wide are near each other, the signal level traces get routed as wide traces.  When these need to go through vias and inner layers, it doesn't leave enough room for the rest of the signal level traces.  (Note that I have created some polygons around some of the signals, for example U4 11 - 16.  That does help routing somewhat.)

     

    And then, consider the same problem when you look at GND.  I have a similar number of high current traces.  Though I have a ground plane, I need to specify some vias as larger than others into the ground plane in order to carry the current.

     

    I'm starting to think that maybe Eagle isn't useful for boards with mixed trace widths and high density.  I might be better off having a professional layout firm do the last step.

     

    Thanks for reading.

     

    Dave

     

    In your schematic, connect the non_high current nets to the high current

    nets with a 0 ohm resistor, they'll have a different name.

    Specify the adequate width to the high-current nets using class, route

    as usual, then remove the resistor and connect directly.

    there is some work in the schematic.

    HTH

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    My apologies if I'm being dense.

     

    I don't appear to be able to change the width on any unrouted traces.  Am I missing something?

     

    Manually routing some nodes doesn't seem like a good option.  If I tweak anything and need to start over, it takes a lot of time.

     

    I could route the wide traces first, but I can't rip some of the traces on a node and leave others alone, then auto routed the ripped wide traces with a smaller width.  At least, not without a lot of manual work.  Seems I'd need to route wide traces, rip the ones that don't need to be wide, then change the width of the signals on that net, and finally continue routing with the new widths.  Again, this is a lot of manual work.

     

    To give an idea, here are my high current nodes:

     

    N$61  C21      1        P$1        3 *** up to 1 amp
             C22      1        P$1        3 *** up to 1 amp
             L3        2        2          3 *** up to 2 amps
             R24      1        P$1        3 signal level
             R25      2        P$2        3 signal level
             R26      C        P$2        3 *** up to 2 amps
             R27      2        P$2        3 signal level
             U4       9        VON        3 signal level

     

    N$60   C19      2        P$2        3 signal level
             L3        1        1            3 *** up to 2 amps
             U4       11       SW         3 *** up to 1 amp
             U4       12       SW         3 *** up to 1 amp
             U4       13       SW         3 *** up to 1 amp
             U4       14       SW         3 *** up to 1 amp
             U4       15       SW         3 *** up to 1 amp
             U4       16       SW         3 *** up to 1 amp

     

    N$62   Q8       4        S          3 *** up to 2 amps
             R26      A        P$1        3 *** up to 2 amps
             U5       6        -IN        3 signal level
             U7       6        -IN        3 signal level

     

    N$63   Q10      4        S          3 *** up to 2 amps
             Q11      4        S          3 *** up to 2 amps
             Q8       1        D          3 *** up to 2 amps
             Q8       2        D          3 *** up to 2 amps
             Q8       5        D          3 *** up to 2 amps
             Q8       6        D          3 *** up to 2 amps

     

    You can see that there are low current (skinny traces) mixed in with high current (wide) traces.  Even though the traces that need to be wide are near each other, the signal level traces get routed as wide traces.  When these need to go through vias and inner layers, it doesn't leave enough room for the rest of the signal level traces.  (Note that I have created some polygons around some of the signals, for example U4 11 - 16.  That does help routing somewhat.)

     

    And then, consider the same problem when you look at GND.  I have a similar number of high current traces.  Though I have a ground plane, I need to specify some vias as larger than others into the ground plane in order to carry the current.

     

    I'm starting to think that maybe Eagle isn't useful for boards with mixed trace widths and high density.  I might be better off having a professional layout firm do the last step.

     

    Thanks for reading.

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    My apologies if I'm being dense.

     

    I don't appear to be able to change the width on any unrouted traces.  Am I missing something?

     

    Manually routing some nodes doesn't seem like a good option.  If I tweak anything and need to start over, it takes a lot of time.

     

    I could route the wide traces first, but I can't rip some of the traces on a node and leave others alone, then auto routed the ripped wide traces with a smaller width.  At least, not without a lot of manual work.  Seems I'd need to route wide traces, rip the ones that don't need to be wide, then change the width of the signals on that net, and finally continue routing with the new widths.  Again, this is a lot of manual work.

     

    To give an idea, here are my high current nodes:

     

    N$61  C21      1        P$1        3 *** up to 1 amp
             C22      1        P$1        3 *** up to 1 amp
             L3        2        2          3 *** up to 2 amps
             R24      1        P$1        3 signal level
             R25      2        P$2        3 signal level
             R26      C        P$2        3 *** up to 2 amps
             R27      2        P$2        3 signal level
             U4       9        VON        3 signal level

     

    N$60   C19      2        P$2        3 signal level
             L3        1        1            3 *** up to 2 amps
             U4       11       SW         3 *** up to 1 amp
             U4       12       SW         3 *** up to 1 amp
             U4       13       SW         3 *** up to 1 amp
             U4       14       SW         3 *** up to 1 amp
             U4       15       SW         3 *** up to 1 amp
             U4       16       SW         3 *** up to 1 amp

     

    N$62   Q8       4        S          3 *** up to 2 amps
             R26      A        P$1        3 *** up to 2 amps
             U5       6        -IN        3 signal level
             U7       6        -IN        3 signal level

     

    N$63   Q10      4        S          3 *** up to 2 amps
             Q11      4        S          3 *** up to 2 amps
             Q8       1        D          3 *** up to 2 amps
             Q8       2        D          3 *** up to 2 amps
             Q8       5        D          3 *** up to 2 amps
             Q8       6        D          3 *** up to 2 amps

     

    You can see that there are low current (skinny traces) mixed in with high current (wide) traces.  Even though the traces that need to be wide are near each other, the signal level traces get routed as wide traces.  When these need to go through vias and inner layers, it doesn't leave enough room for the rest of the signal level traces.  (Note that I have created some polygons around some of the signals, for example U4 11 - 16.  That does help routing somewhat.)

     

    And then, consider the same problem when you look at GND.  I have a similar number of high current traces.  Though I have a ground plane, I need to specify some vias as larger than others into the ground plane in order to carry the current.

     

    I'm starting to think that maybe Eagle isn't useful for boards with mixed trace widths and high density.  I might be better off having a professional layout firm do the last step.

     

    Thanks for reading.

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Ivan,

     

    Thanks for the suggestions.  Yes, that's pretty much what I thought

    needed to be done.  But as my initial report said, I'm a new user so

    I'm still learning a lot.  One thing that stops me from manually

    routing is I ran into a roadblock adding vias.  I couldn't figure out

    how to make the corresponding hole in the ground plane to run the via through.

     

    In the meantime, I figure I can go to 2 oz copper and thinner

    traces.  I'm pretty close in routing everything (3 wires out of 350),

    so figure I can get there with some care.

     

    Not sure about some manual routing.  I don't know enough about Eagle yet.

     

    Thanks again!!!

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Dave,

     

    If you insist in 0-ohm "bridges", you might (most likely, according to your description how this is becoming complicated) want to add more than one split-resistor per net.

     

    To get a good estimation about number of 0-ohm resistors needed, perform the following steps: (1) run autorouter, (2) highlight trace of interest, (3) count number of trace branches mixing high and low current flows. These joints are initial candidates for your 0-ohm resistors location.

     

     

    BTW: I prefer (at least) partial manual routing.

     

     

    Best wishes,  Ivan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Morosh

    Hi Morosh,

     

    Yes, that is where I started in my original post.  I tried doing it and it got complicated.  Maybe I'll try again.

     

    Thanks,

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Morosh
    Morosh over 14 years ago in reply to e14 Contributor

    On 10/06/2012 09:10, Dave Wills wrote:

    My apologies if I'm being dense.

     

    I don't appear to be able to change the width on any unrouted traces.  Am I missing something?

     

    Manually routing some nodes doesn't seem like a good option.  If I tweak anything and need to start over, it takes a lot of time.

     

    I could route the wide traces first, but I can't rip some of the traces on a node and leave others alone, then auto routed the ripped wide traces with a smaller width.  At least, not without a lot of manual work.  Seems I'd need to route wide traces, rip the ones that don't need to be wide, then change the width of the signals on that net, and finally continue routing with the new widths.  Again, this is a lot of manual work.

     

    To give an idea, here are my high current nodes:

     

    N$61  C21      1        P$1        3 *** up to 1 amp

              C22      1        P$1        3 *** up to 1 amp

              L3        2        2          3 *** up to 2 amps

              R24      1        P$1        3 signal level

              R25      2        P$2        3 signal level

              R26      C        P$2        3 *** up to 2 amps

              R27      2        P$2        3 signal level

              U4       9        VON        3 signal level

     

    N$60   C19      2        P$2        3 signal level

              L3        1        1            3 *** up to 2 amps

              U4       11       SW         3 *** up to 1 amp

              U4       12       SW         3 *** up to 1 amp

              U4       13       SW         3 *** up to 1 amp

              U4       14       SW         3 *** up to 1 amp

              U4       15       SW         3 *** up to 1 amp

              U4       16       SW         3 *** up to 1 amp

     

    N$62   Q8       4        S          3 *** up to 2 amps

              R26      A        P$1        3 *** up to 2 amps

              U5       6        -IN        3 signal level

              U7       6        -IN        3 signal level

     

    N$63   Q10      4        S          3 *** up to 2 amps

              Q11      4        S          3 *** up to 2 amps

              Q8       1        D          3 *** up to 2 amps

              Q8       2        D          3 *** up to 2 amps

              Q8       5        D          3 *** up to 2 amps

              Q8       6        D          3 *** up to 2 amps

     

    You can see that there are low current (skinny traces) mixed in with high current (wide) traces.  Even though the traces that need to be wide are near each other, the signal level traces get routed as wide traces.  When these need to go through vias and inner layers, it doesn't leave enough room for the rest of the signal level traces.  (Note that I have created some polygons around some of the signals, for example U4 11 - 16.  That does help routing somewhat.)

     

    And then, consider the same problem when you look at GND.  I have a similar number of high current traces.  Though I have a ground plane, I need to specify some vias as larger than others into the ground plane in order to carry the current.

     

    I'm starting to think that maybe Eagle isn't useful for boards with mixed trace widths and high density.  I might be better off having a professional layout firm do the last step.

     

    Thanks for reading.

     

    Dave

     

    In your schematic, connect the non_high current nets to the high current

    nets with a 0 ohm resistor, they'll have a different name.

    Specify the adequate width to the high-current nets using class, route

    as usual, then remove the resistor and connect directly.

    there is some work in the schematic.

    HTH