Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Mac 6.2 Backup and Auto Save
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 1200 views
  • Users 0 members are here
Related

Mac 6.2 Backup and Auto Save

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I just lost about 4 hours of work from last night because my files

weren't saved when I closed Eagle. I have Auto Save Interval set to 5

min.and Automatically Save Project File set. These functions either are

not working, or I don't understand what they do. Here are some

questions that I can't find an answer to in the manual.

 

1) If the number of backup files are set to 9, and you have filled the

9 slots, what happens next? Does Eagle write over the old backups or

just stop autobacking up. In my case Eagle stopped autobacking the

files.

 

2) If a backup file is generated, is the active file also saved?

 

3) If Automatically Save Project File is set, does this save the board

and schematic files? In my case this definitely did not happen.

 

4) If a file is changed (schematic, library, or board) is it marked as

"dirty" and will Eagle generate a dialog asking to save the file when

the file is being closed? This seems to happen erratically. Sometimes

yes, sometimes no.

 

Thanks

 

 

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 6/28/2012 12:11 AM, Joe wrote:

     

     

    So, if Eagle crashes (like it did today when I tried to Disapprove some

    errors in the DRC check, actually it froze and I had to force quit), and

    so the file is not saved, the latest backup will actually be x## and not

    x#1. Right?

     

    >

    That is correct assuming more than 5 minutes had elapsed from the last save.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 2012-06-27 21:40:26 +0000, Jorge Garcia <jorge@cadsoftusa.com> said:

     

    On 6/21/2012 11:53 AM, Joe wrote:

    >> Hi,

    >>

    >> I just lost about 4 hours of work from last night because my files

    >> weren't saved when I closed Eagle. I have Auto Save Interval set to 5

    >> min.and Automatically Save Project File set. These functions either are

    >> not working, or I don't understand what they do. Here are some questions

    >> that I can't find an answer to in the manual.

    >>

    >> 1) If the number of backup files are set to 9, and you have filled the 9

    >> slots, what happens next? Does Eagle write over the old backups or just

    >> stop autobacking up. In my case Eagle stopped autobacking the files.

    When you reach the max number of backups eagle will then overwrite 1,

    it's always the most recent backup. It won't loop through the sequence

    it will just overwrite 1, so that would explain why it may appear that

    eagle hasn't backed up in a while, look at the first back up #1.

     

    >>

    >> 2) If a backup file is generated, is the active file also saved?

    This requires some clarification. Let's say you set your save interval

    to 5 minutes. EAGLE counts this time from the last save, so if you save

    every three minutes for 30 minutes then EAGLE will not generate a

    backup during that time span because 5 minutes do not elapse from any

    given save.

     

    If more than 5 minutes elapse from the last save and you make a change

    eagle creates a x## file the next time you save it will become x#1. If

    you don't save the x## file will still be there and that will be your

    most recent backup.

     

    This behaviour should also explain what you're seeing, with long gaps

    between backups.

     

    >>

    >> 3) If Automatically Save Project File is set, does this save the board

    >> and schematic files? In my case this definitely did not happen.

    This option will only save the board and schematic files if they're

    defined as a Project. A project will appear as a red folder in the

    EAGLE control panel, not a yellow folder. The main difference is that a

    project folder contains a file with a .epf extension. If you're just

    saving your files to ordinary folders and not saving them as projects

    then this option doesn't apply and your work won't be automatically

    saved.

    >>

    >> 4) If a file is changed (schematic, library, or board) is it marked as

    >> "dirty" and will Eagle generate a dialog asking to save the file when

    >> the file is being closed? This seems to happen erratically. Sometimes

    >> yes, sometimes no.

    If a change has been made to the file then yes EAGLE does mark the file

    as "dirty" and the dialog should appear warning you.

    >>

    >> Thanks

    >>

    >>

     

    Hi Joe,

     

    I've answered your questions inline above.

     

    hth,

    Jorge Garcia

     

    Thanks for the response.

     

    So, if Eagle crashes (like it did today when I tried to Disapprove some

    errors in the DRC check, actually it froze and I had to force quit),

    and so the file is not saved, the latest backup will actually be x##

    and not x#1. Right?

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 6/21/2012 11:53 AM, Joe wrote:

    Hi,

     

    I just lost about 4 hours of work from last night because my files

    weren't saved when I closed Eagle. I have Auto Save Interval set to 5

    min.and Automatically Save Project File set. These functions either are

    not working, or I don't understand what they do. Here are some questions

    that I can't find an answer to in the manual.

     

    1) If the number of backup files are set to 9, and you have filled the 9

    slots, what happens next? Does Eagle write over the old backups or just

    stop autobacking up. In my case Eagle stopped autobacking the files.

    When you reach the max number of backups eagle will then overwrite 1,

    it's always the most recent backup. It won't loop through the sequence

    it will just overwrite 1, so that would explain why it may appear that

    eagle hasn't backed up in a while, look at the first back up #1.

     

     

    2) If a backup file is generated, is the active file also saved?

    This requires some clarification. Let's say you set your save interval

    to 5 minutes. EAGLE counts this time from the last save, so if you save

    every three minutes for 30 minutes then EAGLE will not generate a backup

    during that time span because 5 minutes do not elapse from any given save.

     

    If more than 5 minutes elapse from the last save and you make a change

    eagle creates a x## file the next time you save it will become x#1. If

    you don't save the x## file will still be there and that will be your

    most recent backup.

     

    This behaviour should also explain what you're seeing, with long gaps

    between backups.

     

     

    3) If Automatically Save Project File is set, does this save the board

    and schematic files? In my case this definitely did not happen.

    This option will only save the board and schematic files if they're

    defined as a Project. A project will appear as a red folder in the EAGLE

    control panel, not a yellow folder. The main difference is that a

    project folder contains a file with a .epf extension. If you're just

    saving your files to ordinary folders and not saving them as projects

    then this option doesn't apply and your work won't be automatically saved.

     

    4) If a file is changed (schematic, library, or board) is it marked as

    "dirty" and will Eagle generate a dialog asking to save the file when

    the file is being closed? This seems to happen erratically. Sometimes

    yes, sometimes no.

    If a change has been made to the file then yes EAGLE does mark the file

    as "dirty" and the dialog should appear warning you.

     

    Thanks

     

    >

     

    Hi Joe,

     

    I've answered your questions inline above.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 2012-06-21 15:53:47 +0000, Joe <jtowich@montanasky.net> said:

     

    Hi,

     

    I just lost about 4 hours of work from last night because my files

    weren't saved when I closed Eagle. I have Auto Save Interval set to 5

    min.and Automatically Save Project File set. These functions either are

    not working, or I don't understand what they do. Here are some

    questions that I can't find an answer to in the manual.

     

    1) If the number of backup files are set to 9, and you have filled the

    9 slots, what happens next? Does Eagle write over the old backups or

    just stop autobacking up. In my case Eagle stopped autobacking the

    files.

     

    2) If a backup file is generated, is the active file also saved?

     

    3) If Automatically Save Project File is set, does this save the board

    and schematic files? In my case this definitely did not happen.

     

    4) If a file is changed (schematic, library, or board) is it marked as

    "dirty" and will Eagle generate a dialog asking to save the file when

    the file is being closed? This seems to happen erratically. Sometimes

    yes, sometimes no.

     

    Thanks

     

    Anyone home?

     

    I just noticed that Eagle hasn't autobackedup anything for the past two

    days. Does this feature work?