Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Seems to be a mistake in  V-REG.lbr SOT89R
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 487 views
  • Users 0 members are here
Related

Seems to be a mistake in  V-REG.lbr SOT89R

e14 Contributor
e14 Contributor over 14 years ago

Hello,

It seems I found a mistake in standard library

SOT89R has 2 3 1 oder instead of usual 1 2 3

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hello Dmitry Chikov !:

     

    It seems I found a mistake in standard library

    SOT89R has 2 3 1 oder instead of usual 1 2 3

     

    The most experienced users are talking : NOT to use any original lib

    before exactly check for some mistakes !!!. Best way is to create own

    libraries. Really a lot of libraries have very different errors incl.

    wrong raster for TQFP, wrong connection pins to pads etc.

     

    BR

    --

    Grzegorz Zalot

     

    complex ltd.

    office tel/fax : +48 32 2505840

    mobil : +48 501 301515

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thats true. I had to check it. But I thaught if it is 3 pin IC, which is widely used - there were no chance to make a mistake. And it was vice versa - I ordered component according to LBR not find LBR according to IC. That was the problem. It would be really funny when Eagle make a cart directly from eagle app.

    You use component from LBR Eagle -> order -> FAIL!!!! .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thats true. I had to check it. But I thaught if it is 3 pin IC, which is widely used - there were no chance to make a mistake. And it was vice versa - I ordered component according to LBR not find LBR according to IC. That was the problem. It would be really funny when Eagle make a cart directly from eagle app.

    You use component from LBR Eagle -> order -> FAIL!!!! .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hello Dmitry Chikov !:

    Thats true. I had to check it. But I thaught if it is 3 pin IC, which

    is widely used - there were no chance to make a mistake. And it was

    vice versa - I ordered component according to LBR not find LBR

    according to IC. That was the problem. I would be really funny when

    Eagle make a cart directly from eagle app.

     

    This is possible using apriopriate ULP. But of course you MUST have good

    libraries.

     

    Did you try the new features connecting a bit Eagle to Farnell ?

     

    You use component from LBR Eagle -> order -> FAIL!!!! .

     

    I never used Eagle to generate order of material. And maybe 0,01% of

    material is from Farnell ...

     

    But I check all components which I am using in my projects. Some are

    from "original lib" but exactly checked with data sheet.

     

    BR

    --

    Grzegorz Zalot

     

    complex ltd.

    office tel/fax : +48 32 2505840

    mobil : +48 501 301515