Is there a command to highlight unrouted signals on a board besides the layer on/off of unrouted signals? Dense boards make finding unrouted wires difficult to see.
Thanks,
Bob Moreno
Is there a command to highlight unrouted signals on a board besides the layer on/off of unrouted signals? Dense boards make finding unrouted wires difficult to see.
Thanks,
Bob Moreno
On 11.07.2012 22:04, Bob Moreno wrote:
Is there a command to highlight unrouted signals on a board besides
the layer on/off of unrouted signals? Dense boards make finding
unrouted wires difficult to see.
Thanks,
Bob Moreno
Go to Options/Set/Misc and set the Catch factor to 100%.
Activate ROUTE and click into the drawing. The airwire next to the
mouse cursor catches the cursor........
--
Mit freundlichen Gruessen / Best regards
Richard Hammerl
CadSoft Support -- hotline@cadsoft.de
FAQ: http://www.cadsoft.de/training/faq/
Thanks for the tip. Any way to just highlight without cursor use, so that no routes are started, just to see where one stands as far as routing goes?
Thanks again for the tip.
Thanks for the tip. Any way to just highlight without cursor use, so that no routes are started, just to see where one stands as far as routing goes?
Thanks again for the tip.