Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Polygon trouble (4.16r2)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 445 views
  • Users 0 members are here
Related

Polygon trouble (4.16r2)

e14 Contributor
e14 Contributor over 14 years ago

In the attached file I've created two polygons on the bottom layer on the

lower half of the board.  The upper polygon consists of three regions: a

horizontal one with two fingers extending from its bottom edge.  I've named

all the polygons GND (the same as my GND net) and was asked if I wanted to

connect them to GND, to which I said yes.  Both polygons are connected to a

ground trace with a single wire.  My problem is that only the horizontal

region displays as filled in Eagle, and outputs to the gerber for the

bottom layer.  The three other polygons don't display as filled, and don't

appear in the gerber.  What am I dong wrong?  Thanks.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Karl Lautman wrote:

     

    >In the attached file I've created two polygons on the bottom layer on the

    >lower half of the board.  The upper polygon consists of three regions: a

    >horizontal one with two fingers extending from its bottom edge.  I've named

    >all the polygons GND (the same as my GND net) and was asked if I wanted to

    >connect them to GND, to which I said yes.  Both polygons are connected to a

    >ground trace with a single wire.  My problem is that only the horizontal

    >region displays as filled in Eagle, and outputs to the gerber for the

    >bottom layer.  The three other polygons don't display as filled, and don't

    >appear in the gerber.  What am I dong wrong?  Thanks.

     

    this polygons don't have actual connections (pad, via, track) to the

    related signal.

     

    But you can change their orphant flag to on (change orphans on) to get

    them filled without connection.

     

    By the way, the small stub at (1,8 0,75) to (1,8 0,8) is not connected

    to the gnd net and therefor does not take care of connecting the lower

    polygon.

    It also causes an overlap DRC error (3 actually).

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Karl Lautman wrote:

     

    >In the attached file I've created two polygons on the bottom layer on the

    >lower half of the board.  The upper polygon consists of three regions: a

    >horizontal one with two fingers extending from its bottom edge.  I've named

    >all the polygons GND (the same as my GND net) and was asked if I wanted to

    >connect them to GND, to which I said yes.  Both polygons are connected to a

    >ground trace with a single wire.  My problem is that only the horizontal

    >region displays as filled in Eagle, and outputs to the gerber for the

    >bottom layer.  The three other polygons don't display as filled, and don't

    >appear in the gerber.  What am I dong wrong?  Thanks.

     

    this polygons don't have actual connections (pad, via, track) to the

    related signal.

     

    But you can change their orphant flag to on (change orphans on) to get

    them filled without connection.

     

    By the way, the small stub at (1,8 0,75) to (1,8 0,8) is not connected

    to the gnd net and therefor does not take care of connecting the lower

    polygon.

    It also causes an overlap DRC error (3 actually).

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks, Lorenz.  I finally got things to work, but I'm not sure what I did

    differently than I did originally.  I guess I'm wondering what the proper

    way is to connect a polygon to a signal.  E.g., if I want to create a small

    ground plane, I draw the outline with the polygon tool and name it GND (if

    that's the name of all my ground signals).  Don't I still need to connect

    the polygon to a GND signal somewhere?  I've been doing that by drawing a

    small bridge using the wire tool and eventually it works, but I figure it

    should work the first time unless there's some other step I'm skipping.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.