Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Nets won't connect to pins
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 1394 views
  • Users 0 members are here
Related

Nets won't connect to pins

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I'm having problems making changes to a schematic I created a couple of

weeks ago. Basically I can't get any new nets to actually connect to any of

the pins I drop them on. I can place the ends of the net without problems,

but if I then try to pick up and move either the component or the net then

the two become separated (demonstrating that they weren't connected

properly in the first place). I've had this problem before, and it can

normally be cured by matching the size of the schematic grid to the

component grid. However, this isn't working this time.

 

I've also tried setting the grid size to 'finest' and zooming right onto

the components before attempting the connection, but the results are the

same. There's nothing special about any of the components I'm using either,

I've already got several copies of them successfully connected elsewhere on

the same schematic.

 

I'm using version 5.11 for windows running on windows XP professional.

 

Any help appreciated!

 

Thanks

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Ok, I seem to have got a work-around even if I still don't know the exact

    cause of the problem in the first place. I've deleted the extra components

    from the schematic, and then added them again from the library, I can now

    connect a net to them without problems.

     

    It appears (IMHO) that the components somehow 'inherited' it's grid

    settings when I cut 'n' pasted them into the schematic in the 1st place,

    somehow preventing them from connecting to the net in the new schematic.

     

    I'm still not sure why (assuming this is the case) even when I set the grid

    to 'finest' I couldn't attach any net connections to them.

     

    If anyone has a better answer, then I'd still like to know.

     

    Thanks 

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Lima schrieb:

     

    Ok, I seem to have got a work-around even if I still don't know the exact

    cause of the problem in the first place. I've deleted the extra components

    from the schematic, and then added them again from the library, I can now

    connect a net to them without problems.

     

    Obviously the symbols were off-grid for whatever reason/cause.

     

    You might also have snapped them to the grid again by holding the ctl

    key down when picking them with MOVE (see manual and/or help).

     

    (Additionally, there are snapping ULPs if it's about many symbols.)

     

    It appears (IMHO) that the components somehow 'inherited' it's grid

    settings when I cut 'n' pasted them into the schematic in the 1st place,

    somehow preventing them from connecting to the net in the new schematic.

     

    Hard to say afterwards what has happened, at least for anyone else.

    Eventually you had another grid active when doing the CUT/PASTE, or you

    used the right mouse button after CUT instead of defining an on-grid

    reference coordinate with the left mouse button...

     

    I'm still not sure why (assuming this is the case) even when I set the grid

    to 'finest' I couldn't attach any net connections to them.

     

    Just Forget "grid finest" - it's simply not possible to exactly hit

    the pins with that, and finally you make things even worse by moving

    more objects into off-grid positions.

     

    Tilmann

     

    P.S. There's only one good use for "grid finest": measuring distances

    (related to the MARK position), since EAGLE lacks a proper instrument

    for this.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Lima schrieb:

     

    Ok, I seem to have got a work-around even if I still don't know the exact

    cause of the problem in the first place. I've deleted the extra components

    from the schematic, and then added them again from the library, I can now

    connect a net to them without problems.

     

    Obviously the symbols were off-grid for whatever reason/cause.

     

    You might also have snapped them to the grid again by holding the ctl

    key down when picking them with MOVE (see manual and/or help).

     

    (Additionally, there are snapping ULPs if it's about many symbols.)

     

    It appears (IMHO) that the components somehow 'inherited' it's grid

    settings when I cut 'n' pasted them into the schematic in the 1st place,

    somehow preventing them from connecting to the net in the new schematic.

     

    Hard to say afterwards what has happened, at least for anyone else.

    Eventually you had another grid active when doing the CUT/PASTE, or you

    used the right mouse button after CUT instead of defining an on-grid

    reference coordinate with the left mouse button...

     

    I'm still not sure why (assuming this is the case) even when I set the grid

    to 'finest' I couldn't attach any net connections to them.

     

    Just Forget "grid finest" - it's simply not possible to exactly hit

    the pins with that, and finally you make things even worse by moving

    more objects into off-grid positions.

     

    Tilmann

     

    P.S. There's only one good use for "grid finest": measuring distances

    (related to the MARK position), since EAGLE lacks a proper instrument

    for this.