EAGLE User Support (English) Eagle v6.2.0 Crashes using ULP or Design Rules?
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
  • Replies 14 replies
  • Subscribers 182 subscribers
  • Views 1082 views
  • Users 0 members are here
  • eagle
  • crash
  • mac
Related

Eagle v6.2.0 Crashes using ULP or Design Rules?

Former Member
Former Member over 13 years ago

Hi All,

 

I am experiencing application crashes with v6.2.0 of Eagle running under Mountain Lion OSX 10.8.0. Whenever I try to use the ULP function or load a Design Rules file - The File List window appears momentarily, then closes and Eagle crashes.

 

I have tried removing the Eagle folder/Application. Reinstalling v6.2.0 and v6.1.0 but both have the same issue.

 

Has anyone else experienced this issue? Does anyone have any ideas why this might be happening?

 

Many thank, in advance.

Jeremy

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 12 years ago

    After going through the permissions deal I was still craashing

    Then Jorge told me about not saving to apps folder

    So I setup a folder in Documents and put all the folders in there except the App itself and the Bin folder I left in a folder in my apps folder.

    I relinked the directly folders in Eagle and so far no crashing at all when doing a save as to a different folder

    Hope that helps someone

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    I will corroborate with what user John Suhr says.

     

    I am running OSX 10.8.5 with Eagle 6.5.0. Every time I tried to run a ULP or CAM job (or anything that opened a folder window) Eagle crashed on me.  Changing permissions didn't work, but moving everything except the app and the /bin folder OUT of of the Applications/EAGLE-6.5.0 folder did work.  I had to do this through terminal, since I needed sudo permissions.  I then went into the Eagle's Options>Directories dropdown and updated the paths for everything.  It works now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    I will corroborate with what user John Suhr says.

     

    I am running OSX 10.8.5 with Eagle 6.5.0. Every time I tried to run a ULP or CAM job (or anything that opened a folder window) Eagle crashed on me.  Changing permissions didn't work, but moving everything except the app and the /bin folder OUT of of the Applications/EAGLE-6.5.0 folder did work.  I had to do this through terminal, since I needed sudo permissions.  I then went into the Eagle's Options>Directories dropdown and updated the paths for everything.  It works now.